Using E2 studio, is it possible to pad the SREC output file registers 0x0100 A150 – 0x0100 A16F with 32 bytes consisting of 0xFF?
Currently only pads from 0x0100 A150 to 0x0100 A15F with 16 bytes of 0xFF.
Using RA6 MCU R7FA6M3AH
Cheers,
Chris
The FSP configurator BSP properties does not have entries for the AWS settings which are at the 0x0100A16x addresses. The AWS settings can be modified by application code and FSP provided APIs.
Ian.