USB PCDC: descriptor request failed

Hello,

I'm working on the USB PCDC on RA6M5 MCU. When I connect the USB to the Host(Windows machine), I got this error:

Here is the USB PCDC stack configuration:

Here is the init code:

void USBInit(void)
{
    fsp_err_t err = FSP_SUCCESS;
    
    R_IOPORT_PinCfg(
            &g_ioport_ctrl,
            BSP_IO_PORT_04_PIN_07,
            ((uint32_t) IOPORT_CFG_PERIPHERAL_PIN
                | (uint32_t) IOPORT_PERIPHERAL_USB_FS));
    
    err = R_USB_Open(&g_basic0_ctrl, &g_basic0_cfg);
    if (err == FSP_ERR_USB_BUSY)
    {
        // usb is already open, close and reopen to re-enable interrupts
        R_USB_Close(&g_basic0_ctrl);
        err = R_USB_Open(&g_basic0_ctrl, &g_basic0_cfg);
    }
    
    if (err != FSP_SUCCESS)
    {
        printf("ERROR: faild to open usb\n");
        return;
    }
    
    err = R_USB_ClassTypeGet(&g_basic0_ctrl, &g_usb_class_type);
    if (err != FSP_SUCCESS)
    {
        printf("ERROR: faild to get usb class\n");
        return;
    }
    
    err = R_USB_ModuleNumberGet(&g_basic0_ctrl, &g_usb_module_number);
    if (err != FSP_SUCCESS)
    {
        printf("ERROR: faild to get module number\n");
        return;
    }
}

The init code works. Then I called this:

static void usbProcessEvents(void)
{
    fsp_err_t err = FSP_SUCCESS;
    static usb_pcdc_linecoding_t g_line_coding;
    usb_instance_ctrl_t event_ctrl = g_basic0_ctrl;
    
    do
    {
        err = R_USB_EventGet(&event_ctrl, &usb_event);
        if (err != FSP_SUCCESS)
        {
            break;
        }

        switch (usb_event)
        {
            case USB_STATUS_CONFIGURED:
            {
                b_usb_attach = true;
                
                err = R_USB_Read(
                        &event_ctrl,
                        g_read_buffer,
                        READ_BUFFER_SIZE,
                        (uint8_t)g_usb_class_type);
                if (err != FSP_SUCCESS)
                {
                    printf("USB: starting read failed \r\n");
                }
                break;
            }

            case USB_STATUS_WRITE_COMPLETE:
            {
              ... 
            }
            ...
            default:
            {
                break;
            }
        }
    }
    while (usb_event != USB_STATUS_NONE);
}

Here is the descriptor file I copied from the sample project. I'll adjust it to use our vendor ID and manufacturer ID later:

/***********************************************************************************************************************
 * File Name    : r_usb_pcdc_descriptor.c
 * Description  : USB PCDC Descriptor definition.
 **********************************************************************************************************************/
/***********************************************************************************************************************
 * DISCLAIMER
 * This software is supplied by Renesas Electronics Corporation and is only intended for use with Renesas products. No
 * other uses are authorized. This software is owned by Renesas Electronics Corporation and is protected under all
 * applicable laws, including copyright laws.
 * THIS SOFTWARE IS PROVIDED "AS IS" AND RENESAS MAKES NO WARRANTIES REGARDING
 * THIS SOFTWARE, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING BUT NOT LIMITED TO WARRANTIES OF MERCHANTABILITY,
 * FITNESS FOR A PARTICULAR PURPOSE AND NON-INFRINGEMENT. ALL SUCH WARRANTIES ARE EXPRESSLY DISCLAIMED. TO THE MAXIMUM
 * EXTENT PERMITTED NOT PROHIBITED BY LAW, NEITHER RENESAS ELECTRONICS CORPORATION NOR ANY OF ITS AFFILIATED COMPANIES
 * SHALL BE LIABLE FOR ANY DIRECT, INDIRECT, SPECIAL, INCIDENTAL OR CONSEQUENTIAL DAMAGES FOR ANY REASON RELATED TO THIS
 * SOFTWARE, EVEN IF RENESAS OR ITS AFFILIATES HAVE BEEN ADVISED OF THE POSSIBILITY OF SUCH DAMAGES.
 * Renesas reserves the right, without notice, to make changes to this software and to discontinue the availability of
 * this software. By using this software, you agree to the additional terms and conditions found by accessing the
 * following link:
 * http://www.renesas.com/disclaimer
 *
 * Copyright (C) 2020 Renesas Electronics Corporation. All rights reserved.
 ***********************************************************************************************************************/

/******************************************************************************
 Includes   <System Includes> , "Project Includes"
 ******************************************************************************/
#include <r_usb_basic.h>
#include <r_usb_basic_api.h>
#include "r_usb_basic_cfg.h"

/******************************************************************************
 Macro definitions
 ******************************************************************************/
/* bcdUSB */
#define USB_BCDNUM                      (0x0200U)
/* Release Number */
#define USB_RELEASE                     (0x0200U)
/* DCP max packet size */
#define USB_DCPMAXP                     (64U)
/* Configuration number */
#define USB_CONFIGNUM                   (1U)
/* Vendor ID */
#define USB_VENDORID                    (0x298EU)
/* Product ID */
#define USB_PRODUCTID                   (0x07D1U)

//#define USB_VENDORID                    (0x045BU)
/* Product ID */
//#define USB_PRODUCTID                   (0x5310U)

/* Class-Specific Configuration Descriptors */
#define     USB_PCDC_CS_INTERFACE                               (0x24U)

/* bDescriptor SubType in Communications Class Functional Descriptors */
/* Header Functional Descriptor */
#define     USB_PCDC_DT_SUBTYPE_HEADER_FUNC                     (0x00U)
/* Call Management Functional Descriptor. */
#define     USB_PCDC_DT_SUBTYPE_CALL_MANAGE_FUNC                (0x01U)
/* Abstract Control Management Functional Descriptor. */
#define     USB_PCDC_DT_SUBTYPE_ABSTRACT_CTR_MANAGE_FUNC        (0x02U)
/* Union Functional Descriptor */
#define     USB_PCDC_DT_SUBTYPE_UNION_FUNC                      (0x06U)

/* Communications Class Subclass Codes */
#define     USB_PCDC_CLASS_SUBCLASS_CODE_ABS_CTR_MDL            (0x02U)

/* USB Class Definitions for Communications Devices Specification
 release number in binary-coded decimal. */
#define     USB_PCDC_BCD_CDC          (0x0110U)

/* Descriptor length */
#define USB_PCDC_QD_LEN               (10U)
#define USB_PCDC_CD1_LEN              (67U)
#define STRING_DESCRIPTOR0_LEN        (4U)
#define STRING_DESCRIPTOR1_LEN        (16U)
#define STRING_DESCRIPTOR2_LEN        (44U)
#define STRING_DESCRIPTOR3_LEN        (46U)
#define STRING_DESCRIPTOR4_LEN        (22U)
#define STRING_DESCRIPTOR5_LEN        (18U)
#define STRING_DESCRIPTOR6_LEN        (28U)

/* Descriptor data Mask */
#define USB_UCHAR_MAX                 (0xffU)
#define USB_W_TOTAL_LENGTH_MASK       (256U)
#define USB_W_MAX_PACKET_SIZE_MASK    (64U)
#define USB_PCDC_BCD_CDC_MASK         (256U)

/******************************************************************************
 Private global variables and functions
 ******************************************************************************/

/******************************************************************************
 Exported global variables
 ******************************************************************************/

/******************************************************************************
 Exported global functions (to be accessed by other files)
 ******************************************************************************/

/* Standard Device Descriptor */
uint8_t g_apl_device[USB_DD_BLENGTH + ( USB_DD_BLENGTH % 2)] =
{
    USB_DD_BLENGTH,                                     /*  0:bLength */
    USB_DT_DEVICE,                                      /*  1:bDescriptorType */
    (USB_BCDNUM & (uint8_t) USB_UCHAR_MAX),                     /*  2:bcdUSB_lo */
    ((uint8_t) (USB_BCDNUM >> 8) & (uint8_t) USB_UCHAR_MAX),    /*  3:bcdUSB_hi */
    USB_IFCLS_CDCC,                                     /*  4:bDeviceClass */
    0,                                                  /*  5:bDeviceSubClass */
    0,                                                  /*  6:bDeviceProtocol */
    (uint8_t) USB_DCPMAXP,                              /*  7:bMAXPacketSize(for DCP) */
    (USB_VENDORID & (uint8_t) USB_UCHAR_MAX),                   /*  8:idVendor_lo */
    ((uint8_t) (USB_VENDORID >> 8) & (uint8_t) USB_UCHAR_MAX),  /*  9:idVendor_hi */
    ((uint16_t) USB_PRODUCTID & (uint8_t) USB_UCHAR_MAX),       /* 10:idProduct_lo */
    ((uint8_t) (USB_PRODUCTID >> 8) & (uint8_t) USB_UCHAR_MAX), /* 11:idProduct_hi */
    (USB_RELEASE & (uint8_t) USB_UCHAR_MAX),                    /* 12:bcdDevice_lo */
    ((uint8_t) (USB_RELEASE >> 8) & (uint8_t) USB_UCHAR_MAX),   /* 13:bcdDevice_hi */
    1,                                                  /* 14:iManufacturer */
    2,                                                  /* 15:iProduct */
    6,                                                  /* 16:iSerialNumber */
    USB_CONFIGNUM /* 17:bNumConfigurations */
};

/************************************************************
 *  Device Qualifier Descriptor   *
 ************************************************************/
uint8_t g_apl_qualifier_descriptor[USB_PCDC_QD_LEN + ( USB_PCDC_QD_LEN % 2)] =
{
    USB_PCDC_QD_LEN,                                    /*  0:bLength */
    USB_DT_DEVICE_QUALIFIER,                            /*  1:bDescriptorType */
    (USB_BCDNUM & (uint8_t) USB_UCHAR_MAX),                  /*  2:bcdUSB_lo */
    ((uint8_t) (USB_BCDNUM >> 8) & (uint8_t) USB_UCHAR_MAX), /*  3:bcdUSB_hi */
    0,                                                  /*  4:bDeviceClass */
    0,                                                  /*  5:bDeviceSubClass */
    0,                                                  /*  6:bDeviceProtocol */
    (uint8_t) USB_DCPMAXP,                              /*  7:bMAXPacketSize(for DCP) */
    USB_CONFIGNUM,                                      /*  8:bNumConfigurations */
    0 /*  9:bReserved */
};

/************************************************************
 *  Configuration Or Other_Speed_Configuration Descriptor   *
 ************************************************************/
/* For Full-Speed */
uint8_t g_apl_configuration[USB_PCDC_CD1_LEN + ( USB_PCDC_CD1_LEN % 2)] =
{
    USB_CD_BLENGTH,                 /*  0:bLength */
    USB_SOFT_CHANGE,                /*  1:bDescriptorType */
    USB_PCDC_CD1_LEN % USB_W_TOTAL_LENGTH_MASK, /*  2:wTotalLength(L) */
    USB_PCDC_CD1_LEN / USB_W_TOTAL_LENGTH_MASK, /*  3:wTotalLength(H) */
    2,                              /*  4:bNumInterfaces */
    1,                              /*  5:bConfigurationValue */
    0,                              /*  6:iConfiguration */
    USB_CF_RESERVED | USB_CF_SELFP, /*  7:bmAttributes */
    (10 / 2),                       /*  8:MAXPower (2mA unit) */

    /* Interface Descriptor */
    USB_ID_BLENGTH,                 /*  0:bLength */
    USB_DT_INTERFACE,               /*  1:bDescriptor */
    0,                              /*  2:bInterfaceNumber */
    0,                              /*  3:bAlternateSetting */
    1,                              /*  4:bNumEndpoints */
    USB_IFCLS_CDCC,                 /*  5:bInterfaceClass */
    USB_PCDC_CLASS_SUBCLASS_CODE_ABS_CTR_MDL,   /*  6:bInterfaceSubClass */
    1,                              /*  7:bInterfaceProtocol */
    0,                              /*  8:iInterface */

        /* Communications Class Functional Descriptorss */
        5,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_HEADER_FUNC,    /*  2:bDescriptorSubtype */
        USB_PCDC_BCD_CDC % USB_W_TOTAL_LENGTH_MASK,     /*  3:bcdCDC_lo */
        USB_PCDC_BCD_CDC / USB_W_TOTAL_LENGTH_MASK,     /*  4:bcdCDC_hi */

        /* Communications Class Functional Descriptorss */
        4,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_ABSTRACT_CTR_MANAGE_FUNC,   /*  2:bDescriptorSubtype */
        2,                          /*  3:bmCapabilities */

        /* Communications Class Functional Descriptorss */
        5,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_UNION_FUNC, /*  2:bDescriptorSubtype */
        0,                          /*  3:bMasterInterface */
        1,                          /*  4:bSlaveInterface0 */

        /* Communications Class Functional Descriptorss */
        5,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_CALL_MANAGE_FUNC,   /*  2:bDescriptorSubtype */
        /* D1:1-Device can send/receive call management
         information over a Data Class interface. */
        /* D0:1-Device handles call management itself. */
        3,                          /*  3:bmCapabilities */
        1,                          /*  4:bDataInterface */

        /* Endpoint Descriptor 0 */
        7,                          /*  0:bLength */
        USB_DT_ENDPOINT,            /*  1:bDescriptorType */
        USB_EP_IN | USB_EP3,        /*  2:bEndpointAddress */
        USB_EP_INT,                 /*  3:bmAttribute */
        16,                         /*  4:wMAXPacketSize_lo */
        0,                          /*  5:wMAXPacketSize_hi */
        0x10,                       /*  6:bInterval */

    /* Interface Descriptor */
    USB_ID_BLENGTH,                 /*  0:bLength */
    USB_DT_INTERFACE,               /*  1:bDescriptor */
    1,                              /*  2:bInterfaceNumber */
    0,                              /*  3:bAlternateSetting */
    2,                              /*  4:bNumEndpoints */
    USB_IFCLS_CDCD,                 /*  5:bInterfaceClass */
    0,                              /*  6:bInterfaceSubClass */
    0,                              /*  7:bInterfaceProtocol */
    0,                              /*  8:iInterface */

        /* Endpoint Descriptor 0 */
        USB_ED_BLENGTH,             /*  0:bLength */
        USB_DT_ENDPOINT,            /*  1:bDescriptorType */
        USB_EP_IN | USB_EP1,        /*  2:bEndpointAddress */
        USB_EP_BULK,                /*  3:bmAttribute */
		USB_W_MAX_PACKET_SIZE_MASK, /*  4:wMAXPacketSize_lo */
        0,                          /*  5:wMAXPacketSize_hi */
        0,                          /*  6:bInterval */

        /* Endpoint Descriptor 1 */
        USB_ED_BLENGTH,             /*  0:bLength */
        USB_DT_ENDPOINT,            /*  1:bDescriptorType */
        USB_EP_OUT | USB_EP2,       /*  2:bEndpointAddress */
        USB_EP_BULK,                /*  3:bmAttribute */
		USB_W_MAX_PACKET_SIZE_MASK, /*  4:wMAXPacketSize_lo */
        0,                          /*  5:wMAXPacketSize_hi */
        0,                          /*  6:bInterval */
};

/* For High-Speed */
uint8_t g_apl_hs_configuration[USB_PCDC_CD1_LEN + ( USB_PCDC_CD1_LEN % 2)] =
{
    9,                              /*  0:bLength */
    USB_SOFT_CHANGE,                /*  1:bDescriptorType */
    USB_PCDC_CD1_LEN % USB_W_TOTAL_LENGTH_MASK,         /*  2:wTotalLength(L) */
    USB_PCDC_CD1_LEN / USB_W_TOTAL_LENGTH_MASK,         /*  3:wTotalLength(H) */
    2,                              /*  4:bNumInterfaces */
    1,                              /*  5:bConfigurationValue */
    0,                              /*  6:iConfiguration */
    USB_CF_RESERVED | USB_CF_SELFP, /*  7:bmAttributes */
    (10 / 2),                       /*  8:MAXPower (2mA unit) */

    /* Interface Descriptor */
    9,                              /*  0:bLength */
    USB_DT_INTERFACE,               /*  1:bDescriptor */
    0,                              /*  2:bInterfaceNumber */
    0,                              /*  3:bAlternateSetting */
    1,                              /*  4:bNumEndpoints */
    USB_IFCLS_CDCC,                 /*  5:bInterfaceClass */
    USB_PCDC_CLASS_SUBCLASS_CODE_ABS_CTR_MDL,   /*  6:bInterfaceSubClass */
    1,                              /*  7:bInterfaceProtocol */
    0,                              /*  8:iInterface */

        /* Communications Class Functional Descriptorss */
        5, /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_HEADER_FUNC,    /*  2:bDescriptorSubtype */
        USB_PCDC_BCD_CDC % USB_PCDC_BCD_CDC_MASK,     /*  3:bcdCDC_lo */
        USB_PCDC_BCD_CDC / USB_PCDC_BCD_CDC_MASK,     /*  4:bcdCDC_hi */

        /* Communications Class Functional Descriptorss */
        4,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_ABSTRACT_CTR_MANAGE_FUNC,   /*  2:bDescriptorSubtype */
        2,                          /*  3:bmCapabilities */

        /* Communications Class Functional Descriptorss */
        5,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_UNION_FUNC, /*  2:bDescriptorSubtype */
        0,                          /*  3:bMasterInterface */
        1,                          /*  4:bSlaveInterface0 */

        /* Communications Class Functional Descriptorss */
        5,                          /*  0:bLength */
        USB_PCDC_CS_INTERFACE,      /*  1:bDescriptorType */
        USB_PCDC_DT_SUBTYPE_CALL_MANAGE_FUNC,   /*  2:bDescriptorSubtype */
        /* D1:1-Device can send/receive call management
         information over a Data Class interface. */
        /* D0:1-Device handles call management itself. */
        3,                          /*  3:bmCapabilities */
        1,                          /*  4:bDataInterface */

        /* Endpoint Descriptor 0 */
        7,                          /*  0:bLength */
        USB_DT_ENDPOINT,            /*  1:bDescriptorType */
        USB_EP_IN | USB_EP3,        /*  2:bEndpointAddress */
        USB_EP_INT,                 /*  3:bmAttribute */
        16,                         /*  4:wMAXPacketSize_lo */
        0,                          /*  5:wMAXPacketSize_hi */
        0x10,                       /*  6:bInterval */

    /* Interface Descriptor */
    9,                              /*  0:bLength */
    USB_DT_INTERFACE,               /*  1:bDescriptor */
    1,                              /*  2:bInterfaceNumber */
    0,                              /*  3:bAlternateSetting */
    2,                              /*  4:bNumEndpoints */
    USB_IFCLS_CDCD,                 /*  5:bInterfaceClass */
    0,                              /*  6:bInterfaceSubClass */
    0,                              /*  7:bInterfaceProtocol */
    0,                              /*  8:iInterface */

        /* Endpoint Descriptor 0 */
        7,                          /*  0:bLength */
        USB_DT_ENDPOINT,            /*  1:bDescriptorType */
        USB_EP_IN | USB_EP1,        /*  2:bEndpointAddress */
        USB_EP_BULK,                /*  3:bmAttribute */
        0,                          /*  4:wMAXPacketSize_lo */
        2,                          /*  5:wMAXPacketSize_hi */
        0,                          /*  6:bInterval */

        /* Endpoint Descriptor 1 */
        7,                          /*  0:bLength */
        USB_DT_ENDPOINT,            /*  1:bDescriptorType */
        USB_EP_OUT | USB_EP2,       /*  2:bEndpointAddress */
        USB_EP_BULK,                /*  3:bmAttribute */
        0,                          /*  4:wMAXPacketSize_lo */
        2,                          /*  5:wMAXPacketSize_hi */
        0,                          /*  6:bInterval */
};

/*************************************
 *    String Descriptor              *
 *************************************/
/* UNICODE 0x0409 English (United States) */
uint8_t g_cdc_string_descriptor0[STRING_DESCRIPTOR0_LEN + ( STRING_DESCRIPTOR0_LEN % 2)] =
{
    STRING_DESCRIPTOR0_LEN,     /*  0:bLength */
    USB_DT_STRING,              /*  1:bDescriptorType */
    0x09, 0x04                  /*  2:wLANGID[0] */
};

/* iManufacturer */
uint8_t g_cdc_string_descriptor1[STRING_DESCRIPTOR1_LEN + ( STRING_DESCRIPTOR1_LEN % 2)] =
{
    STRING_DESCRIPTOR1_LEN,     /*  0:bLength */
    USB_DT_STRING,              /*  1:bDescriptorType */
    'R', 0x00,                  /*  2:wLANGID[0] */
    'E', 0x00,
    'N', 0x00,
    'E', 0x00,
    'S', 0x00,
    'A', 0x00,
    'S', 0x00,
};

/* iProduct */
uint8_t g_cdc_string_descriptor2[STRING_DESCRIPTOR2_LEN + ( STRING_DESCRIPTOR2_LEN % 2)] =
{
    STRING_DESCRIPTOR2_LEN, /*  0:bLength */
    USB_DT_STRING,          /*  1:bDescriptorType */
    'C', 0x00,
    'D', 0x00,
    'C', 0x00,
    ' ', 0x00,
    'U', 0x00,
    'S', 0x00,
    'B', 0x00,
    ' ', 0x00,
    'D', 0x00,
    'e', 0x00,
    'm', 0x00,
    'o', 0x00,
    'n', 0x00,
    's', 0x00,
    't', 0x00,
    'r', 0x00,
    'a', 0x00,
    't', 0x00,
    'i', 0x00,
    'o', 0x00,
    'n', 0x00,
};

/* iInterface */
uint8_t g_cdc_string_descriptor3[STRING_DESCRIPTOR3_LEN + ( STRING_DESCRIPTOR3_LEN % 2)] =
{
    STRING_DESCRIPTOR3_LEN, /*  0:bLength */
    USB_DT_STRING,          /*  1:bDescriptorType */
    'C', 0x00,
    'o', 0x00,
    'm', 0x00,
    'm', 0x00,
    'u', 0x00,
    'n', 0x00,
    'i', 0x00,
    'c', 0x00,
    'a', 0x00,
    't', 0x00,
    'i', 0x00,
    'o', 0x00,
    'n', 0x00,
    's', 0x00,
    ' ', 0x00,
    'D', 0x00,
    'e', 0x00,
    'v', 0x00,
    'i', 0x00,
    'c', 0x00,
    'e', 0x00,
    's', 0x00
};

/* iConfiguration */
uint8_t g_cdc_string_descriptor4[STRING_DESCRIPTOR4_LEN + ( STRING_DESCRIPTOR4_LEN % 2)] =
{
    STRING_DESCRIPTOR4_LEN, /*  0:bLength */
    USB_DT_STRING,          /*  1:bDescriptorType */
    'F', 0x00,              /*  2:wLANGID[0] */
    'u', 0x00,
    'l', 0x00,
    'l', 0x00,
    '-', 0x00,
    'S', 0x00,
    'p', 0x00,
    'e', 0x00,
    'e', 0x00,
    'd', 0x00
};

/* iConfiguration */
uint8_t g_cdc_string_descriptor5[STRING_DESCRIPTOR5_LEN + ( STRING_DESCRIPTOR5_LEN % 2)] =
{
    STRING_DESCRIPTOR5_LEN, /*  0:bLength */
    USB_DT_STRING,          /*  1:bDescriptorType */
    'H', 0x00,              /*  2:wLANGID[0] */
    'i', 0x00,
    '-', 0x00,
    'S', 0x00,
    'p', 0x00,
    'e', 0x00,
    'e', 0x00,
    'd', 0x00
};

/* iSerialNumber */
uint8_t g_cdc_string_descriptor6[STRING_DESCRIPTOR6_LEN + ( STRING_DESCRIPTOR6_LEN % 2)] =
{
    STRING_DESCRIPTOR6_LEN, /*  0:bLength */
    USB_DT_STRING,          /*  1:bDescriptorType */
    '0', 0x00,              /*  2:wLANGID[0] */
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '0', 0x00,
    '1', 0x00,
};

uint8_t *g_apl_string_table[] =
{
    g_cdc_string_descriptor0,
    g_cdc_string_descriptor1,
    g_cdc_string_descriptor2,
    g_cdc_string_descriptor3,
    g_cdc_string_descriptor4,
    g_cdc_string_descriptor5,
    g_cdc_string_descriptor6
};

/******************************************************************************
 Renesas Abstracted Peripheral Communications Devices Class Driver API functions
 ******************************************************************************/

/******************************************************************************
 End  Of File
 ******************************************************************************/

Could you please help find out where is the problem for the descriptor failure? Also, how can I test the USB features on the device? Is there a way to send some string from Windows side or from the device side?

Thanks!