RA6M4 - FSP 4.2.0 - AZURE OS - TX_TIMER_TICKS_PER_SECOND to 1000

Hi,
I need to put my timer scheduler to 1ms
So I declared in my project option TX_TIMER_TICKS_PER_SECOND=1000
It's ok.


But wich value do I put for Netx ?

NX_IP_PERIODIC_RATE
NX_IP_FAST_TIMER_RATE

NX_TCP_FAST_TIMER_RATE
NX_TCP_ACK_TIMER_RATE

Because my timing tcp retry is now to 100ms instead of 1000ms

I tried this values, but my BSD socket never send "SYN" now :

Any idea ?

Best regards,

Phil