Azure Netx Duo Telnet Client stops receiving packages

Hello,

Currently I use the EK-RA6M3 board with the Azure RTOS ThreadX and Azure RTOS NetX Duo Telnet Client to connect with an Telnet Server and to receive messages from it. 

This works, but after 6 messages (sent with an interval of 1 sec.), the Client doesn't seems to receive any new messages any more.

I checked the server side and I'am pretty sure that it is still sending messages to the client. Also when I connect with laptop+RealTerm instead of the EK-RA6M3 board, I received messages without any interuption or what ever...

My first thoughts were a buffer or queue what is getting full and it doesn't take any message any more but I tried many "increase-size" actions of buffers, but without any success...

I'm really have no idea what the issue is, and I hope someone could point me in a direction to search..

I use the E2 studio with the FSP v3.8.0 package configurator. 

If more information is needed, please let me know!

Thanks for any comments in advance!

BR,

Frank

Parents Reply Children
No Data