Hi,
i want to use the virtual eeprom on a RA2E1. In principal this mechanism is working and i can write and read the record IDs. During production of the board i want to be able to program the initial content of this rec id. Is there any documentation or example how to build the binary file of the memory address starting from 0x40100000.
Thanks Michael
Then the .bin file should program the data flash with data that can be used from VEEPROM drivers (segment header, initial record, reference data).
The way of programming the data flash would be the same…
If you decide to use the reference data to keep that unique value, you just need to program the reference data. It should go into the last bytes of your data flash. For reference, see code from RM_VEE_…
You can download it from the Downloads tab on https://www.renesas.com/us/en/software-tool/renesas-flash-programmer-programming-gui?downloads-title-filter=wind#download