Hello. I have the Ek_RA6M3G card. I am trying to do project with APPwizard with it. I am following the instructions to the sample file and to create the project. I did it all. I'm stuck on 2 issues.
1. Problem: I can't exclude 2 files in the project from compilation. It is different from the example project. Images are attached.
This is what happens when I do as above.
This is what happens in the sample project.
I am applying the one in figure 49 in the r11an0463eu0200-fsp-graphics-app document, it gives an error.
The project is attached. I would be glad if you could check and help.
Have a nice day.Endoskopi_Screen.rar
Hello,
Thanks for posting your question online. Here is a suggested solution:
1) Right click on 'AppWizard' folder, go to Properties and uncheck the following option:
2) Then try to exclude from build the selected subfolders.
Hope it helps.
Regards