EK-RA6M3G DOCUMENT

Hello. I have the Ek_RA6M3G card. I am trying to do project with APPwizard with it. I am following the instructions to the sample file and to create the project. I did it all. I'm stuck on 2 issues.

1. Problem: I can't exclude 2 files in the project from compilation. It is different from the example project. Images are attached.

This is what happens when I do as above.

This is what happens in the sample project.

I am applying the one in figure 49 in the r11an0463eu0200-fsp-graphics-app document, it gives an error.

The project is attached. I would be glad if you could check and help.

Have a nice day.Endoskopi_Screen.rar

Parents Reply Children
No Data