Bug in FSP 4.4.0

I have noticed some undefined behavior in my code running FSP 4.4.0 and may have found a bug.
I am writing code to interface a SRAM to read and write floats. While testing my code, I noticed that the loop conditions in my 'for' loop were being reset causing the software to be stuck in that loop but I am not modifying the loop conditions anywhere. Here is loop where 'k' will reset to 0 after completing the function 'spi_readf'.

for (int k = 0; k < dwt_samples; k++)

{

spi_readf(address_datax, &buffer2, 1);

axis_data.xAxis_g = buffer2;

spi_readf(address_datay, &buffer2, 1);

axis_data.yAxis_g = buffer2;

spi_readf(address_dataz, &buffer2, 1);

axis_data.zAxis_g = buffer2;

address_datax[2]++;

address_datay[2]++;

address_dataz[2]++;

ftoa(axis_data.xAxis_g, xAxis, 2); ftoa(axis_data.yAxis_g, yAxis, 2); ftoa(axis_data.zAxis_g, zAxis, 2);

//write data to uart

status = write_uart("R RAW: x-axis: "); status = write_uart(xAxis);

status = write_uart("\ty-axis: "); status = write_uart(yAxis);

status = write_uart("\tz-axis: "); status = write_uart(zAxis);

status = write_uart("\t(m/s^2)\n");

}



fsp_err_t spi_readf(uint8_t* address, uint32_t* output, uint16_t size)

{

status = R_IOPORT_PinWrite(&g_ioport_ctrl, BSP_IO_PORT_01_PIN_03, BSP_IO_LEVEL_LOW);

uint8_t buffer[4] = {read_cmd, address[0], address[1], address[2]};

uint8_t buffer2[dwt_samples * 4] = {0};

uint32_t buff[dwt_samples] = {0};

status = R_SPI_WriteRead(&g_spi0_ctrl, buffer, (float*)0x00, 4, SPI_BIT_WIDTH_8_BITS);

if (FSP_SUCCESS != status)

{

deinit_spi();

return status;

}

status = spi_event_wait(SPI_EVENT_TRANSFER_COMPLETE);

if (FSP_SUCCESS != status)

{

deinit_spi();

return status;

}

status = R_SPI_WriteRead(&g_spi0_ctrl, (float*)0x00, buffer2, (size * 4), SPI_BIT_WIDTH_8_BITS);

if (FSP_SUCCESS != status)

{

deinit_spi();

return status;

}

status = spi_event_wait(SPI_EVENT_TRANSFER_COMPLETE);

if (FSP_SUCCESS != status)

{

deinit_spi();

return status;

}

*************resetting of loop condition is caused by this loop.******************

for (l = 0; l < dwt_samples * 4; l += 4)                   

{

buff[l / 4] = ((buffer2[l] << 24)) | ((buffer2[l + 1] << 16)) | ((buffer2[l + 2] << 8)) | buffer2[l + 3];

memcpy(&output[l/4], &buff[l/4], 4);

}

status = R_IOPORT_PinWrite(&g_ioport_ctrl, BSP_IO_PORT_01_PIN_03, BSP_IO_LEVEL_HIGH);

return status;

}


Parents Reply
  • Hello,

    Apologies for the delay!

    After checking your project and launching a debug session in FSP version 4.4.0, it seems that you should change on Project Properties-> C/C++ Build-> Settings--> Optimization to Optimize for debug (-Og).

    And it seems that the value of variable i is getting incremented without being reset.

    Regards,

    IK

Children
No Data