Ethernet RA6M3 Transmit request fail.

Hi,

Controller : RA6M3

PART NO: R7FA6M3AF3CFP

PHY: LAN8710A

 I referred the "r20an0560eu0121-ek-ra6m3-exampleprojects” this example code and I checked with “EK-RA6M3 evaluation board its working fine. I am able to ping.

Same configaration I did in custom board. I that I am getting Transmit request fail. I refer the ra6m3 datasheet there they mentioned " The EDTRR register controls EDMAC transmission. After the EDMAC transmits one frame, it reads the next descriptor. When the TD0.TACT bit in the descriptor is 1, the EDMAC continues transmission. When the TD0.TACT bit is 0, the EDMAC sets the TR bit to 0 and stops transmission." In my case the TR bit always 1. what might be the issue and how to resolve the same.

thanks,

Parents Reply Children
  • Hi,

    please check the attached configuration.xml file.

    <?xml version="1.0" encoding="UTF-8" standalone="no"?>
    <raConfiguration version="6">
      <generalSettings>
        <option key="#Board#" value="board.custom"/>
        <option key="CPU" value="RA6M3"/>
        <option key="#TargetName#" value="R7FA6M3AF3CFP"/>
        <option key="#TargetARCHITECTURE#" value="cortex-m4"/>
        <option key="#DeviceCommand#" value="R7FA6M3AF"/>
        <option key="#RTOS#" value="rtos.awsfreertos"/>
        <option key="#pinconfiguration#" value="RA6M3-EK.pincfg"/>
        <option key="#FSPVersion#" value="3.2.0"/>
        <option key="#DefaultLinkerScript#" value="ra6m3.ld"/>
        <option key="#ConfigurationFragments#" value="Renesas##BSP##Board##ra6m3_ek##"/>
        <option key="#SELECTED_TOOLCHAIN#" value="gcc-arm-embedded"/>
      </generalSettings>
      <raBspConfiguration>
        <config id="config.bsp.ra6m3.R7FA6M3AF3CFP">
          <property id="config.bsp.part_number" value="config.bsp.part_number.value"/>
          <property id="config.bsp.rom_size_bytes" value="config.bsp.rom_size_bytes.value"/>
          <property id="config.bsp.rom_size_bytes_hidden" value="1048576"/>
          <property id="config.bsp.ram_size_bytes" value="config.bsp.ram_size_bytes.value"/>
          <property id="config.bsp.data_flash_size_bytes" value="config.bsp.data_flash_size_bytes.value"/>
          <property id="config.bsp.package_style" value="config.bsp.package_style.value"/>
          <property id="config.bsp.package_pins" value="config.bsp.package_pins.value"/>
        </config>
        <config id="config.bsp.ra6m3">
          <property id="config.bsp.series" value="config.bsp.series.value"/>
        </config>
        <config id="config.bsp.ra6m3.fsp">
          <property id="config.bsp.fsp.OFS0.iwdt_start_mode" value="config.bsp.fsp.OFS0.iwdt_start_mode.disabled"/>
          <property id="config.bsp.fsp.OFS0.iwdt_timeout" value="config.bsp.fsp.OFS0.iwdt_timeout.2048"/>
          <property id="config.bsp.fsp.OFS0.iwdt_divisor" value="config.bsp.fsp.OFS0.iwdt_divisor.128"/>
          <property id="config.bsp.fsp.OFS0.iwdt_window_end" value="config.bsp.fsp.OFS0.iwdt_window_end.0"/>
          <property id="config.bsp.fsp.OFS0.iwdt_window_start" value="config.bsp.fsp.OFS0.iwdt_window_start.100"/>
          <property id="config.bsp.fsp.OFS0.iwdt_reset_interrupt" value="config.bsp.fsp.OFS0.iwdt_reset_interrupt.Reset"/>
          <property id="config.bsp.fsp.OFS0.iwdt_stop_control" value="config.bsp.fsp.OFS0.iwdt_stop_control.stops"/>
          <property id="config.bsp.fsp.OFS0.wdt_start_mode" value="config.bsp.fsp.OFS0.wdt_start_mode.register"/>
          <property id="config.bsp.fsp.OFS0.wdt_timeout" value="config.bsp.fsp.OFS0.wdt_timeout.16384"/>
          <property id="config.bsp.fsp.OFS0.wdt_divisor" value="config.bsp.fsp.OFS0.wdt_divisor.128"/>
          <property id="config.bsp.fsp.OFS0.wdt_window_end" value="config.bsp.fsp.OFS0.wdt_window_end.0"/>
          <property id="config.bsp.fsp.OFS0.wdt_window_start" value="config.bsp.fsp.OFS0.wdt_window_start.100"/>
          <property id="config.bsp.fsp.OFS0.wdt_reset_interrupt" value="config.bsp.fsp.OFS0.wdt_reset_interrupt.Reset"/>
          <property id="config.bsp.fsp.OFS0.wdt_stop_control" value="config.bsp.fsp.OFS0.wdt_stop_control.stops"/>
          <property id="config.bsp.fsp.OFS1.voltage_detection0.start" value="config.bsp.fsp.OFS1.voltage_detection0.start.disabled"/>
          <property id="config.bsp.fsp.OFS1.voltage_detection0_level" value="config.bsp.fsp.OFS1.voltage_detection0_level.280"/>
          <property id="config.bsp.fsp.OFS1.hoco_osc" value="config.bsp.fsp.OFS1.hoco_osc.disabled"/>
          <property id="config.bsp.fsp.mpu_pc0_enable" value="config.bsp.fsp.mpu_pc0_enable.disabled"/>
          <property id="config.bsp.fsp.mpu_pc0_start" value="0xFFFFFFFC"/>
          <property id="config.bsp.fsp.mpu_pc0_end" value="0xFFFFFFFF"/>
          <property id="config.bsp.fsp.mpu_pc1_enable" value="config.bsp.fsp.mpu_pc1_enable.disabled"/>
          <property id="config.bsp.fsp.mpu_pc1_start" value="0xFFFFFFFC"/>
          <property id="config.bsp.fsp.mpu_pc1_end" value="0xFFFFFFFF"/>
          <property id="config.bsp.fsp.mpu_reg0_enable" value="config.bsp.fsp.mpu_reg0_enable.disabled"/>
          <property id="config.bsp.fsp.mpu_reg0_start" value="0x00FFFFFC"/>
          <property id="config.bsp.fsp.mpu_reg0_end" value="0x00FFFFFF"/>
          <property id="config.bsp.fsp.mpu_reg1_enable" value="config.bsp.fsp.mpu_reg1_enable.disabled"/>
          <property id="config.bsp.fsp.mpu_reg1_start" value="0x200FFFFC"/>
          <property id="config.bsp.fsp.mpu_reg1_end" value="0x200FFFFF"/>
          <property id="config.bsp.fsp.mpu_reg2_enable" value="config.bsp.fsp.mpu_reg2_enable.disabled"/>
          <property id="config.bsp.fsp.mpu_reg2_start" value="0x407FFFFC"/>
          <property id="config.bsp.fsp.mpu_reg2_end" value="0x407FFFFF"/>
          <property id="config.bsp.fsp.mpu_reg3_enable" value="config.bsp.fsp.mpu_reg3_enable.disabled"/>
          <property id="config.bsp.fsp.mpu_reg3_start" value="0x400DFFFC"/>
          <property id="config.bsp.fsp.mpu_reg3_end" value="0x400DFFFF"/>
          <property id="config.bsp.fsp.hoco_fll" value="config.bsp.fsp.hoco_fll.disabled"/>
          <property id="config.bsp.common.main_osc_wait" value="config.bsp.common.main_osc_wait.wait_8163"/>
          <property id="config.bsp.fsp.mcu.adc.max_freq_hz" value="60000000"/>
          <property id="config.bsp.fsp.mcu.sci_uart.max_baud" value="20000000"/>
          <property id="config.bsp.fsp.mcu.adc.sample_and_hold" value="1"/>
          <property id="config.bsp.fsp.mcu.sci_spi.max_bitrate" value="30000000"/>
          <property id="config.bsp.fsp.mcu.spi.max_bitrate" value="30000000"/>
          <property id="config.bsp.fsp.mcu.iic_master.rate.rate_fastplus" value="1"/>
          <property id="config.bsp.common.id_mode" value="config.bsp.common.id_mode.unlocked"/>
          <property id="config.bsp.common.id_code" value="FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF"/>
          <property id="config.bsp.common.id1" value=""/>
          <property id="config.bsp.common.id2" value=""/>
          <property id="config.bsp.common.id3" value=""/>
          <property id="config.bsp.common.id4" value=""/>
          <property id="config.bsp.common.id_fixed" value=""/>
        </config>
        <config id="config.bsp.ra">
          <property id="config.bsp.common.main" value="0x1000"/>
          <property id="config.bsp.common.heap" value="0x2000"/>
          <property id="config.bsp.common.vcc" value="3300"/>
          <property id="config.bsp.common.checking" value="config.bsp.common.checking.enabled"/>
          <property id="config.bsp.common.assert" value="config.bsp.common.assert.none"/>
          <property id="config.bsp.common.error_log" value="config.bsp.common.error_log.none"/>
          <property id="config.bsp.common.soft_reset" value="config.bsp.common.soft_reset.disabled"/>
          <property id="config.bsp.common.main_osc_populated" value="config.bsp.common.main_osc_populated.enabled"/>
          <property id="config.bsp.common.pfs_protect" value="config.bsp.common.pfs_protect.enabled"/>
          <property id="config.bsp.common.c_runtime_init" value="config.bsp.common.c_runtime_init.enabled"/>
          <property id="config.bsp.common.main_osc_clock_source" value="config.bsp.common.main_osc_clock_source.crystal"/>
          <property id="config.bsp.common.subclock_populated" value="config.bsp.common.subclock_populated.enabled"/>
          <property id="config.bsp.common.subclock_drive" value="config.bsp.common.subclock_drive.standard"/>
          <property id="config.bsp.common.subclock_stabilization_ms" value="1000"/>
        </config>
      </raBspConfiguration>
      <raClockConfiguration>
        <node id="board.clock.xtal.freq" mul="24000000" option="_edit"/>
        <node id="board.clock.usbmclk.freq" option="board.clock.usbmclk.freq"/>
        <node id="board.clock.pll.source" option="board.clock.pll.source.hoco"/>
        <node id="board.clock.hoco.freq" option="board.clock.hoco.freq.20m"/>
        <node id="board.clock.loco.freq" option="board.clock.loco.freq.32768"/>
        <node id="board.clock.moco.freq" option="board.clock.moco.freq.8m"/>
        <node id="board.clock.subclk.freq" option="board.clock.subclk.freq.32768"/>
        <node id="board.clock.pll.div" option="board.clock.pll.div.2"/>
        <node id="board.clock.pll.mul" option="board.clock.pll.mul.240"/>
        <node id="board.clock.pll.display" option="board.clock.pll.display.value"/>
        <node id="board.clock.clock.source" option="board.clock.clock.source.pll"/>
        <node id="board.clock.iclk.div" option="board.clock.iclk.div.2"/>
        <node id="board.clock.iclk.display" option="board.clock.iclk.display.value"/>
        <node id="board.clock.pclka.div" option="board.clock.pclka.div.2"/>
        <node id="board.clock.pclka.display" option="board.clock.pclka.display.value"/>
        <node id="board.clock.pclkb.div" option="board.clock.pclkb.div.4"/>
        <node id="board.clock.pclkb.display" option="board.clock.pclkb.display.value"/>
        <node id="board.clock.pclkc.div" option="board.clock.pclkc.div.4"/>
        <node id="board.clock.pclkc.display" option="board.clock.pclkc.display.value"/>
        <node id="board.clock.pclkd.div" option="board.clock.pclkd.div.2"/>
        <node id="board.clock.pclkd.display" option="board.clock.pclkd.display.value"/>
        <node id="board.clock.sdclkout.div" option="board.clock.sdclkout.div.1"/>
        <node id="board.clock.sdclkout.display" option="board.clock.sdclkout.display.value"/>
        <node id="board.clock.bclk.div" option="board.clock.bclk.div.2"/>
        <node id="board.clock.bclk.display" option="board.clock.bclk.display.value"/>
        <node id="board.clock.bclkout.div" option="board.clock.bclkout.div.2"/>
        <node id="board.clock.bclkout.display" option="board.clock.bclkout.display.value"/>
        <node id="board.clock.uclk.div" option="board.clock.uclk.div.5"/>
        <node id="board.clock.uclk.display" option="board.clock.uclk.display.value"/>
        <node id="board.clock.fclk.div" option="board.clock.fclk.div.4"/>
        <node id="board.clock.fclk.display" option="board.clock.fclk.display.value"/>
        <node id="board.clock.clkout.source" option="board.clock.clkout.source.disabled"/>
        <node id="board.clock.clkout.div" option="board.clock.clkout.div.1"/>
        <node id="board.clock.clkout.display" option="board.clock.clkout.display.value"/>
      </raClockConfiguration>
      <raComponentSelection>
        <component apiversion="" class="RTOS" condition="" group="FreeRTOS" subgroup="all" variant="" vendor="AWS" version="10.4.3+fsp.3.2.0">
          <description>FreeRTOS</description>
          <originalPack>Amazon.FreeRTOS-Kernel.10.4.3+fsp.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="Heaps" condition="" group="FreeRTOS" subgroup="heap_4" variant="" vendor="AWS" version="10.4.3+fsp.3.2.0">
          <description>FreeRTOS - Memory Management - Heap 4</description>
          <originalPack>Amazon.FreeRTOS-Kernel.10.4.3+fsp.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="Libraries" condition="" group="FreeRTOS" subgroup="BufferAllocation2" variant="" vendor="AWS" version="2.3.2+fsp.3.2.0">
          <description>FreeRTOS - Buffer Allocation 2</description>
          <originalPack>Amazon.FreeRTOS-Plus-TCP.2.3.2+fsp.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="Libraries" condition="" group="FreeRTOS_Plus" subgroup="FreeRTOS_Plus_TCP" variant="" vendor="AWS" version="2.3.2+fsp.3.2.0">
          <description>FreeRTOS+TCP</description>
          <originalPack>Amazon.FreeRTOS-Plus-TCP.2.3.2+fsp.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="BSP" condition="" group="ra6m3" subgroup="device" variant="" vendor="Renesas" version="3.2.0">
          <description>Board support package for RA6M3</description>
          <originalPack>Renesas.RA_mcu_ra6m3.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="BSP" condition="" group="ra6m3" subgroup="fsp" variant="" vendor="Renesas" version="3.2.0">
          <description>Board support package for RA6M3 - FSP Data</description>
          <originalPack>Renesas.RA_mcu_ra6m3.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="Common" condition="" group="all" subgroup="fsp_common" variant="" vendor="Renesas" version="3.2.0">
          <description>Board Support Package Common Files</description>
          <originalPack>Renesas.RA.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="HAL Drivers" condition="" group="all" subgroup="r_ether_phy" variant="" vendor="Renesas" version="3.2.0">
          <description>Ethernet PHY</description>
          <originalPack>Renesas.RA.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="HAL Drivers" condition="" group="all" subgroup="r_ether" variant="" vendor="Renesas" version="3.2.0">
          <description>Ethernet</description>
          <originalPack>Renesas.RA.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="HAL Drivers" condition="" group="all" subgroup="r_ioport" variant="" vendor="Renesas" version="3.2.0">
          <description>I/O Port</description>
          <originalPack>Renesas.RA.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="Middleware" condition="" group="all" subgroup="rm_freertos_plus_tcp" variant="" vendor="Renesas" version="3.2.0">
          <description>r_ether to FreeRTOS+TCP Wrapper</description>
          <originalPack>Renesas.RA.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="CMSIS" condition="" group="CMSIS5" subgroup="CoreM" variant="" vendor="Arm" version="5.7.0+fsp.3.2.0">
          <description>Arm CMSIS Version 5 - Core (M)</description>
          <originalPack>Arm.CMSIS5.5.7.0+fsp.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="BSP" condition="" group="ra6m3" subgroup="device" variant="R7FA6M3AF3CFP" vendor="Renesas" version="3.2.0">
          <description>Board support package for R7FA6M3AF3CFP</description>
          <originalPack>Renesas.RA_mcu_ra6m3.3.2.0.pack</originalPack>
        </component>
        <component apiversion="" class="BSP" condition="" group="Board" subgroup="custom" variant="" vendor="Renesas" version="3.2.0">
          <description>Custom Board Support Files</description>
          <originalPack>Renesas.RA_board_custom.3.2.0.pack</originalPack>
        </component>
      </raComponentSelection>
      <raElcConfiguration/>
      <raIcuConfiguration/>
      <raModuleConfiguration>
        <module id="module.driver.ioport_on_ioport.0">
          <property id="module.driver.ioport.name" value="g_ioport"/>
          <property id="module.driver.ioport.elc_trigger_ioport1" value="_disabled"/>
          <property id="module.driver.ioport.elc_trigger_ioport2" value="_disabled"/>
          <property id="module.driver.ioport.elc_trigger_ioport3" value="_disabled"/>
          <property id="module.driver.ioport.elc_trigger_ioport4" value="_disabled"/>
          <property id="module.driver.ioport.pincfg" value="g_bsp_pin_cfg"/>
        </module>
        <module id="module.aws.freertosplus.freertosplus_tcp.1566011718"/>
        <module id="module.driver.freertos_plus_tcp_on_ether.1322876274"/>
        <module id="module.driver.ether_on_ether.1983497079">
          <property id="module.driver.ether.name" value="g_ether0"/>
          <property id="module.driver.ether.channel" value="module.driver.ether.channel.0"/>
          <property id="module.driver.ether.mac_address" value="00:11:22:33:44:55"/>
          <property id="module.driver.ether.zerocopy" value="module.driver.ether.zerocopy.0"/>
          <property id="module.driver.ether.flow_control" value="module.driver.ether.flow_control.1"/>
          <property id="module.driver.ether.multicast" value="module.driver.ether.multicast.1"/>
          <property id="module.driver.ether.promiscuous" value="module.driver.ether.promiscuous.0"/>
          <property id="module.driver.ether.broadcast_filter" value="0"/>
          <property id="module.driver.ether.num_tx_descriptors" value="4"/>
          <property id="module.driver.ether.num_rx_descriptors" value="4"/>
          <property id="module.driver.ether.allocate_rx_buffer" value="module.driver.ether.allocate_rx_buffer.1"/>
          <property id="module.driver.ether.ether_buffer_size" value="1514"/>
          <property id="module.driver.ether.padding" value="module.driver.ether.padding.0"/>
          <property id="module.driver.ether.padding_offset" value="0"/>
          <property id="module.driver.ether.interrupt_priority" value="board.icu.common.irq.priority12"/>
          <property id="module.driver.ether.p_callback" value="NULL"/>
        </module>
        <module id="module.driver.ether_phy_on_ether_phy.2071613776">
          <property id="module.driver.ether_phy.name" value="g_ether_phy0"/>
          <property id="module.driver.ether_phy.channel" value="module.driver.ether_phy.channel.0"/>
          <property id="module.driver.ether_phy.phy_lsi_address" value="0"/>
          <property id="module.driver.ether_phy.phy_reset_wait_time" value="0x00020000"/>
          <property id="module.driver.ether_phy.mii_type" value="module.driver.mii_type.rmii"/>
          <property id="module.driver.ether_phy.mii_bit_access_wait_time" value="8"/>
          <property id="module.driver.ether_phy.flow_control" value="module.driver.ether_phy.flow_control.0"/>
        </module>
        <module id="module.freertos.bufferallocation2.630647168"/>
        <module id="module.freertos.heap.4.2131149949"/>
        <context id="_hal.0">
          <stack module="module.driver.ioport_on_ioport.0"/>
        </context>
        <context id="rtos.awsfreertos.thread.788129143">
          <property id="_symbol" value="net_thread"/>
          <property id="rtos.awsfreertos.thread.name" value="Net Thread"/>
          <property id="rtos.awsfreertos.thread.stack" value="4096"/>
          <property id="rtos.awsfreertos.thread.priority" value="2"/>
          <property id="rtos.awsfreertos.thread.context" value="NULL"/>
          <property id="rtos.awsfreertos.thread.allocation" value="rtos.awsfreertos.thread.allocation.static"/>
          <property id="rtos.awsfreertos.thread.secure_context" value="rtos.awsfreertos.thread.secure_context.enable"/>
          <stack module="module.aws.freertosplus.freertosplus_tcp.1566011718">
            <stack module="module.driver.freertos_plus_tcp_on_ether.1322876274" requires="module.aws.freertosplus.freertosplus_tcp.requires.freertosplus_tcp_driver">
              <stack module="module.driver.ether_on_ether.1983497079" requires="module.driver.freertos_plus_tcp_on_ether.requires.ether">
                <stack module="module.driver.ether_phy_on_ether_phy.2071613776" requires="module.driver.ether.requires.ether_phy"/>
              </stack>
              <stack module="module.freertos.bufferallocation2.630647168" requires="module.driver.freertos_plus_tcp_on_ether.requires.bufferallocation2"/>
            </stack>
          </stack>
          <stack module="module.freertos.heap.4.2131149949"/>
        </context>
        <config id="config.driver.ioport">
          <property id="config.driver.ioport.checking" value="config.driver.ioport.checking.system"/>
        </config>
        <config id="config.driver.ether">
          <property id="config.driver.ether.param_checking_enable" value="config.driver.ether.param_checking_enable.bsp"/>
          <property id="config.driver.ether.link_present" value="config.driver.ether.link_present.0"/>
          <property id="config.driver.ether.use_linksta" value="config.driver.ether.use_linksta.0"/>
        </config>
        <config id="config.awsfreertos.thread">
          <property id="config.awsfreertos.custom_freertosconfig" value=""/>
          <property id="config.awsfreertos.thread.configuse_preemption" value="config.awsfreertos.thread.configuse_preemption.enabled"/>
          <property id="config.awsfreertos.thread.configuse_port_optimised_task_selection" value="config.awsfreertos.thread.configuse_port_optimised_task_selection.disabled"/>
          <property id="config.awsfreertos.thread.configuse_tickless_idle" value="config.awsfreertos.thread.configuse_tickless_idle.disabled"/>
          <property id="config.awsfreertos.thread.configuse_idle_hook" value="config.awsfreertos.thread.configuse_idle_hook.disabled"/>
          <property id="config.awsfreertos.thread.configuse_malloc_failed_hook" value="config.awsfreertos.thread.configuse_malloc_failed_hook.disabled"/>
          <property id="config.awsfreertos.thread.configuse_daemon_task_startup_hook" value="config.awsfreertos.thread.configuse_daemon_task_startup_hook.disabled"/>
          <property id="config.awsfreertos.thread.configuse_tick_hook" value="config.awsfreertos.thread.configuse_tick_hook.disabled"/>
          <property id="config.awsfreertos.thread.configcpu_clock_hz" value="SystemCoreClock"/>
          <property id="config.awsfreertos.thread.configtick_rate_hz" value="100"/>
          <property id="config.awsfreertos.thread.configmax_priorities" value="5"/>
          <property id="config.awsfreertos.thread.configminimal_stack_size" value="512"/>
          <property id="config.awsfreertos.thread.configmax_task_name_len" value="16"/>
          <property id="config.awsfreertos.thread.configuse_trace_facility" value="config.awsfreertos.thread.configuse_trace_facility.disabled"/>
          <property id="config.awsfreertos.thread.configuse_stats_formatting_functions" value="config.awsfreertos.thread.configuse_stats_formatting_functions.disabled"/>
          <property id="config.awsfreertos.thread.configuse_16_bit_ticks" value="config.awsfreertos.thread.configuse_16_bit_ticks.disabled"/>
          <property id="config.awsfreertos.thread.configidle_should_yield" value="config.awsfreertos.thread.configidle_should_yield.disabled"/>
          <property id="config.awsfreertos.thread.configuse_task_notifications" value="config.awsfreertos.thread.configuse_task_notifications.enabled"/>
          <property id="config.awsfreertos.thread.configuse_mutexes" value="config.awsfreertos.thread.configuse_mutexes.disabled"/>
          <property id="config.awsfreertos.thread.configuse_recursive_mutexes" value="config.awsfreertos.thread.configuse_recursive_mutexes.disabled"/>
          <property id="config.awsfreertos.thread.configuse_counting_semaphores" value="config.awsfreertos.thread.configuse_counting_semaphores.enabled"/>
          <property id="config.awsfreertos.thread.configcheck_for_stack_overflow" value="config.awsfreertos.thread.configcheck_for_stack_overflow.disabled"/>
          <property id="config.awsfreertos.thread.configqueue_registry_size" value="10"/>
          <property id="config.awsfreertos.thread.configuse_queue_sets" value="config.awsfreertos.thread.configuse_queue_sets.disabled"/>
          <property id="config.awsfreertos.thread.configuse_time_slicing" value="config.awsfreertos.thread.configuse_time_slicing.disabled"/>
          <property id="config.awsfreertos.thread.configuse_newlib_reentrant" value="config.awsfreertos.thread.configuse_newlib_reentrant.disabled"/>
          <property id="config.awsfreertos.thread.configenable_backward_compatibility" value="config.awsfreertos.thread.configenable_backward_compatibility.disabled"/>
          <property id="config.awsfreertos.thread.confignum_thread_local_storage_pointers" value="5"/>
          <property id="config.awsfreertos.thread.configstack_depth_type" value="uint32_t"/>
          <property id="config.awsfreertos.thread.configmessage_buffer_length_type" value="size_t"/>
          <property id="config.awsfreertos.thread.configsupport_static_allocation" value="config.awsfreertos.thread.configsupport_static_allocation.enabled"/>
          <property id="config.awsfreertos.thread.configsupport_dynamic_allocation" value="config.awsfreertos.thread.configsupport_dynamic_allocation.enabled"/>
          <property id="config.awsfreertos.thread.configtotal_heap_size" value="0x8000"/>
          <property id="config.awsfreertos.thread.configapplication_allocated_heap" value="config.awsfreertos.thread.configapplication_allocated_heap.disabled"/>
          <property id="config.awsfreertos.thread.configgenerate_run_time_stats" value="config.awsfreertos.thread.configgenerate_run_time_stats.disabled"/>
          <property id="config.awsfreertos.thread.configuse_timers" value="config.awsfreertos.thread.configuse_timers.enabled"/>
          <property id="config.awsfreertos.thread.configtimer_task_priority" value="3"/>
          <property id="config.awsfreertos.thread.configtimer_queue_length" value="10"/>
          <property id="config.awsfreertos.thread.configtimer_task_stack_depth" value="128"/>
          <property id="config.awsfreertos.thread.configlibrary_max_syscall_interrupt_priority" value="board.icu.common.irq.priority1"/>
          <property id="config.awsfreertos.thread.configassert" value="assert ( x )"/>
          <property id="config.awsfreertos.thread.configinclude_application_defined_privileged_functions" value="config.awsfreertos.thread.configinclude_application_defined_privileged_functions.disabled"/>
          <property id="config.awsfreertos.thread.include_vtaskpriorityset" value="config.awsfreertos.thread.include_vtaskpriorityset.enabled"/>
          <property id="config.awsfreertos.thread.include_uxtaskpriorityget" value="config.awsfreertos.thread.include_uxtaskpriorityget.enabled"/>
          <property id="config.awsfreertos.thread.include_vtaskdelete" value="config.awsfreertos.thread.include_vtaskdelete.enabled"/>
          <property id="config.awsfreertos.thread.include_vtasksuspend" value="config.awsfreertos.thread.include_vtasksuspend.enabled"/>
          <property id="config.awsfreertos.thread.include_xresumefromisr" value="config.awsfreertos.thread.include_xresumefromisr.enabled"/>
          <property id="config.awsfreertos.thread.include_vtaskdelayuntil" value="config.awsfreertos.thread.include_vtaskdelayuntil.enabled"/>
          <property id="config.awsfreertos.thread.include_vtaskdelay" value="config.awsfreertos.thread.include_vtaskdelay.enabled"/>
          <property id="config.awsfreertos.thread.include_xtaskgetschedulerstate" value="config.awsfreertos.thread.include_xtaskgetschedulerstate.enabled"/>
          <property id="config.awsfreertos.thread.include_xtaskgetcurrenttaskhandle" value="config.awsfreertos.thread.include_xtaskgetcurrenttaskhandle.enabled"/>
          <property id="config.awsfreertos.thread.include_uxtaskgetstackhighwatermark" value="config.awsfreertos.thread.include_uxtaskgetstackhighwatermark.disabled"/>
          <property id="config.awsfreertos.thread.include_xtaskgetidletaskhandle" value="config.awsfreertos.thread.include_xtaskgetidletaskhandle.disabled"/>
          <property id="config.awsfreertos.thread.include_etaskgetstate" value="config.awsfreertos.thread.include_etaskgetstate.disabled"/>
          <property id="config.awsfreertos.thread.include_xeventgroupsetbitfromisr" value="config.awsfreertos.thread.include_xeventgroupsetbitfromisr.enabled"/>
          <property id="config.awsfreertos.thread.include_xtimerpendfunctioncall" value="config.awsfreertos.thread.include_xtimerpendfunctioncall.disabled"/>
          <property id="config.awsfreertos.thread.include_xtaskabortdelay" value="config.awsfreertos.thread.include_xtaskabortdelay.disabled"/>
          <property id="config.awsfreertos.thread.include_xtaskgethandle" value="config.awsfreertos.thread.include_xtaskgethandle.disabled"/>
          <property id="config.awsfreertos.thread.include_xtaskresumefromisr" value="config.awsfreertos.thread.include_xtaskresumefromisr.enabled"/>
          <property id="config.awsfreertos.thread.include_hw_stack_monitor" value="config.awsfreertos.thread.include_hw_stack_monitor.disabled"/>
          <property id="config.awsfreertos.thread.print_function" value="printf(x)"/>
          <property id="config.awsfreertos.thread.max_length" value="192"/>
          <property id="config.awsfreertos.thread.include_time_and_task" value="config.awsfreertos.thread.include_time_and_task.disabled"/>
        </config>
        <config id="config.driver.ether_phy">
          <property id="config.driver.ether_phy.param_checking_enable" value="config.driver.ether_phy.param_checking_enable.bsp"/>
          <property id="config.driver.ether_phy.use_phy" value="config.driver.ether_phy.use_phy.other"/>
          <property id="config.driver.ether_phy.use_reference_clock" value="config.driver.ether_phy.use_reference_clock.enabled"/>
        </config>
        <config id="config.aws.freertosplus.freertosplus_tcp">
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigHAS_DEBUG_PRINTF" value="config.aws.freertosplus.freertosplus_tcp.ipconfigHAS_DEBUG_PRINTF.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigHAS_PRINTF" value="config.aws.freertosplus.freertosplus_tcp.ipconfigHAS_PRINTF.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigBYTE_ORDER" value="config.aws.freertosplus.freertosplus_tcp.ipconfigBYTE_ORDER.pdFREERTOS_LITTLE_ENDIAN"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigDRIVER_INCLUDED_RX_IP_CHECKSUM" value="config.aws.freertosplus.freertosplus_tcp.ipconfigDRIVER_INCLUDED_RX_IP_CHECKSUM.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigSOCK_DEFAULT_RECEIVE_BLOCK_TIME" value="2000"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigSOCK_DEFAULT_SEND_BLOCK_TIME" value="2000"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DNS_CACHE" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DNS_CACHE.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigDNS_REQUEST_ATTEMPTS" value="5"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigIP_TASK_PRIORITY" value="configMAX_PRIORITIES - 1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigIP_TASK_STACK_SIZE_WORDS" value="configMINIMAL_STACK_SIZE * 10"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_NETWORK_EVENT_HOOK" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_NETWORK_EVENT_HOOK.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUDP_MAX_SEND_BLOCK_TIME_TICKS" value="15000 / portTICK_PERIOD_MS"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DHCP" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DHCP.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigDHCP_REGISTER_HOSTNAME" value="config.aws.freertosplus.freertosplus_tcp.ipconfigDHCP_REGISTER_HOSTNAME.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigDHCP_USES_UNICAST" value="config.aws.freertosplus.freertosplus_tcp.ipconfigDHCP_USES_UNICAST.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigDHCP_SEND_DISCOVER_AFTER_AUTO_IP" value="config.aws.freertosplus.freertosplus_tcp.ipconfigDHCP_SEND_DISCOVER_AFTER_AUTO_IP.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DHCP_HOOK" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DHCP_HOOK.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigMAXIMUM_DISCOVER_TX_PERIOD" value="120000 / portTICK_PERIOD_MS"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigARP_CACHE_ENTRIES" value="6"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigMAX_ARP_RETRANSMISSIONS" value="5"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigMAX_ARP_AGE" value="150"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigINCLUDE_FULL_INET_ADDR" value="config.aws.freertosplus.freertosplus_tcp.ipconfigINCLUDE_FULL_INET_ADDR.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigNUM_NETWORK_BUFFER_DESCRIPTORS" value="16"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigEVENT_QUEUE_LENGTH" value="ipconfigNUM_NETWORK_BUFFER_DESCRIPTORS + 5"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigALLOW_SOCKET_SEND_WITHOUT_BIND" value="config.aws.freertosplus.freertosplus_tcp.ipconfigALLOW_SOCKET_SEND_WITHOUT_BIND.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUDP_TIME_TO_LIVE" value="128"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_TIME_TO_LIVE" value="128"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_TCP" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_TCP.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_TCP_WIN" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_TCP_WIN.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigNETWORK_MTU" value="1500"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DNS" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_DNS.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigREPLY_TO_INCOMING_PINGS" value="config.aws.freertosplus.freertosplus_tcp.ipconfigREPLY_TO_INCOMING_PINGS.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigSUPPORT_OUTGOING_PINGS" value="config.aws.freertosplus.freertosplus_tcp.ipconfigSUPPORT_OUTGOING_PINGS.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigSUPPORT_SELECT_FUNCTION" value="config.aws.freertosplus.freertosplus_tcp.ipconfigSUPPORT_SELECT_FUNCTION.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigFILTER_OUT_NON_ETHERNET_II_FRAMES" value="config.aws.freertosplus.freertosplus_tcp.ipconfigFILTER_OUT_NON_ETHERNET_II_FRAMES.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigETHERNET_DRIVER_FILTERS_FRAME_TYPES" value="config.aws.freertosplus.freertosplus_tcp.ipconfigETHERNET_DRIVER_FILTERS_FRAME_TYPES.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigIGNORE_UNKNOWN_PACKETS" value="config.aws.freertosplus.freertosplus_tcp.ipconfigIGNORE_UNKNOWN_PACKETS.1"/>
          <property id="configWINDOWS_MAC_INTERRUPT_SIMULATOR_DELAY" value="20 / portTICK_PERIOD_MS"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigPACKET_FILLER_SIZE" value="2"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_WIN_SEG_COUNT" value="240"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_RX_BUFFER_LENGTH" value="3000"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_TX_BUFFER_LENGTH" value="3000"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_KEEP_ALIVE" value="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_KEEP_ALIVE.1"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigTCP_KEEP_ALIVE_INTERVAL" value="120"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigSOCKET_HAS_USER_SEMAPHORE" value="config.aws.freertosplus.freertosplus_tcp.ipconfigSOCKET_HAS_USER_SEMAPHORE.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigSOCKET_HAS_USER_WAKE_CALLBACK" value="config.aws.freertosplus.freertosplus_tcp.ipconfigSOCKET_HAS_USER_WAKE_CALLBACK.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_CALLBACKS" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_CALLBACKS.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigZERO_COPY_TX_DRIVER" value="config.aws.freertosplus.freertosplus_tcp.ipconfigZERO_COPY_TX_DRIVER.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigZERO_COPY_RX_DRIVER" value="config.aws.freertosplus.freertosplus_tcp.ipconfigZERO_COPY_RX_DRIVER.0"/>
          <property id="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_LINKED_RX_MESSAGES" value="config.aws.freertosplus.freertosplus_tcp.ipconfigUSE_LINKED_RX_MESSAGES.0"/>
        </config>
      </raModuleConfiguration>
      <raPinConfiguration>
        <symbolicName propertyId="p400.symbolic_name" value="IRQ0"/>
        <pincfg active="true" name="RA6M3-EK.pincfg" selected="false" symbol="g_bsp_pin_cfg">
          <configSetting altId="adc0.an00.p000" configurationId="adc0.an00"/>
          <configSetting altId="adc0.an01.p001" configurationId="adc0.an01"/>
          <configSetting altId="adc0.an02.p002" configurationId="adc0.an02"/>
          <configSetting altId="adc0.an05.p014" configurationId="adc0.an05"/>
          <configSetting altId="adc0.an20.p508" configurationId="adc0.an20"/>
          <configSetting altId="adc0.mode.custom" configurationId="adc0.mode"/>
          <configSetting altId="adc1.mode.custom" configurationId="adc1.mode"/>
          <configSetting altId="cgc0.extal.p212" configurationId="cgc0.extal"/>
          <configSetting altId="cgc0.mode.mainsub" configurationId="cgc0.mode"/>
          <configSetting altId="cgc0.xtal.p213" configurationId="cgc0.xtal"/>
          <configSetting altId="debug0.mode.jtag" configurationId="debug0.mode"/>
          <configSetting altId="debug0.tck.p300" configurationId="debug0.tck"/>
          <configSetting altId="debug0.tdi.p110" configurationId="debug0.tdi"/>
          <configSetting altId="debug0.tdo.p109" configurationId="debug0.tdo"/>
          <configSetting altId="debug0.tms.p108" configurationId="debug0.tms"/>
          <configSetting altId="etherc0.rmii.crs_dv.p408" configurationId="etherc0.rmii.crs_dv"/>
          <configSetting altId="etherc0.rmii.mdc.p401" configurationId="etherc0.rmii.mdc"/>
          <configSetting altId="etherc0.rmii.mdio.p402" configurationId="etherc0.rmii.mdio"/>
          <configSetting altId="etherc0.rmii.mode.rmii.free" configurationId="etherc0.rmii.mode"/>
          <configSetting altId="etherc0.rmii.pairing.free" configurationId="etherc0.rmii.pairing"/>
          <configSetting altId="etherc0.rmii.ref50ck.p412" configurationId="etherc0.rmii.ref50ck"/>
          <configSetting altId="etherc0.rmii.rx_er.p409" configurationId="etherc0.rmii.rx_er"/>
          <configSetting altId="etherc0.rmii.rxd0.p411" configurationId="etherc0.rmii.rxd0"/>
          <configSetting altId="etherc0.rmii.rxd1.p410" configurationId="etherc0.rmii.rxd1"/>
          <configSetting altId="etherc0.rmii.txd0.p413" configurationId="etherc0.rmii.txd0"/>
          <configSetting altId="etherc0.rmii.txd1.p414" configurationId="etherc0.rmii.txd1"/>
          <configSetting altId="etherc0.rmii.txd_en.p415" configurationId="etherc0.rmii.txd_en"/>
          <configSetting altId="glcdc0.lcd_clk.p101" configurationId="glcdc0.lcd_clk"/>
          <configSetting altId="glcdc0.lcd_data00.p106" configurationId="glcdc0.lcd_data00"/>
          <configSetting altId="glcdc0.lcd_data01.p107" configurationId="glcdc0.lcd_data01"/>
          <configSetting altId="glcdc0.lcd_data02.p600" configurationId="glcdc0.lcd_data02"/>
          <configSetting altId="glcdc0.lcd_data03.p601" configurationId="glcdc0.lcd_data03"/>
          <configSetting altId="glcdc0.lcd_data04.p602" configurationId="glcdc0.lcd_data04"/>
          <configSetting altId="glcdc0.lcd_data05.p610" configurationId="glcdc0.lcd_data05"/>
          <configSetting altId="glcdc0.lcd_data06.p609" configurationId="glcdc0.lcd_data06"/>
          <configSetting altId="glcdc0.lcd_data07.p608" configurationId="glcdc0.lcd_data07"/>
          <configSetting altId="glcdc0.lcd_data08.p115" configurationId="glcdc0.lcd_data08"/>
          <configSetting altId="glcdc0.lcd_data09.p114" configurationId="glcdc0.lcd_data09"/>
          <configSetting altId="glcdc0.lcd_data10.p113" configurationId="glcdc0.lcd_data10"/>
          <configSetting altId="glcdc0.lcd_data11.p112" configurationId="glcdc0.lcd_data11"/>
          <configSetting altId="glcdc0.lcd_data12.p111" configurationId="glcdc0.lcd_data12"/>
          <configSetting altId="glcdc0.lcd_data13.p301" configurationId="glcdc0.lcd_data13"/>
          <configSetting altId="glcdc0.lcd_data14.p302" configurationId="glcdc0.lcd_data14"/>
          <configSetting altId="glcdc0.lcd_data15.p303" configurationId="glcdc0.lcd_data15"/>
          <configSetting altId="glcdc0.lcd_tcon0.p102" configurationId="glcdc0.lcd_tcon0"/>
          <configSetting altId="glcdc0.lcd_tcon1.p103" configurationId="glcdc0.lcd_tcon1"/>
          <configSetting altId="glcdc0.lcd_tcon2.p104" configurationId="glcdc0.lcd_tcon2"/>
          <configSetting altId="glcdc0.mode.custom.a" configurationId="glcdc0.mode"/>
          <configSetting altId="glcdc0.pairing.a" configurationId="glcdc0.pairing"/>
          <configSetting altId="gpt0.gtioca.p415" configurationId="gpt0.gtioca"/>
          <configSetting altId="gpt0.mode.gtiocaorgtiocb.free" configurationId="gpt0.mode"/>
          <configSetting altId="gpt7.mode.gtiocaorgtiocb.free" configurationId="gpt7.mode"/>
          <configSetting altId="irq0.irq09.p004" configurationId="irq0.irq09"/>
          <configSetting altId="irq0.irq11.p708" configurationId="irq0.irq11"/>
          <configSetting altId="irq0.irq12.p008" configurationId="irq0.irq12"/>
          <configSetting altId="irq0.mode.enabled" configurationId="irq0.mode"/>
          <configSetting altId="p000.adc0.an00" configurationId="p000"/>
          <configSetting altId="p000.gpio_mode.gpio_mode_an" configurationId="p000.gpio_mode"/>
          <configSetting altId="p001.adc0.an01" configurationId="p001"/>
          <configSetting altId="p001.gpio_mode.gpio_mode_an" configurationId="p001.gpio_mode"/>
          <configSetting altId="p002.adc0.an02" configurationId="p002"/>
          <configSetting altId="p002.gpio_mode.gpio_mode_an" configurationId="p002.gpio_mode"/>
          <configSetting altId="p004.irq0.irq09" configurationId="p004"/>
          <configSetting altId="p004.gpio_irq.gpio_irq_enabled" configurationId="p004.gpio_irq"/>
          <configSetting altId="p004.gpio_mode.gpio_mode_irq" configurationId="p004.gpio_mode"/>
          <configSetting altId="p008.irq0.irq12" configurationId="p008"/>
          <configSetting altId="p008.gpio_irq.gpio_irq_enabled" configurationId="p008.gpio_irq"/>
          <configSetting altId="p008.gpio_mode.gpio_mode_irq" configurationId="p008.gpio_mode"/>
          <configSetting altId="p014.adc0.an05" configurationId="p014"/>
          <configSetting altId="p014.gpio_mode.gpio_mode_an" configurationId="p014.gpio_mode"/>
          <configSetting altId="p100.output.low" configurationId="p100"/>
          <configSetting altId="p100.gpio_mode.gpio_mode_out.low" configurationId="p100.gpio_mode"/>
          <configSetting altId="p101.glcdc0.lcd_clk" configurationId="p101"/>
          <configSetting altId="p101.gpio_speed.gpio_speed_high" configurationId="p101.gpio_drivecapacity"/>
          <configSetting altId="p101.gpio_mode.gpio_mode_peripheral" configurationId="p101.gpio_mode"/>
          <configSetting altId="p102.glcdc0.lcd_tcon0" configurationId="p102"/>
          <configSetting altId="p102.gpio_speed.gpio_speed_high" configurationId="p102.gpio_drivecapacity"/>
          <configSetting altId="p102.gpio_mode.gpio_mode_peripheral" configurationId="p102.gpio_mode"/>
          <configSetting altId="p103.glcdc0.lcd_tcon1" configurationId="p103"/>
          <configSetting altId="p103.gpio_speed.gpio_speed_high" configurationId="p103.gpio_drivecapacity"/>
          <configSetting altId="p103.gpio_mode.gpio_mode_peripheral" configurationId="p103.gpio_mode"/>
          <configSetting altId="p104.glcdc0.lcd_tcon2" configurationId="p104"/>
          <configSetting altId="p104.gpio_speed.gpio_speed_high" configurationId="p104.gpio_drivecapacity"/>
          <configSetting altId="p104.gpio_mode.gpio_mode_peripheral" configurationId="p104.gpio_mode"/>
          <configSetting altId="p106.glcdc0.lcd_data00" configurationId="p106"/>
          <configSetting altId="p106.gpio_speed.gpio_speed_high" configurationId="p106.gpio_drivecapacity"/>
          <configSetting altId="p106.gpio_mode.gpio_mode_peripheral" configurationId="p106.gpio_mode"/>
          <configSetting altId="p107.glcdc0.lcd_data01" configurationId="p107"/>
          <configSetting altId="p107.gpio_speed.gpio_speed_high" configurationId="p107.gpio_drivecapacity"/>
          <configSetting altId="p107.gpio_mode.gpio_mode_peripheral" configurationId="p107.gpio_mode"/>
          <configSetting altId="p108.debug0.tms" configurationId="p108"/>
          <configSetting altId="p108.gpio_mode.gpio_mode_peripheral" configurationId="p108.gpio_mode"/>
          <configSetting altId="p109.debug0.tdo" configurationId="p109"/>
          <configSetting altId="p109.gpio_mode.gpio_mode_peripheral" configurationId="p109.gpio_mode"/>
          <configSetting altId="p110.debug0.tdi" configurationId="p110"/>
          <configSetting altId="p110.gpio_mode.gpio_mode_peripheral" configurationId="p110.gpio_mode"/>
          <configSetting altId="p111.glcdc0.lcd_data12" configurationId="p111"/>
          <configSetting altId="p111.gpio_speed.gpio_speed_high" configurationId="p111.gpio_drivecapacity"/>
          <configSetting altId="p111.gpio_mode.gpio_mode_peripheral" configurationId="p111.gpio_mode"/>
          <configSetting altId="p112.glcdc0.lcd_data11" configurationId="p112"/>
          <configSetting altId="p112.gpio_speed.gpio_speed_high" configurationId="p112.gpio_drivecapacity"/>
          <configSetting altId="p112.gpio_mode.gpio_mode_peripheral" configurationId="p112.gpio_mode"/>
          <configSetting altId="p113.glcdc0.lcd_data10" configurationId="p113"/>
          <configSetting altId="p113.gpio_speed.gpio_speed_high" configurationId="p113.gpio_drivecapacity"/>
          <configSetting altId="p113.gpio_mode.gpio_mode_peripheral" configurationId="p113.gpio_mode"/>
          <configSetting altId="p114.glcdc0.lcd_data09" configurationId="p114"/>
          <configSetting altId="p114.gpio_speed.gpio_speed_high" configurationId="p114.gpio_drivecapacity"/>
          <configSetting altId="p114.gpio_mode.gpio_mode_peripheral" configurationId="p114.gpio_mode"/>
          <configSetting altId="p115.glcdc0.lcd_data08" configurationId="p115"/>
          <configSetting altId="p115.gpio_speed.gpio_speed_high" configurationId="p115.gpio_drivecapacity"/>
          <configSetting altId="p115.gpio_mode.gpio_mode_peripheral" configurationId="p115.gpio_mode"/>
          <configSetting altId="p205.spi1.ssl0" configurationId="p205"/>
          <configSetting altId="p205.gpio_mode.gpio_mode_peripheral" configurationId="p205.gpio_mode"/>
          <configSetting altId="p206.input" configurationId="p206"/>
          <configSetting altId="p206.gpio_irq.gpio_irq_enabled" configurationId="p206.gpio_irq"/>
          <configSetting altId="p206.gpio_mode.gpio_mode_in" configurationId="p206.gpio_mode"/>
          <configSetting altId="p206.gpio_pupd.gpio_pupd_ip_up" configurationId="p206.gpio_pupd"/>
          <configSetting altId="p208.trace0.tdata3" configurationId="p208"/>
          <configSetting altId="p208.gpio_speed.gpio_speed_high" configurationId="p208.gpio_drivecapacity"/>
          <configSetting altId="p208.gpio_mode.gpio_mode_peripheral" configurationId="p208.gpio_mode"/>
          <configSetting altId="p209.trace0.tdata2" configurationId="p209"/>
          <configSetting altId="p209.gpio_speed.gpio_speed_high" configurationId="p209.gpio_drivecapacity"/>
          <configSetting altId="p209.gpio_mode.gpio_mode_peripheral" configurationId="p209.gpio_mode"/>
          <configSetting altId="p210.trace0.tdata1" configurationId="p210"/>
          <configSetting altId="p210.gpio_speed.gpio_speed_high" configurationId="p210.gpio_drivecapacity"/>
          <configSetting altId="p210.gpio_mode.gpio_mode_peripheral" configurationId="p210.gpio_mode"/>
          <configSetting altId="p211.trace0.tdata0" configurationId="p211"/>
          <configSetting altId="p211.gpio_speed.gpio_speed_high" configurationId="p211.gpio_drivecapacity"/>
          <configSetting altId="p211.gpio_mode.gpio_mode_peripheral" configurationId="p211.gpio_mode"/>
          <configSetting altId="p212.cgc0.extal" configurationId="p212"/>
          <configSetting altId="p212.gpio_mode.gpio_mode_peripheral" configurationId="p212.gpio_mode"/>
          <configSetting altId="p213.cgc0.xtal" configurationId="p213"/>
          <configSetting altId="p213.gpio_mode.gpio_mode_peripheral" configurationId="p213.gpio_mode"/>
          <configSetting altId="p214.trace0.tclk" configurationId="p214"/>
          <configSetting altId="p214.gpio_speed.gpio_speed_high" configurationId="p214.gpio_drivecapacity"/>
          <configSetting altId="p214.gpio_mode.gpio_mode_peripheral" configurationId="p214.gpio_mode"/>
          <configSetting altId="p300.debug0.tck" configurationId="p300"/>
          <configSetting altId="p300.gpio_mode.gpio_mode_peripheral" configurationId="p300.gpio_mode"/>
          <configSetting altId="p301.glcdc0.lcd_data13" configurationId="p301"/>
          <configSetting altId="p301.gpio_speed.gpio_speed_high" configurationId="p301.gpio_drivecapacity"/>
          <configSetting altId="p301.gpio_mode.gpio_mode_peripheral" configurationId="p301.gpio_mode"/>
          <configSetting altId="p302.glcdc0.lcd_data14" configurationId="p302"/>
          <configSetting altId="p302.gpio_speed.gpio_speed_high" configurationId="p302.gpio_drivecapacity"/>
          <configSetting altId="p302.gpio_mode.gpio_mode_peripheral" configurationId="p302.gpio_mode"/>
          <configSetting altId="p303.glcdc0.lcd_data15" configurationId="p303"/>
          <configSetting altId="p303.gpio_speed.gpio_speed_high" configurationId="p303.gpio_drivecapacity"/>
          <configSetting altId="p303.gpio_mode.gpio_mode_peripheral" configurationId="p303.gpio_mode"/>
          <configSetting altId="p304.output.high" configurationId="p304"/>
          <configSetting altId="p304.gpio_mode.gpio_mode_out.high" configurationId="p304.gpio_mode"/>
          <configSetting altId="p305.qspi0.qspclk" configurationId="p305"/>
          <configSetting altId="p305.gpio_speed.gpio_speed_high" configurationId="p305.gpio_drivecapacity"/>
          <configSetting altId="p305.gpio_mode.gpio_mode_peripheral" configurationId="p305.gpio_mode"/>
          <configSetting altId="p306.qspi0.qssl" configurationId="p306"/>
          <configSetting altId="p306.gpio_speed.gpio_speed_high" configurationId="p306.gpio_drivecapacity"/>
          <configSetting altId="p306.gpio_mode.gpio_mode_peripheral" configurationId="p306.gpio_mode"/>
          <configSetting altId="p307.qspi0.qio0" configurationId="p307"/>
          <configSetting altId="p307.gpio_speed.gpio_speed_high" configurationId="p307.gpio_drivecapacity"/>
          <configSetting altId="p307.gpio_mode.gpio_mode_peripheral" configurationId="p307.gpio_mode"/>
          <configSetting altId="p400.output.low" configurationId="p400"/>
          <configSetting altId="p400.gpio_mode.gpio_mode_out.low" configurationId="p400.gpio_mode"/>
          <configSetting altId="p401.etherc0.rmii.mdc" configurationId="p401"/>
          <configSetting altId="p401.gpio_speed.gpio_speed_high" configurationId="p401.gpio_drivecapacity"/>
          <configSetting altId="p401.gpio_mode.gpio_mode_peripheral" configurationId="p401.gpio_mode"/>
          <configSetting altId="p402.etherc0.rmii.mdio" configurationId="p402"/>
          <configSetting altId="p402.gpio_speed.gpio_speed_high" configurationId="p402.gpio_drivecapacity"/>
          <configSetting altId="p402.gpio_mode.gpio_mode_peripheral" configurationId="p402.gpio_mode"/>
          <configSetting altId="p403.output.low" configurationId="p403"/>
          <configSetting altId="p403.gpio_mode.gpio_mode_out.low" configurationId="p403.gpio_mode"/>
          <configSetting altId="p404.output.high" configurationId="p404"/>
          <configSetting altId="p404.gpio_mode.gpio_mode_out.high" configurationId="p404.gpio_mode"/>
          <configSetting altId="p407.usbfs0.vbus" configurationId="p407"/>
          <configSetting altId="p407.gpio_mode.gpio_mode_peripheral" configurationId="p407.gpio_mode"/>
          <configSetting altId="p408.sci3.scl" configurationId="p408"/>
          <configSetting altId="p408.gpio_mode.gpio_mode_peripheral" configurationId="p408.gpio_mode"/>
          <configSetting altId="p408.gpio_otype.gpio_otype_n_ch_od" configurationId="p408.gpio_otype"/>
          <configSetting altId="p409.sci3.sda" configurationId="p409"/>
          <configSetting altId="p409.gpio_mode.gpio_mode_peripheral" configurationId="p409.gpio_mode"/>
          <configSetting altId="p409.gpio_otype.gpio_otype_n_ch_od" configurationId="p409.gpio_otype"/>
          <configSetting altId="p410.spi0.miso" configurationId="p410"/>
          <configSetting altId="p410.gpio_mode.gpio_mode_peripheral" configurationId="p410.gpio_mode"/>
          <configSetting altId="p411.spi0.mosi" configurationId="p411"/>
          <configSetting altId="p411.gpio_mode.gpio_mode_peripheral" configurationId="p411.gpio_mode"/>
          <configSetting altId="p412.spi0.rspck" configurationId="p412"/>
          <configSetting altId="p412.gpio_mode.gpio_mode_peripheral" configurationId="p412.gpio_mode"/>
          <configSetting altId="p413.output.low" configurationId="p413"/>
          <configSetting altId="p413.gpio_mode.gpio_mode_out.low" configurationId="p413.gpio_mode"/>
          <configSetting altId="p414.spi0.ssl1" configurationId="p414"/>
          <configSetting altId="p414.gpio_mode.gpio_mode_peripheral" configurationId="p414.gpio_mode"/>
          <configSetting altId="p415.gpt0.gtioca" configurationId="p415"/>
          <configSetting altId="p415.gpio_mode.gpio_mode_peripheral" configurationId="p415.gpio_mode"/>
          <configSetting altId="p500.usbfs0.vbusen" configurationId="p500"/>
          <configSetting altId="p500.gpio_mode.gpio_mode_peripheral" configurationId="p500.gpio_mode"/>
          <configSetting altId="p501.usbfs0.ovrcura" configurationId="p501"/>
          <configSetting altId="p501.gpio_mode.gpio_mode_peripheral" configurationId="p501.gpio_mode"/>
          <configSetting altId="p503.output.low" configurationId="p503"/>
          <configSetting altId="p503.gpio_mode.gpio_mode_out.low" configurationId="p503.gpio_mode"/>
          <configSetting altId="p504.output.low" configurationId="p504"/>
          <configSetting altId="p504.gpio_mode.gpio_mode_out.low" configurationId="p504.gpio_mode"/>
          <configSetting altId="p508.adc0.an20" configurationId="p508"/>
          <configSetting altId="p508.gpio_mode.gpio_mode_an" configurationId="p508.gpio_mode"/>
          <configSetting altId="p600.glcdc0.lcd_data02" configurationId="p600"/>
          <configSetting altId="p600.gpio_speed.gpio_speed_high" configurationId="p600.gpio_drivecapacity"/>
          <configSetting altId="p600.gpio_mode.gpio_mode_peripheral" configurationId="p600.gpio_mode"/>
          <configSetting altId="p601.glcdc0.lcd_data03" configurationId="p601"/>
          <configSetting altId="p601.gpio_speed.gpio_speed_high" configurationId="p601.gpio_drivecapacity"/>
          <configSetting altId="p601.gpio_mode.gpio_mode_peripheral" configurationId="p601.gpio_mode"/>
          <configSetting altId="p602.glcdc0.lcd_data04" configurationId="p602"/>
          <configSetting altId="p602.gpio_speed.gpio_speed_high" configurationId="p602.gpio_drivecapacity"/>
          <configSetting altId="p602.gpio_mode.gpio_mode_peripheral" configurationId="p602.gpio_mode"/>
          <configSetting altId="p608.glcdc0.lcd_data07" configurationId="p608"/>
          <configSetting altId="p608.gpio_speed.gpio_speed_high" configurationId="p608.gpio_drivecapacity"/>
          <configSetting altId="p608.gpio_mode.gpio_mode_peripheral" configurationId="p608.gpio_mode"/>
          <configSetting altId="p609.glcdc0.lcd_data06" configurationId="p609"/>
          <configSetting altId="p609.gpio_speed.gpio_speed_high" configurationId="p609.gpio_drivecapacity"/>
          <configSetting altId="p609.gpio_mode.gpio_mode_peripheral" configurationId="p609.gpio_mode"/>
          <configSetting altId="p610.glcdc0.lcd_data05" configurationId="p610"/>
          <configSetting altId="p610.gpio_speed.gpio_speed_high" configurationId="p610.gpio_drivecapacity"/>
          <configSetting altId="p610.gpio_mode.gpio_mode_peripheral" configurationId="p610.gpio_mode"/>
          <configSetting altId="p708.irq0.irq11" configurationId="p708"/>
          <configSetting altId="p708.gpio_irq.gpio_irq_enabled" configurationId="p708.gpio_irq"/>
          <configSetting altId="p708.gpio_mode.gpio_mode_irq" configurationId="p708.gpio_mode"/>
          <configSetting altId="qspi0.qio0.p307" configurationId="qspi0.qio0"/>
          <configSetting altId="qspi0.qspclk.p305" configurationId="qspi0.qspclk"/>
          <configSetting altId="qspi0.qssl.p306" configurationId="qspi0.qssl"/>
          <configSetting altId="sci3.mode.iic.a" configurationId="sci3.mode"/>
          <configSetting altId="sci3.pairing.a" configurationId="sci3.pairing"/>
          <configSetting altId="sci3.scl.p408" configurationId="sci3.scl"/>
          <configSetting altId="sci3.sda.p409" configurationId="sci3.sda"/>
          <configSetting altId="sci8.pairing.a" configurationId="sci8.pairing"/>
          <configSetting altId="spi0.miso.p410" configurationId="spi0.miso"/>
          <configSetting altId="spi0.mode.enabled.free" configurationId="spi0.mode"/>
          <configSetting altId="spi0.mosi.p411" configurationId="spi0.mosi"/>
          <configSetting altId="spi0.pairing.free" configurationId="spi0.pairing"/>
          <configSetting altId="spi0.rspck.p412" configurationId="spi0.rspck"/>
          <configSetting altId="spi0.ssl1.p414" configurationId="spi0.ssl1"/>
          <configSetting altId="spi1.ssl0.p205" configurationId="spi1.ssl0"/>
          <configSetting altId="trace0.mode.trace4bit" configurationId="trace0.mode"/>
          <configSetting altId="trace0.tclk.p214" configurationId="trace0.tclk"/>
          <configSetting altId="trace0.tdata0.p211" configurationId="trace0.tdata0"/>
          <configSetting altId="trace0.tdata1.p210" configurationId="trace0.tdata1"/>
          <configSetting altId="trace0.tdata2.p209" configurationId="trace0.tdata2"/>
          <configSetting altId="trace0.tdata3.p208" configurationId="trace0.tdata3"/>
          <configSetting altId="usbfs0.mode.custom" configurationId="usbfs0.mode"/>
          <configSetting altId="usbfs0.ovrcura.p501" configurationId="usbfs0.ovrcura"/>
          <configSetting altId="usbfs0.vbus.p407" configurationId="usbfs0.vbus"/>
          <configSetting altId="usbfs0.vbusen.p500" configurationId="usbfs0.vbusen"/>
        </pincfg>
        <pincfg active="false" name="R7FA6M3AH3CFC.pincfg" selected="false" symbol="">
          <configSetting altId="debug0.mode.jtag" configurationId="debug0.mode"/>
          <configSetting altId="debug0.tck.p300" configurationId="debug0.tck"/>
          <configSetting altId="debug0.tdi.p110" configurationId="debug0.tdi"/>
          <configSetting altId="debug0.tdo.p109" configurationId="debug0.tdo"/>
          <configSetting altId="debug0.tms.p108" configurationId="debug0.tms"/>
          <configSetting altId="p108.debug0.tms" configurationId="p108"/>
          <configSetting altId="p108.gpio_mode.gpio_mode_peripheral" configurationId="p108.gpio_mode"/>
          <configSetting altId="p109.debug0.tdo" configurationId="p109"/>
          <configSetting altId="p109.gpio_mode.gpio_mode_peripheral" configurationId="p109.gpio_mode"/>
          <configSetting altId="p110.debug0.tdi" configurationId="p110"/>
          <configSetting altId="p110.gpio_mode.gpio_mode_peripheral" configurationId="p110.gpio_mode"/>
          <configSetting altId="p300.debug0.tck" configurationId="p300"/>
          <configSetting altId="p300.gpio_mode.gpio_mode_peripheral" configurationId="p300.gpio_mode"/>
        </pincfg>
        <pincfg active="false" name="R7FA6M3AF3CFP.pincfg" selected="true" symbol="">
          <configSetting altId="debug0.mode.jtag" configurationId="debug0.mode"/>
          <configSetting altId="debug0.tck.p300" configurationId="debug0.tck"/>
          <configSetting altId="debug0.tdi.p110" configurationId="debug0.tdi"/>
          <configSetting altId="debug0.tdo.p109" configurationId="debug0.tdo"/>
          <configSetting altId="debug0.tms.p108" configurationId="debug0.tms"/>
          <configSetting altId="etherc0.rmii.crs_dv.p408" configurationId="etherc0.rmii.crs_dv"/>
          <configSetting altId="etherc0.rmii.mdc.p401" configurationId="etherc0.rmii.mdc"/>
          <configSetting altId="etherc0.rmii.mdio.p402" configurationId="etherc0.rmii.mdio"/>
          <configSetting altId="etherc0.rmii.mode.rmii.free" configurationId="etherc0.rmii.mode"/>
          <configSetting altId="etherc0.rmii.pairing.free" configurationId="etherc0.rmii.pairing"/>
          <configSetting altId="etherc0.rmii.ref50ck.p412" configurationId="etherc0.rmii.ref50ck"/>
          <configSetting altId="etherc0.rmii.rx_er.p409" configurationId="etherc0.rmii.rx_er"/>
          <configSetting altId="etherc0.rmii.rxd0.p411" configurationId="etherc0.rmii.rxd0"/>
          <configSetting altId="etherc0.rmii.rxd1.p410" configurationId="etherc0.rmii.rxd1"/>
          <configSetting altId="etherc0.rmii.txd0.p413" configurationId="etherc0.rmii.txd0"/>
          <configSetting altId="etherc0.rmii.txd1.p406" configurationId="etherc0.rmii.txd1"/>
          <configSetting altId="etherc0.rmii.txd_en.p405" configurationId="etherc0.rmii.txd_en"/>
          <configSetting altId="p108.debug0.tms" configurationId="p108"/>
          <configSetting altId="p108.gpio_mode.gpio_mode_peripheral" configurationId="p108.gpio_mode"/>
          <configSetting altId="p109.debug0.tdo" configurationId="p109"/>
          <configSetting altId="p109.gpio_mode.gpio_mode_peripheral" configurationId="p109.gpio_mode"/>
          <configSetting altId="p110.debug0.tdi" configurationId="p110"/>
          <configSetting altId="p110.gpio_mode.gpio_mode_peripheral" configurationId="p110.gpio_mode"/>
          <configSetting altId="p300.debug0.tck" configurationId="p300"/>
          <configSetting altId="p300.gpio_mode.gpio_mode_peripheral" configurationId="p300.gpio_mode"/>
          <configSetting altId="p401.etherc0.rmii.mdc" configurationId="p401"/>
          <configSetting altId="p401.gpio_speed.gpio_speed_high" configurationId="p401.gpio_drivecapacity"/>
          <configSetting altId="p401.gpio_mode.gpio_mode_peripheral" configurationId="p401.gpio_mode"/>
          <configSetting altId="p402.etherc0.rmii.mdio" configurationId="p402"/>
          <configSetting altId="p402.gpio_speed.gpio_speed_high" configurationId="p402.gpio_drivecapacity"/>
          <configSetting altId="p402.gpio_mode.gpio_mode_peripheral" configurationId="p402.gpio_mode"/>
          <configSetting altId="p405.etherc0.rmii.txd_en" configurationId="p405"/>
          <configSetting altId="p405.gpio_speed.gpio_speed_high" configurationId="p405.gpio_drivecapacity"/>
          <configSetting altId="p405.gpio_mode.gpio_mode_peripheral" configurationId="p405.gpio_mode"/>
          <configSetting altId="p406.etherc0.rmii.txd1" configurationId="p406"/>
          <configSetting altId="p406.gpio_speed.gpio_speed_high" configurationId="p406.gpio_drivecapacity"/>
          <configSetting altId="p406.gpio_mode.gpio_mode_peripheral" configurationId="p406.gpio_mode"/>
          <configSetting altId="p408.etherc0.rmii.crs_dv" configurationId="p408"/>
          <configSetting altId="p408.gpio_speed.gpio_speed_high" configurationId="p408.gpio_drivecapacity"/>
          <configSetting altId="p408.gpio_mode.gpio_mode_peripheral" configurationId="p408.gpio_mode"/>
          <configSetting altId="p409.etherc0.rmii.rx_er" configurationId="p409"/>
          <configSetting altId="p409.gpio_speed.gpio_speed_high" configurationId="p409.gpio_drivecapacity"/>
          <configSetting altId="p409.gpio_mode.gpio_mode_peripheral" configurationId="p409.gpio_mode"/>
          <configSetting altId="p410.etherc0.rmii.rxd1" configurationId="p410"/>
          <configSetting altId="p410.gpio_speed.gpio_speed_high" configurationId="p410.gpio_drivecapacity"/>
          <configSetting altId="p410.gpio_mode.gpio_mode_peripheral" configurationId="p410.gpio_mode"/>
          <configSetting altId="p411.etherc0.rmii.rxd0" configurationId="p411"/>
          <configSetting altId="p411.gpio_speed.gpio_speed_high" configurationId="p411.gpio_drivecapacity"/>
          <configSetting altId="p411.gpio_mode.gpio_mode_peripheral" configurationId="p411.gpio_mode"/>
          <configSetting altId="p412.etherc0.rmii.ref50ck" configurationId="p412"/>
          <configSetting altId="p412.gpio_speed.gpio_speed_high" configurationId="p412.gpio_drivecapacity"/>
          <configSetting altId="p412.gpio_mode.gpio_mode_peripheral" configurationId="p412.gpio_mode"/>
          <configSetting altId="p413.etherc0.rmii.txd0" configurationId="p413"/>
          <configSetting altId="p413.gpio_speed.gpio_speed_high" configurationId="p413.gpio_drivecapacity"/>
          <configSetting altId="p413.gpio_mode.gpio_mode_peripheral" configurationId="p413.gpio_mode"/>
        </pincfg>
      </raPinConfiguration>
    </raConfiguration>
    

    thanks

    Tukaram

  • Hello Tukaram,

    Thank you for sharing with me your configuration.xml it seems that you have chosen RMII mode.

    What are the connections you have done on the PHY chip?

    Have you also tried to put an oscilloscope to check the clock frequency provided to the PHY?

    When calling FreeRTOS_IPInit() function what is the return value you get?

    Regards,

    IK

  • Hi IK,

    1. Schimatic for the ethernet PHY (LAN8710A)
    2. Yes checked clock its 50MHz
    3. When calling FreeRTOS_IPInit() function the return value is= 1(pdTRUE)
  • Hello,

    Apologies for my delayed response.

    Please check this app note provided here. It provides the design guidelines, when using the RA MCU with RMII modes for Ethernet specific applications.

    https://www.renesas.com/us/en/document/apn/ra-ethernet-design-and-custom-phy-setup-using-fsp

    Hope it helps.

    Regards,

    IK

  • Hi IK,

    Thanks for your response, I referred to that document and made the changes still I have transmission request fail issue.

    Regards

    Tukaram 

  • Hi IK,

    Do you have RA6M3 ethernet MAC loop back test sample code, please send me MAC loopback test document or source code.

    Thanks

    Tukaram

  • Hello,

    Thank you for your feedback! Please let me inform you that we have received the same request from you on our internal ticketing system and you will get support there.

    Thank you!

    Best Regards,

    IK

  • Hi IK,

    Thanks for your response, in that ticket I added source code. please suggest what might be the issue.

    Thanks 

    Tukaram

  • Hi IK,

    Still I am not able to get the response for the ping and receive issue. ticket number: 379336

    thanks

    tukaram

  • Hello Tukaram,

    Apologies for any delay! Please check the ticket I have provided to you an answer and a sample project.

    But also let me provide the answer and here:

    Please find here attached a sample application on EK-RA6M3, the required modification for the loopback for during the initialization can be food from the macro

    "ETHER_PHY_LOCAL_DIGITAL_LOOP_BACK".

    fsp_ethernet_loopback_test_ra6m3.zip

    Hope this helps!

    Best Regards,

    IK