Hi,
i have the need to monitor a lot a CAN IDs. Is this possible with the can Stack of the FSP Configuration.
I have the need to check the can message regardless which CAN Identifier is used. Therefore I can not assign a CAN ID to the mailboxes.
Thanks Michael
Hello,
Do you want a mailbox to 'listen' to multiple CAN IDs ?
yes i want a mailbox to "listen" to multiple CAN IDs
You can set a group mask to allow all CAN IDs:
If all bits are '1' then the mailbox can listen only to one ID (fully masked).
If all or some bits are '0' then the mailbox can listen to multiple IDs depending on the mask.
The above option sets the MKR registers: