Hello,
I am using EK-RA2E1 board with device R7FA2E1A92DFM.
I am trying to boot the application using UART and xmodem.
I have set the baudrate at 115200 bps at both the (primary and secondary) applications (usng swap upgrade mode) and teraterm is connected at 115200 bps. (see the images below).
Attaching the clock settings below too.
But I see weird characters printed on TeraTerm (see image below).
I tried the same with 9600 bps too but same output.
Thank You.
Thanks for reaching out Renesas Engineering Community!
Have you tried to put a logic analyzer in TX pin of the MCU to check if the messages are transmitted with no garbage?
Also could you please share with us some code to check how you print these messages to Tera Term?
Best Regards,
IK
Hi,
This is the menu to be printed on Teraterm :
Hello again,
Please let me inform you that I did not receive any .zip file in private. Also this comms_send function seems to call the Write API of UART. Would it be possible to share also the body of this function?
Regards,
Hi, I am not able to send mesage. Can you send me a ping so that i can send you the zip file?
Thank You
Hello Keniz,
According to the application note here:
https://www.renesas.com/us/en/document/apn/ra6-secure-firmware-update-using-mcuboot-and-flash-dual-bank-application-project
And the example projects for Firmware update through UART for RA6M4:
https://github.com/renesas/ra-fsp-examples/tree/master/application_projects/r11an0570/example_projects_with_bootloader
I have created for you an example for EK-RA2L1 to take it as reference.
In the .zip folder I will attach for you it is included the bootloader project using swap upgrade mode as you would like to use and 2 application projects.
The one is the app_primary_uart_ra2l1 including also a downloader thread to perform firmware update through a USB to UART and by using XMODEM via Tera Term.
As soon as I open the Tera Term I connect to serial port and make the settings according to my UART setting in the app_primary_uart_ra2l1 project.
And then run the project. I see these messages printed on Tera Term.
If I press 1 in the provided menu I see image slot information.
Then I press 2 to transfer my file through XMODEM:
I choose the bin.signed file of my app_secondary_uart_ra2l1 project:
And I can see the file being tranfered:
As soon is completed I see a message saying that we should wait while the system is resetting
And the as soon as the reset is done I can see again the same menu being displayed but now from app_secondary_uart_ra2l1 project image loaded in my board.
And if I press 1 again to display the image slot info, I get:
I read now the swapped memory layout.
MCUBOOT_UART_XMODEM_RA2L1.zip
Hope this project will help you proceed.
Thank you!
Thank You !