Hello
I want to design a boot application for my MCU RA6 controller.
I can generate project and build it correctly the boot project, but when i build the primary project it's built OK but then
when generates the signed file it cannot generate it and i have some error messages. These are the messages:
15:51:48 **** Boot Image Build of configuration Debug for project app_ra6m3_primary ****python "C:\\Proyectos\\MCUboot_Encrypted_Initial_Projects\\ra_mcuboot_ra6m3_swap_testmode/ra/fsp/src/rm_mcuboot_port/rm_mcuboot_port_sign.py" sign --header-size 0x200 --align 128 --max-align 128 --slot-size 0x20000 --max-sectors 4 --pad --pad-header app_ra6m3_primary.elf app_ra6m3_primary.bin.signed C:\Proyectos\MCUboot_Encrypted_Initial_Projects\ra_mcuboot_ra6m3_swap_testmode\ra\fsp\src\rm_mcuboot_port\rm_mcuboot_port_sign.py:19: DeprecationWarning: pkg_resources is deprecated as an API. See setuptools.pypa.io/.../pkg_resources.html import pkg_resourcesTraceback (most recent call last):ERROR: Required python packages are missing. Run the following command to install: File "C:\Proyectos\MCUboot_Encrypted_Initial_Projects\ra_mcuboot_ra6m3_swap_testmode\ra\fsp\src\rm_mcuboot_port\rm_mcuboot_port_sign.py", line 20, in <module>pip install -r ra/mcu-tools/MCUboot/scripts/requirements.txt pkg_resources.require(mcuboot_requirements) File "C:\Users\TL\.local\lib\python3.10-mingw_x86_64\site-packages\pkg_resources\__init__.py", line 968, in require needed = self.resolve(parse_requirements(requirements)) File "C:\Users\TL\.local\lib\python3.10-mingw_x86_64\site-packages\pkg_resources\__init__.py", line 829, in resolve dist = self._resolve_dist( File "C:\Users\TL\.local\lib\python3.10-mingw_x86_64\site-packages\pkg_resources\__init__.py", line 870, in _resolve_dist raise DistributionNotFound(req, requirers)pkg_resources.DistributionNotFound: The 'cbor2' distribution was not found and is required by the application15:51:49 Build finished
Can you please help me to resolve this problem? it seems that some python resources are outdated.
Thanks and best regards.
Luis Svensson