Failing to Erase RA6M1

Hello!

I currently face a problem, in which I'm unable to flash my EK-RA6M1. Im currently trying to develop a USBFS-interface but cant really test my code, since flashing is not possible. What I try to do is erasing my Device via the j-Link Commander V7.94. When using the Erase command i get the following Error:

Type "connect" to establish a target connection, '?' for help
J-Link>connect
Please specify device / core. <Default>: R7FA6M1AD
Type '?' for selection dialog
Device>
Please specify target interface:
  J) JTAG (Default)
  S) SWD
  T) cJTAG
TIF>S
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "R7FA6M1AD" selected.


Connecting to target via SWD
InitTarget() start
Identifying target device...
SWD selected. Executing JTAG -> SWD switching sequence...
Initializing DAP...
DAP initialized successfully.
Low power mode detected. Waking device from low power mode.
InitTarget() end - Took 10.8ms
Found SW-DP with ID 0x5BA02477
DPIDR: 0x5BA02477
CoreSight SoC-400 or earlier
Scanning AP map to find all available APs
AP[2]: Stopped AP scan as end of AP map has been reached
AP[0]: AHB-AP (IDR: 0x24770011)
AP[1]: APB-AP (IDR: 0x44770002)
Iterating through AP map to find AHB-AP to use
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
[0][5]: E0041000 CID B105900D PID 000BB925 ETM
[0][6]: E0042000 CID B105900D PID 002BB908 CSTF
[0][7]: E0043000 CID B105900D PID 001BB961 TMC
[0][8]: E0044000 CID B105F00D PID 001BB101 TSG
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M4 identified.
J-Link>erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset & halt of MCU.
Reset: Halt core after reset via DEMCR.VC_CORERESET.
Reset: Reset device via AIRCR.SYSRESETREQ.
Erasing device...
J-Link: Flash download: Only internal flash banks will be erased.
To enable erasing of other flash banks like QSPI or CFI, it needs to be enabled via "exec EnableEraseAllFlashBanks"

****** Error: Failed to erase sectors 0 @ address 0x0100A150 ((erase error))
Failed to erase sectors.

J-Link: Flash download: Total time needed: 0.211s (Prepare: 0.151s, Compare: 0.000s, Erase: 0.016s, Program: 0.000s, Verify: 0.000s, Restore: 0.043s)
ERROR: Erase returned with error code -5.

Parents
  • Hello,

    I have a similar issue on my MCK-RA6T2. I used a sample project "Sensorless vector control for dual permanent magnetic synchronous motor (For MCK/MCB, RA Family)" as base for my code and then made some adjustments trying to implement an UART-Interface, using the default debug-configuration for the project. After a while, i encountered the same problem as in post "Failed to erase sectors 0 @ address 0x00000000 ((erase error)) of RA6M1 - Forum - RA MCU - Renesas Engineering Community". I followed the steps with the J-Link Commander V7.94 like Dansen and got the following error:

     

    Type "connect" to establish a target connection, '?' for help
    J-Link>connect
    Please specify device / core. <Default>: R7FA6T2BD
    Type '?' for selection dialog
    Device>
    Please specify target interface:
      J) JTAG (Default)
      S) SWD
      T) cJTAG
    TIF>S
    Specify target interface speed [kHz]. <Default>: 4000 kHz
    Speed>
    Device "R7FA6T2BD" selected.
    Connecting to target via SWD
    ConfigTargetSettings() start
    Configuring FlashDLNoRMWThreshold=0x200 in order to make sure that option bytes programming is done via read-modify-write
    ConfigTargetSettings() end - Took 419us
    InitTarget() start
    SWD selected. Executing JTAG -> SWD switching sequence.
    DAP initialized successfully.
    Determining TrustZone configuration...
      Secure Debug: Enabled (SSD)
    Determining currently configured transfer type by reading the AHB-AP CSW register.
      --> Correct transfer type configured. Done.
    InitTarget() end - Took 7.82ms
    Found SW-DP with ID 0x6BA02477
    DPIDR: 0x6BA02477
    CoreSight SoC-400 or earlier
    Scanning AP map to find all available APs
    AP[2]: Stopped AP scan as end of AP map has been reached
    AP[0]: AHB-AP (IDR: 0x84770001)
    AP[1]: APB-AP (IDR: 0x54770002)
    Iterating through AP map to find AHB-AP to use
    AP[0]: Core found
    AP[0]: AHB-AP ROM base: 0xE00FE000
    CPUID register: 0x410FD214. Implementer code: 0x41 (ARM)
    Feature set: Mainline
    Cache: No cache
    Found Cortex-M33 r0p4, Little endian.
    FPUnit: 8 code (BP) slots and 0 literal slots
    Security extension: implemented
    Secure debug: enabled
    CoreSight components:
    ROMTbl[0] @ E00FE000
    [0][0]: E0044000 CID B105900D PID 005BB906 DEVARCH 00000000 DEVTYPE 14 CTI (?)
    [0][1]: E0047000 CID B105900D PID 003BB908 DEVARCH 00000000 DEVTYPE 12 CSTF
    [0][2]: E0048000 CID B105900D PID 001BB961 DEVARCH 00000000 DEVTYPE 21 ETB
    [0][3]: E0049000 CID B105F00D PID 001BB101 TSG
    [0][4]: E0040000 CID B105900D PID 000BBD21 DEVARCH 00000000 DEVTYPE 11 TPIU
    [0][5]: E00FF000 CID B105100D PID 000BB4C9 ROM Table
    ROMTbl[1] @ E00FF000
    [1][0]: E000E000 CID B105900D PID 000BBD21 DEVARCH 47702A04 DEVTYPE 00 Cortex-M33
    [1][1]: E0001000 CID B105900D PID 000BBD21 DEVARCH 47701A02 DEVTYPE 00 DWT
    [1][2]: E0002000 CID B105900D PID 000BBD21 DEVARCH 47701A03 DEVTYPE 00 FPB
    [1][3]: E0000000 CID B105900D PID 000BBD21 DEVARCH 47701A01 DEVTYPE 43 ITM
    [1][5]: E0041000 CID B105900D PID 002BBD21 DEVARCH 47724A13 DEVTYPE 13 ETM
    [1][6]: E0042000 CID B105900D PID 000BBD21 DEVARCH 47701A14 DEVTYPE 14 CSS600-CTI
    Memory zones:
      Zone: "Default" Description: Default access mode
    Cortex-M33 identified.
    J-Link>erase
    No address range specified, 'Erase Chip' will be executed
    'erase': Performing implicit reset & halt of MCU.
    Reset: ARMv8M core with Security Extension enabled detected.
    Reset: Halt core after reset via DEMCR.VC_CORERESET.
    Reset: Reset device via AIRCR.SYSRESETREQ.
    Erasing device...
    CPU is running at low speed (2079 kHz).
    J-Link: Flash download: Total time needed: 0.254s (Prepare: 0.221s, Compare: 0.000s, Erase: 0.032s, Program: 0.000s, Verify: 0.000s, Restore: 0.000s)
    
    ****** Error: Failed to erase sectors.
    
    ERROR: Erase returned with error code -5.

    I encountered the same issues as described in "Failed to erase sectors 0 @ address 0x00000000 ((erase error)) of RA6M1 - Forum - RA MCU - Renesas Engineering Community". 

    In e2-Studio i get teh following log:

    GDB Server for Renesas targets.
    	Version 9.1.0.v20230405-115727 [dd3207d3] (Apr  6 2023 16:06:04)
    
    
    Starting server with the following options: 
            Raw options                : C:\Users\mzerl\.eclipse\com.renesas.platform_1435879475\DebugComp\\RA\e2-server-gdb -g SEGGERJLINKARM -t R7FA6T2BD -uConnectionTimeout= 30 -uSelect= USB -uJLinkSetting= C:\Users\mzerl\e2_studio\workspace\pucMoc/pucMoc Debug_Flat.jlink -uJLinkLog= C:\Users\mzerl\e2_studio\workspace\pucMoc/JLinkLog.log -uLowPower= 0 -uInteface= SWD -uIfSpeed= 4000 -uNoReset= 1 -uResetPreRun= 1 -uResetCon= 1 -uResetBefDownload= 1 -uReleaseCM3= 0 -uDisconnectionMode= 1 -uSWOcoreClock= 0 -uEnableSciBoot= 1 -uresetOnReload= 1 -n 0 -uFlashBp= 1 -uSimulation= 0 -ueraseRomOnDownload= 0 -ueraseDataRomOnDownload= 0 -uOSRestriction= 0 -uProgReWriteIRom= 0 -uCPUFrequency= 0 -uCECycle= 1 -uMemRegion= 0x00000000:0x80000:FLASH:n -uMemRegion= 0x08000000:0x4000:DATA_FLASH:n -uTz= SSD -l -uCore= SINGLE_CORE|enabled|1|main -uSyncMode= async -uFirstGDB= main --gdbVersion= 7.2
    Using J-Link version V7.88d - C:\Users\mzerl\.eclipse\com.renesas.platform_1435879475\DebugComp\RA\ARM\Segger_v7.88.4\JLinkARM.dll
    
    Connecting to R7FA6T2BD, ARM Target
            GDBServer endian           : little
            Target power from emulator : Off 
    Starting target connection
    
    Current TrustZone device status
    	DLM state	: Secure Software Development (SSD)
    	Debug level	: 2
    	Secure/NSC memory partition size	: 
    	-	Code Flash Secure	(kB)	: 40
    	-	Code Flash NSC		(kB)	: 24
    	-	Data Flash Secure	(kB)	: 0
    	-	SRAM Secure		(kB)	: 5
    	-	SRAM NSC		(kB)	: 3
    Finished target connection
    GDB: 58818
    Target connection status - OK
    Target connection status - OK
    Starting download
    Option Function Select, writing to address 0x0100a100 with data ffffffffffffffffffffffffffffffff
    Option Function Select, writing to address 0x0100a134 with data ffffffff
    Option Function Select, writing to address 0x0100a200 with data fffdf0ffffffffffffffffffffffffff...
    Finished download
    GDB action 'Finished download', has failed with error report, failed to download
    Hardware breakpoint set at address 0x327c
    Hardware breakpoint set at address 0x3364
    Hardware breakpoint set at address 0x33bc
    Hardware breakpoint set at address 0x48d6
    GDB action 'read memory', has failed with error code, 0xffffffff
    Disconnected from the Target Debugger.

  • Please create a new post as this is a different device.

Reply Children
No Data