Unable to flash program

I just started using Renesus but I don't know what files to flash. which I followed the manual by selecting Intel .hex 

After receiving the .hex file, I opened Renesas Flash Programmer V3.15 and followed the steps, but an error occurred as shown in the picture. Where should I set it? please explain to me.

error

Renesas Flash Programmer V3.15.00 [1 Apr 2024]
Loading Project (C:\Users\Tiraporn\Documents\Renesas Flash Programmer\V3.15\Test1\Test1.rpj)
Loading File (C:\Users\Tiraporn\e2_studio\workspace\Project_LED\Debug\Project_LED.hex) CRC-32=AFEBAD66

Target device : RA

Connecting the tool
Tool : E2 emulator Lite (1LS038476B), Interface : SWD
Emulator's supply power : OFF
Emulator's firmware version:3.04.01.000
Connecting to the target device
Connecting to the target device
Communication speed : 3.0 MHz
Signature:
Device: RA
Device Code: 00390447

Erasing the selected blocks
[Code Flash 1] 0x00000000 - 0x0000FFFF size : 64 K
[Data Flash 1] 0x40100000 - 0x40100FFF size : 4 K

Writing data to the target device
[Code Flash 1] 0x00000000 - 0x00002E7F size : 11.6 K
[Config Area 1] 0x01010018 - 0x01010033 size : 28

Verifying data
[Code Flash 1] 0x00000000 - 0x00002E7F size : 11.6 K
Setting the target device

Disconnecting the tool
Error(E300010A): The data do not match. (Address: 0x00000000)
Operation failed.

Parents
  • Hello kati,

    What RA part number do you use and on what board ( your customized board or some of the Renesas eval kits)?

    Also, could you please attach your whole project.

    Just to mention that you seem to follows the correct process to produce the hex file and flash it using RFP.

    Regards,

    AL_Renesas

Reply
  • Hello kati,

    What RA part number do you use and on what board ( your customized board or some of the Renesas eval kits)?

    Also, could you please attach your whole project.

    Just to mention that you seem to follows the correct process to produce the hex file and flash it using RFP.

    Regards,

    AL_Renesas

Children