I just started using Renesus but I don't know what files to flash. which I followed the manual by selecting Intel .hex
After receiving the .hex file, I opened Renesas Flash Programmer V3.15 and followed the steps, but an error occurred as shown in the picture. Where should I set it? please explain to me.
error
Renesas Flash Programmer V3.15.00 [1 Apr 2024]Loading Project (C:\Users\Tiraporn\Documents\Renesas Flash Programmer\V3.15\Test1\Test1.rpj)Loading File (C:\Users\Tiraporn\e2_studio\workspace\Project_LED\Debug\Project_LED.hex) CRC-32=AFEBAD66
Target device : RA
Connecting the toolTool : E2 emulator Lite (1LS038476B), Interface : SWDEmulator's supply power : OFFEmulator's firmware version:3.04.01.000Connecting to the target deviceConnecting to the target deviceCommunication speed : 3.0 MHzSignature: Device: RA Device Code: 00390447
Erasing the selected blocks [Code Flash 1] 0x00000000 - 0x0000FFFF size : 64 K [Data Flash 1] 0x40100000 - 0x40100FFF size : 4 K
Writing data to the target device [Code Flash 1] 0x00000000 - 0x00002E7F size : 11.6 K [Config Area 1] 0x01010018 - 0x01010033 size : 28
Verifying data [Code Flash 1] 0x00000000 - 0x00002E7F size : 11.6 KSetting the target device
Disconnecting the toolError(E300010A): The data do not match. (Address: 0x00000000)Operation failed.