FreeRTOS critical section causes hard fault

I have a custom board running code (RA6M5/FSP4.5.0/FreeRTOS) which can occasionally generate a hard-fault.

The hard-fault is related to memory access performed inside a critical section. When the system operates solely using taskENTER_CRITICAL() or taskENTER_CRITICAL_FROM_ISR() everything works fine. But mixing the two will eventually cause a hard fault.

The debugger when the hard fault occurs makes the call stack look nonsensical. Its hard to get insight once you are in the hard fault handler.

Investigating taskENTER_CRITICAL I saw this on line 198:

```NOTE: This may alter the stack (depending on the portable implementation)
so must be used with care!```

This lead me to assume this was the case and try to use methods that might fix the issue. In particular I added calls to __DSB() at the beginning of each critical section. These seem to work but only when I run the program using the debugger.

I'm open to trying different primitive instead of a critical section. Inside that critical section is access to a simple circular buffer.

Parents
  • I've been reading https://www.freertos.org/RTOS-Cortex-M3-M4.html , I'm currently using a CM33 (RA6M5) so I believe it applies.

    #ifndef configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY
    #define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY ((1))
    #endif
    #ifndef configMAX_SYSCALL_INTERRUPT_PRIORITY
    #define configMAX_SYSCALL_INTERRUPT_PRIORITY (configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - __NVIC_PRIO_BITS))
    #endif

    R7FA6M5BH.h  defines __NVIC_PRIO_BITS as 4 which would mean that configMAX_SYSCALL_INTERRUPT_PRIORITY = 1 << (8-4) = 16

    If I read the documentation correctly this means that I would have to specify any interrupt that uses a critical section at 16 or above... Trouble is 15 is highest priority I can set with the FSP.

    Am I missing something here?

  • If the program runs for a long time and then hangs, it could be because a stack overflow. Please try to increase the stack size.

    Also when the hard fault occurs, what information do you get from the Fault Stats window on e2studio ?

Reply Children