I need to use the RA0E1 IICA_SLAVE.With e² studio 2024-04 and FSP 5.2.0 it was not possible to add it with "New Stack", only IICA_MASTER could be added.
With e² studio 2024-04 and FSP 5.3.0 it is possible to add it with "New Stack";in the Stacks/Properties Tab SCLA and SDAA Pin can be assigned to a port numberbut after changing to the "Pins/Pin Function" Tab there in the Section Peripherals/IICA/IICA0 the Operation Mode is disabled and cannot be Enabled !?
With e² studio 2024-04 and FSP 5.4.0 it is possible to add it with "New Stack";in the Stacks/Properties Tab SCLA and SDAA Pin can be assigned to a port numberbut after changing to the "Pins/Pin Function" Tab there the Section Peripherals/IICA/IICA0 is completely missing !?
The problem is reproducible on another PC of a collegue.Does anybody know if there is a solution to this behaviour ?
Is there any new information on this, especially why the IICA in the Peripherals section is missing? Are we supposed to use the pin configuration in the stack and leave the pin configuration alone?
We are in the process of implementing the RA0E1 as I²C slave and wonder if we have chosen the wrong product
Hello,
Please check my answer below.
Best Regards,
IK