RA0 IICA_SLAVE cannot be configured properly

I need to use the RA0E1 IICA_SLAVE.
With e² studio 2024-04 and FSP 5.2.0 it was not possible to add it with "New Stack", only IICA_MASTER could be added.

With e² studio 2024-04 and FSP 5.3.0 it is possible to add it with "New Stack";
in the Stacks/Properties Tab SCLA and SDAA Pin can be assigned to a port number
but after changing to the "Pins/Pin Function" Tab there in the Section Peripherals/IICA/IICA0 the Operation Mode is disabled and cannot be Enabled !?

With e² studio 2024-04 and FSP 5.4.0 it is possible to add it with "New Stack";
in the Stacks/Properties Tab SCLA and SDAA Pin can be assigned to a port number
but after changing to the "Pins/Pin Function" Tab there the Section Peripherals/IICA/IICA0 is completely missing !?

The problem is reproducible on another PC of a collegue.
Does anybody know if there is a solution to this behaviour ?