Renesas RA6M3 with ESP32 C6

I have try to connect the re6m3 board with ESP32 C6 with the at comment but i am unable to connect to the wifi can someone help me

#include "wifi.h"

#include "hal_data.h"

#include "SEGGER_RTT/SEGGER_RTT.h"

#include "tx_api.h"

#include <string.h> // For string functions

#define UART_BUFFER_SIZE 256

volatile uint8_t g_uart_rx_buffer[UART_BUFFER_SIZE];

volatile uint32_t g_uart_rx_count = 0;

#define WIFI_SSID "Redmi" // Replace with your WiFi SSID

#define WIFI_PASSWORD "12345678" // Replace with your WiFi password

#define AT_CMD_RST "AT+RST\r\n"

#define AT_CMD_CWMODE "AT+CWMODE=1\r\n"

#define AT_CMD_CWJAP "AT+CWJAP=\"" WIFI_SSID "\",\"" WIFI_PASSWORD "\"\r\n"

#define AT_CMD_CWLAP "AT+CWLAP\r\n" // Command to list available networks

void print_received_data(void);

void user_uart_callback(uart_callback_args_t *p_args);

void init_uart(void);

void init_rtt(void);

void send_at_command(const char *cmd);

void receive_response(char *buffer, uint32_t length);

// UART callback function to handle received data

void user_uart_callback(uart_callback_args_t *p_args)

{

if (UART_EVENT_RX_CHAR == p_args->event)

{

if (g_uart_rx_count < UART_BUFFER_SIZE)

{

g_uart_rx_buffer[g_uart_rx_count++] = p_args->data;

}

}

}

// UART initialization

void init_uart(void)

{

fsp_err_t err = R_SCI_UART_Open(&g_uart_ctrl, &g_uart_cfg);

assert(FSP_SUCCESS == err);

}

// RTT initialization for debugging

void init_rtt(void)

{

SEGGER_RTT_ConfigUpBuffer(0, NULL, NULL, 0, SEGGER_RTT_MODE_BLOCK_IF_FIFO_FULL);

}

// Function to print received data via RTT

void print_received_data(void)

{

if (g_uart_rx_count > 0)

{

SEGGER_RTT_WriteString(0, "Received data: ");

SEGGER_RTT_Write(0, (char *)g_uart_rx_buffer, g_uart_rx_count);

SEGGER_RTT_WriteString(0, "\n");

g_uart_rx_count = 0;

}

}

// Function to send an AT command over UART

void send_at_command(const char *cmd)

{

g_uart.p_api->write(g_uart.p_ctrl, (uint8_t *)cmd, strlen(cmd));

}

// Function to receive the response from ESP32-C6

void receive_response(char *buffer, uint32_t length)

{

// Wait until response is received (implementing a simple polling)

while (g_uart_rx_count == 0)

{

tx_thread_sleep(10); // Sleep to avoid blocking the CPU

}

// Copy received data to buffer

if (g_uart_rx_count <= length)

{

memcpy(buffer, g_uart_rx_buffer, g_uart_rx_count);

buffer[g_uart_rx_count] = '\0'; // Null-terminate the string

g_uart_rx_count = 0; // Reset counter for next operation

}

}

// Entry point for WiFi connection

void wifi_entry(void)

{

char response[256] = {0};

int retry_count = 0;

const int max_retries = 3;

init_uart();

init_rtt();

SEGGER_RTT_WriteString(0, "Initializeling...\n");

while (retry_count < max_retries) {

SEGGER_RTT_WriteString(0, "Resetting ESP32...\n");

send_at_command(AT_CMD_RST);

tx_thread_sleep(1000); // Increased delay after reset

receive_response(response, sizeof(response));

SEGGER_RTT_WriteString(0, "Response after AT+RST: ");

SEGGER_RTT_WriteString(0, response);

SEGGER_RTT_WriteString(0, "\n");

if (strstr(response, "ready") == NULL) {

SEGGER_RTT_WriteString(0, "ESP32 reset failed. Retrying...\n");

retry_count++;

continue;

}

// Set WiFi mode

SEGGER_RTT_WriteString(0, "Setting WiFi mode...\n");

send_at_command(AT_CMD_CWMODE);

tx_thread_sleep(500);

receive_response(response, sizeof(response));

SEGGER_RTT_WriteString(0, "Response after AT+CWMODE: ");

SEGGER_RTT_WriteString(0, response);

SEGGER_RTT_WriteString(0, "\n");

if (strstr(response, "OK") == NULL) {

SEGGER_RTT_WriteString(0, "Failed to set WiFi mode. Retrying...\n");

retry_count++;

continue;

}

// Scan networks

SEGGER_RTT_WriteString(0, "Scanning networks...\n");

send_at_command(AT_CMD_CWLAP);

tx_thread_sleep(5000); // Increased delay for network scan

receive_response(response, sizeof(response));

SEGGER_RTT_WriteString(0, "Available Networks: ");

SEGGER_RTT_WriteString(0, response);

SEGGER_RTT_WriteString(0, "\n");

// Connect to WiFi

SEGGER_RTT_WriteString(0, "Connecting to WiFi...\n");

send_at_command(AT_CMD_CWJAP);

tx_thread_sleep(10000); // Increased delay for connection attempt

receive_response(response, sizeof(response));

SEGGER_RTT_WriteString(0, "Response after AT+CWJAP: ");

SEGGER_RTT_WriteString(0, response);

SEGGER_RTT_WriteString(0, "\n");

if (strstr(response, "WIFI CONNECTED") != NULL && strstr(response, "OK") != NULL) {

SEGGER_RTT_WriteString(0, "WiFi connected successfully.\n");

break;

} else {

SEGGER_RTT_WriteString(0, "WiFi connection failed. Retrying...\n");

retry_count++;

}

}

if (retry_count == max_retries) {

SEGGER_RTT_WriteString(0, "Failed to connect after maximum retries.\n");

}

// Main loop

while (1) {

tx_thread_sleep(TX_TIMER_TICKS_PER_SECOND);

}

}

Parents Reply Children
No Data