RA4M2 Uart TX always one more stop bit than expected

Hi,

I'm working on a project with R7FA4M2AD3CFM, we are setting up Modbus RTU communication on uart0, FSP4.0.

Here is the problem, no matter what stop bits is configured from the uart property, there is always one more bit added to actual communication for Tx(read from actual communication RS485 bus).

I understand from the user manual about stop bit for Rx is fine. Just want to know for Tx if this is the expected behavior.

Thanks.

Parents Reply Children
No Data