Hi team!I am trying out the MCUBoot on a the EK-RA6M5, it is going well so far, I have a couple of questions:
Warmest Regards,Dave
Hey Dave,
As per the hardware manual, the MCU supports P384, but it's not supported by the FSP. While it is possible to use a wrapped certificate for image authentication in protected mode with MCUBoot, the current MCUBoot implementation for Renesas devices doesn't natively support certificate-based authentication. You'll need to implement custom features in the FSP-generated code to enable this functionality.
Regards,
Gaurav N