I have installed 3 fsp version 5.3.0, 5.4.0 and 5.5.0. i download zip file and pasted it content in e2studio support area folder it was working fine until i changed my workplace folder. in new workplace folder no fsp is installed error.
Moaz,
That is not the best way to install the FSPs. Please download the .EXE version and run the installer and point to the root directory of your e2 studio. This way it will remain for all workspaces.
I suppose root cause is using workspace created in different version of e² studio (or created as different user). Support area is configured in each workspace and the folder paths are differ depending on e² studio versions.Don't share workspace among multiple versions of e² studio.