Regarding MIPI -DSI interfacing with TFT LCD

I'm working on connecting a TFT LCD (E45RA-MW276-C) to the EK-RA8M1 board using the MIPI-DSI interface through the J58 connector. I need assistance with the specific pin muxing and configuration for this interface.

  1. Which pins on the J58 port are muxed to the MIPI-DSI signals (Clock and Data lanes) when connecting this display?

  2. Are there any other control signals (I2C, Reset, etc.) that need to be muxed or configured for proper operation?

Parents Reply Children
No Data