Regarding MIPI -DSI interfacing with TFT LCD

I'm working on connecting a TFT LCD (E45RA-MW276-C) to the EK-RA8M1 board using the MIPI-DSI interface through the J58 connector. I need assistance with the specific pin muxing and configuration for this interface.

  1. Which pins on the J58 port are muxed to the MIPI-DSI signals (Clock and Data lanes) when connecting this display?

  2. Are there any other control signals (I2C, Reset, etc.) that need to be muxed or configured for proper operation?