Guidelines for Bootloader Firmware with MCUBoot and External QSPI Flash

Hi,

Could someone please provide any available guidelines for Bootloader Firmware using MCUBoot and External QSPI Flash based on the following specifications?

  • MCU: R7FA4M3AFCFP
  • IDE: e2Studio
  • FSP Version: V4.2.0

Thanks,
Parth

Parents Reply
  • I have temporarily disabled encryption in the bootloader to verify that the QSPI is functioning correctly in our custom board. Once it’s confirmed to be working, I will enable the encryption.

    I have not tried sample code, as it includes encryption that I cannot use at the moment. Therefore, I would appreciate your input on what I might have overlooked/missed in the configuration, based on the snapshots I shared earlier.

Children
  • I do not see anything wrong. If you use EK-RA4M3 and the on-board QSPI you should use the same QSPI settings an in the example project.

    The MCUboot settings depend a lot on your application (for example upgrade method, image sizes etc).

  • I believe I may have identified the source of the issue. Here's a brief explanation, and I would appreciate your help in finding a solution. In Approach 1, the data readbacks are incorrect, while in Approach 2, everything works as expected. In Approach 1, I'm directly accessing the memory location, whereas in Approach 2, I’m using the QSPI API with commands. I need to resolve the issue with Approach 1 because the bootloader might be reading data this way (as per approach-1).


    #define QSPI_DEVICE_START_ADDRESS    (0x60000000)

    #define QSPI_FLASH_ADDRESS(page_no)     (uint8_t *) (QSPI_DEVICE_START_ADDRESS + (page_no * PAGE_WRITE_SIZE))

    uint32_t address = (uint32_t)(QSPI_FLASH_ADDRESS(0));

    Approach 1:


    memcpy(write_buffer, (uint8_t *)(address), SIZE_64KB);
    R_BSP_SoftwareDelay(500,1000);

    Approach 2:

    data[0] = 0x03; // Read command
    data[1] = (address >> 16) & 0xFF;
    data[2] = (address >> 8) & 0xFF;
    data[3] = address & 0xFF;
    data[4] = 0x00;
    R_QSPI_DirectWrite(&g_qspi0_ctrl, data, 4, true);
    R_QSPI_DirectRead(&g_qspi0_ctrl, (uint8_t *)write_buffer, SIZE_64KB); // Reading only 3 bytes
    R_BSP_SoftwareDelay(500, BSP_DELAY_UNITS_MILLISECONDS);

    Please assist me to resolve this issue with approach-1.

    Regards,

    Parth