Hello,
Is it possible with FSP Configurator to create threads with entry input?
Threadx Docs have this example:
I dont see any options in the FSP Configurtor where this might be possibile to do.
Looking at the generated code for a thread I see this:
If not possible, do i have to create threads without fsp configurator?
Best Regards
Joe
Hello Joe,
Thanks for reaching out Renesas Engineering Community.
Please check the lab we provide for Azure RTOS in our gallery here: I-004 Introduction to FSP Azure RTOS ThreadX (4.5.0) Course Materials
Hope it helps.
Regards,
IK
Hello IK,
thanks for the docs.
I will get back to you after reading :)
I read the course but I could not find any Information about this particular parameter. I guess I have to create the threads with a custom function and not use the fsp for thread generation?
Regards Joe