How to use timer object

I am trying to use the timer object in my code but i can't use it can you help me to use the timer object in my code 






/*

* Copyright (c) 2020 - 2024 Renesas Electronics Corporation and/or its affiliates

*

* SPDX-License-Identifier: BSD-3-Clause

*/

#include "blinky_thread.h"

#include "FreeRTOS.h"

#include "timers.h"

#define configUSE_TIMERS 1

#define configTIMER_TASK_PRIORITY (configMAX_PRIORITIES - 1)

#define configTIMER_QUEUE_LENGTH 10

#define configTIMER_TASK_STACK_DEPTH 128

extern bsp_leds_t g_bsp_leds;

// Global timer handle

TimerHandle_t g_blinky_timer;

// Callback function for the timer

void blinky_timer_callback(TimerHandle_t xTimer)

{

/* LED type structure */

bsp_leds_t leds = g_bsp_leds;

/* If this board has no LEDs then return */

if (0 == leds.led_count)

{

return;

}

/* Static variable to track pin level */

static bsp_io_level_t pin_level = BSP_IO_LEVEL_LOW;

/* Enable access to the PFS registers */

R_BSP_PinAccessEnable();

/* Update all board LEDs */

for (uint32_t i = 0; i < leds.led_count; i++)

{

/* Get pin to toggle */

uint32_t pin = leds.p_leds[i];

/* Write to this pin */

R_BSP_PinWrite((bsp_io_port_pin_t) pin, pin_level);

}

/* Protect PFS registers */

R_BSP_PinAccessDisable();

/* Toggle level for next write */

pin_level = (BSP_IO_LEVEL_LOW == pin_level) ?

BSP_IO_LEVEL_HIGH : BSP_IO_LEVEL_LOW;

}

void blinky_thread_entry(void * pvParameters)

{

FSP_PARAMETER_NOT_USED(pvParameters);

/* Check if timer was created successfully */

if (g_blinky_timer == NULL)

{

/* Handle timer creation failure */

while(1)

{

/* Trap here if timer creation failed */

}

}

/* Start the timer */

if (xTimerStart(g_blinky_timer, 0) != pdPASS)

{

/* Handle timer start failure */

while(1)

{

/* Trap here if timer start failed */

}

}

vTaskDelete(NULL);

}

Parents Reply Children