I am trying to store the log in the OSPI but some times it shows the error OSPI Write failed! Error code: 40002I have a array of log if the ram i need to store the elements of the log in my OSPI but some times i am facing the above issue.I am not facing the issue in the begging of the thread i am able to store six data continuously while writing the 7 th data i am getting this error
The OSPI code is
#include "access_log.h"
#include "ospi.h"
#include "SEGGER_RTT/SEGGER_RTT.h"
#include "ospi_b_ep.h"
#include "common_utils.h"
#include "ospi_b_commands.h"
// Define OSPI sectors
#define OSPI_B_SECTOR_SIZE (*** * 1024) // 64KB sectors
#define OSPI_B_TOTAL_SECTORS *** // Adjust based on your OSPI chip
#define OSPI_B_SECTOR_LAST (OSPI_B_TOTAL_SECTORS - 2) // Reserve last sector for state
#define OSPI_B_STATE_SECTOR (OSPI_B_TOTAL_SECTORS - 1) // Last sector for storing state
// Structure to track OSPI storage state
typedef struct {
uint32_t next_write_address; // Next available address for writing
uint32_t total_entries; // Total number of entries stored
uint32_t current_sector; // Current sector being written to
} OspiStorageState;
// Global storage state
static OspiStorageState g_storage_state = {
.next_write_address = OSPI_B_APP_ADDRESS(OSPI_B_SECTOR_FIRST),
.total_entries = 0,
.current_sector = OSPI_B_SECTOR_FIRST
};
// Function to load storage state from a reserved area in OSPI
static fsp_err_t load_storage_state(void)
{
fsp_err_t err = FSP_SUCCESS;
// Use direct memory access to read state
uint8_t *state_address = (uint8_t *)OSPI_B_APP_ADDRESS(OSPI_B_STATE_SECTOR);
memcpy(&g_storage_state, state_address, sizeof(OspiStorageState));
// Validate loaded state
if (g_storage_state.current_sector >= OSPI_B_SECTOR_LAST ||
g_storage_state.current_sector < OSPI_B_SECTOR_FIRST)
// Reset to default if invalid
g_storage_state.next_write_address = OSPI_B_APP_ADDRESS(OSPI_B_SECTOR_FIRST);
g_storage_state.total_entries = 0;
g_storage_state.current_sector = OSPI_B_SECTOR_FIRST;
}
return err;
void handle_error(fsp_err_t err, const char *err_str)
if(FSP_SUCCESS != err)
/* Print the error */
APP_PRINT(err_str);
/* Close opened OSPI module*/
if(0U != g_ospi_b_ctrl.open)
if(FSP_SUCCESS != R_OSPI_B_Close(&g_ospi_b_ctrl))
APP_ERR_PRINT("R_OSPI_B_Close FAILED\r\n");
/* Close opened GPT module*/
if(0U != g_timer_ctrl.open)
if(FSP_SUCCESS != R_GPT_Close(&g_timer_ctrl))
APP_ERR_PRINT("R_GPT_Close FAILED\r\n");
APP_ERR_TRAP(err);
fsp_err_t ospi_read_stored_log(void)
uint8_t *p_ospi_address = OSPI_B_APP_ADDRESS(OSPI_B_SECTOR_FIRST);
uint32_t execute_time = RESET_VALUE;
AccessLogEntry read_entry;
uint32_t valid_entries = 0;
/* Start timer for read operation */
err = timer_start_measure();
handle_error(err, "timer_start_measure FAILED\r\n");
/* Read until we find an empty entry or reach sector size */
for (uint32_t i = 0; i < OSPI_B_SECTOR_SIZE_256K / sizeof(AccessLogEntry); i++)
uint8_t *current_address = p_ospi_address + (i * sizeof(AccessLogEntry));
/* Read entry from OSPI */
memcpy(&read_entry, current_address, sizeof(AccessLogEntry));
/* Check if entry is empty or invalid */
if (read_entry.timestamp == 0xFFFFFFFF || read_entry.timestamp == 0)
continue;
/* Convert timestamp to time format */
uint8_t hours = read_entry.timestamp / 3600;
uint8_t minutes = (read_entry.timestamp % 3600) / 60;
uint8_t seconds = read_entry.timestamp % 60;
/* Print entry details with address at the end */
APP_PRINT("[%02u:%02u:%02u] | %d | %u | %d | %s | %s | 0x%08x\r\n",
hours, minutes, seconds,
read_entry.timestamp,
read_entry.rfid,
read_entry.door_no,
read_entry.action ? read_entry.action : "RFID Not Found",
read_entry.processed ? "Yes" : "No",
(uint32_t)current_address);
valid_entries++;
/* Get and print read time */
err = timer_get_measure(&execute_time);
handle_error(err, "timer_get_measure FAILED\r\n");
static void print_last_entries(uint8_t *p_ospi_address, uint32_t total_entries)
uint32_t start_index;
/* Calculate starting point for last 20 entries */
if (total_entries <= 20) {
start_index = 0;
} else {
start_index = total_entries - 20;
APP_PRINT("\r\n=== LAST 20 OSPI ACCESS LOG ENTRIES ===\r\n");
APP_PRINT("Showing entries %lu to %lu of %lu total entries\r\n",
start_index + 1, total_entries, total_entries);
APP_PRINT("Timestamp | RFID | Door | Action | Processed\r\n");
APP_PRINT("---------------------------------------------\r\n");
/* Read and print last 20 valid entries */
for (uint32_t i = start_index; i < total_entries; i++)
memcpy(&read_entry,
p_ospi_address + (i * sizeof(AccessLogEntry)),
sizeof(AccessLogEntry));
/* Print entry details */
APP_PRINT("[%02u:%02u:%02u] %u | %d | %s | %s\r\n",
read_entry.action,
read_entry.processed ? "Yes" : "No");
APP_PRINT("=======================================\r\n");
fsp_err_t ospi_erase_all_data(void)
APP_PRINT("\r\n=== ERASING ALL OSPI DATA ===\r\n");
/* Start timer */
/* Erase sector */
err = ospi_b_erase_operation(p_ospi_address, &execute_time);
handle_error(err, "ospi_b_erase_operation FAILED\r\n");
/* Wait for erase operation to complete */
err = ospi_b_wait_operation(OSPI_B_TIME_ERASE_256K);
handle_error(err, "ospi_b_wait_operation FAILED\r\n");
APP_PRINT("OSPI erase completed in %d nanoseconds\r\n", execute_time);
APP_PRINT("============================\r\n");
void ospi_entry(void *pvParameters)
uint8_t *p_ospi_address = NULL;
static uint16_t last_stored_index = 0;
static uint32_t ospi_write_position = 0;
AccessLogEntry temp_entry;
/* Initialize OSPI */
err = timer_init();
handle_error(err, "timer_init FAILED\r\n");
err = ospi_b_init();
handle_error(err, "ospi_b_init FAILED\r\n");
/* Set OSPI to SPI mode for reliable operation */
err = ospi_b_set_protocol_to_spi();
handle_error(err, "ospi_b_set_protocol_to_spi FAILED\r\n");
/* Set base address for storing logs */
p_ospi_address = OSPI_B_APP_ADDRESS(OSPI_B_SECTOR_FIRST);
/* Find the last written position in OSPI */
bool found_end = false;
uint32_t max_search = OSPI_B_SECTOR_SIZE_256K / sizeof(AccessLogEntry);
APP_PRINT("\r\nInitializing OSPI Storage Thread...\r\n");
APP_PRINT("Searching for last written position in OSPI...\r\n");
/* Search for last written position by looking for first empty entry */
for (uint32_t i = 0; i < max_search; i++)
/* Read entry from current position */
memcpy(&temp_entry,
/* Check if entry is empty (unwritten OSPI will have 0xFF) */
if (temp_entry.timestamp == 0xFFFFFFFF)
ospi_write_position = i;
found_end = true;
break;
if (!found_end) {
ospi_write_position = 0; // Start from beginning if OSPI is full
APP_PRINT("OSPI is full, will start overwriting from beginning\r\n");
APP_PRINT("OSPI write position initialized at index: %lu\r\n", ospi_write_position);
/* Main thread loop */
while(1)
/* Check if mutex is available */
UBaseType_t mutex_count = uxSemaphoreGetCount(globalAccessLogMutex);
if (mutex_count > 0) /* Mutex is free */
/* Check if there are new entries to store */
if (last_stored_index < globalLogIndex)
/* Calculate number of entries to store */
uint16_t entries_to_store = globalLogIndex - last_stored_index;
uint32_t data_size = entries_to_store * sizeof(AccessLogEntry);
/* Check if we need to wrap around */
if ((ospi_write_position + entries_to_store) * sizeof(AccessLogEntry) >= OSPI_B_SECTOR_SIZE_256K)
APP_PRINT("\r\nOSPI storage reached end, wrapping to beginning\r\n");
ospi_write_position = 0;
/* Write new entries to OSPI */
err = R_OSPI_B_Write(&g_ospi_b_ctrl,
(uint8_t *)&globalAccessLog[last_stored_index],
p_ospi_address + (ospi_write_position * sizeof(AccessLogEntry)),
data_size);
if (err != FSP_SUCCESS) {
APP_PRINT("OSPI Write failed! Error code: %d\r\n", err);
/* Wait for write operation to complete */
err = ospi_b_wait_operation(OSPI_B_TIME_WRITE);
APP_PRINT("OSPI Write operation timeout! Error code: %d\r\n", err);
/* Verify written data */
bool verification_error = false;
for (uint16_t i = 0; i < entries_to_store; i++)
AccessLogEntry verify_entry;
memcpy(&verify_entry,
p_ospi_address + ((ospi_write_position + i) * sizeof(AccessLogEntry)),
if (memcmp(&verify_entry, &globalAccessLog[last_stored_index + i],
sizeof(AccessLogEntry)) != 0)
verification_error = true;
APP_PRINT("Data verification failed at entry %d\r\n",
ospi_write_position + i);
if (!verification_error)
/* Update positions */
ospi_write_position += entries_to_store;
last_stored_index = globalLogIndex;
APP_PRINT("\r\n=== NEW ENTRIES STORED IN OSPI ===\r\n");
APP_PRINT("Stored %d new entries\r\n", entries_to_store);
/* Display last 20 entries */
APP_PRINT("\r\n=== LAST 20 ENTRIES ===\r\n");
uint32_t start_idx = (ospi_write_position > 20) ?
(ospi_write_position - 20) : 0;
for (uint32_t i = start_idx; i < ospi_write_position; i++)
AccessLogEntry display_entry;
memcpy(&display_entry,
uint8_t hours = display_entry.timestamp / 3600;
uint8_t minutes = (display_entry.timestamp % 3600) / 60;
uint8_t seconds = display_entry.timestamp % 60;
display_entry.rfid,
display_entry.door_no,
display_entry.action,
display_entry.processed ? "Yes" : "No");
/* Print storage status */
float usage_percent = ((float)ospi_write_position * sizeof(AccessLogEntry)) /
OSPI_B_SECTOR_SIZE_256K * 100;
APP_PRINT("\r\n=== OSPI STORAGE STATUS ===\r\n");
APP_PRINT("Total Entries: %lu\r\n", ospi_write_position);
APP_PRINT("Storage Usage: %.1f%%\r\n", usage_percent);
APP_PRINT("Next Write Position: %lu\r\n", ospi_write_position);
else
APP_PRINT("Failed to verify written data. Retrying...\r\n");
/* Delay before next check */
vTaskDelay(pdMS_TO_TICKS(1000));