Hi,
I'm new on RA MCU, and I need to interface a Serial Flash via QSPI, currently I can't find the R7FA4M2AD3CFM pinout to come out the schematic.
Would like to ask where can find the 64pin Pinout diagram, the hardware manual didn't show which pin as a group to use for QSPI, I found :-
QSPCLK link to pin 48 and pin 49
QSSL link to pin 21 and pin 37
QIO0 link to pin 46
QIO1 link to pin 47
QIO2 link to pin 44
QIO3 link to pin 24 and pin 45
Thanks in advance
Best regards,
Neoh.K.L.
Hello Neoh,
Thank you for reaching out to Renesas! You can view the pinout details directly in the FSP Configuration tab in e² studio after creating a project. Navigate to the Pin Configuration view, where you can assign and verify the pin functions, including the QSPI pins, as shown in the visualization. This will give you a clear mapping of the QSPI-related pins.
Kind Regards,
Payodhi
Dear Payodhi,
Thank you for your answer, I will download the FSP software and try it out.
Neoh K.L.