I have been using RA0E1 microcontroller in a custom board, and I need to transmit data into another microcontroller. For that I’m using Simplified SPI, where the RA0E1 controller acts as a slave. I have assigned SI00, SO00 and SCLK00 pins to transmit data. I have kept SSI00 pin open in my circuit board. Now when I am running my circuit on debug mode, I noticed that the callback function is not being called when the SPI transfer takes place. However, the FSP err is being acknowledged as FSP_SUCCESS. Is it necessary to use SSI00 pin to receive command from master, or can we configure this as output low at all times, or just ground that pin?
Hello,
I've made this code to demonstrate the correct SPI configuration and communication between the two internal channels of RA0E1. Let us know if you need further assistance.
SPIbridge_RA0E1.zip
Kind regards,
Payodhi