RTC returns the wrong time of hour

Hello,

We use RA6M5. The FSP is 3.5.0.

Previously, we used the internal clock as the RTC source, but it caused time-drifting issues, leading to RTC inaccuracy. In the new hardware design, an external 32,768Hz crystal has been added, and we are now using it as the RTC clock source.

However, we encountered an issue with the RTC. Initially, we set the device time to 9:50 AM. When the time reaches 10:00 AM, the R_RTC_CalendarTimeGet() function retrieves the time from the RTC driver. Instead of returning 10:00 AM, it returns 12:00 AM. Additionally, we noticed that the time resets to 12:00 AM every 12 hours.

Do you know why the hour, which should be 10, resets to 0? Could you also provide insights into why the time resets every 12 hours?

By using the internal clock as the RTC clock source, there is no such issue.

Thanks!

Parents
  • We did update the r_rtc.c a little bit. But those changes are minor. It shouldn't impact the hour of time. Please see attached file r_rtc_updated.c. 

    /***********************************************************************************************************************
     * Copyright [2020-2021] Renesas Electronics Corporation and/or its affiliates.  All Rights Reserved.
     *
     * This software and documentation are supplied by Renesas Electronics America Inc. and may only be used with products
     * of Renesas Electronics Corp. and its affiliates ("Renesas").  No other uses are authorized.  Renesas products are
     * sold pursuant to Renesas terms and conditions of sale.  Purchasers are solely responsible for the selection and use
     * of Renesas products and Renesas assumes no liability.  No license, express or implied, to any intellectual property
     * right is granted by Renesas. This software is protected under all applicable laws, including copyright laws. Renesas
     * reserves the right to change or discontinue this software and/or this documentation. THE SOFTWARE AND DOCUMENTATION
     * IS DELIVERED TO YOU "AS IS," AND RENESAS MAKES NO REPRESENTATIONS OR WARRANTIES, AND TO THE FULLEST EXTENT
     * PERMISSIBLE UNDER APPLICABLE LAW, DISCLAIMS ALL WARRANTIES, WHETHER EXPLICITLY OR IMPLICITLY, INCLUDING WARRANTIES
     * OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, AND NONINFRINGEMENT, WITH RESPECT TO THE SOFTWARE OR
     * DOCUMENTATION.  RENESAS SHALL HAVE NO LIABILITY ARISING OUT OF ANY SECURITY VULNERABILITY OR BREACH.  TO THE MAXIMUM
     * EXTENT PERMITTED BY LAW, IN NO EVENT WILL RENESAS BE LIABLE TO YOU IN CONNECTION WITH THE SOFTWARE OR DOCUMENTATION
     * (OR ANY PERSON OR ENTITY CLAIMING RIGHTS DERIVED FROM YOU) FOR ANY LOSS, DAMAGES, OR CLAIMS WHATSOEVER, INCLUDING,
     * WITHOUT LIMITATION, ANY DIRECT, CONSEQUENTIAL, SPECIAL, INDIRECT, PUNITIVE, OR INCIDENTAL DAMAGES; ANY LOST PROFITS,
     * OTHER ECONOMIC DAMAGE, PROPERTY DAMAGE, OR PERSONAL INJURY; AND EVEN IF RENESAS HAS BEEN ADVISED OF THE POSSIBILITY
     * OF SUCH LOSS, DAMAGES, CLAIMS OR COSTS.
     **********************************************************************************************************************/
    
    /***********************************************************************************************************************
     * Includes
     **********************************************************************************************************************/
    #include "r_rtc.h"
    
    /***********************************************************************************************************************
     * Macro definitions
     **********************************************************************************************************************/
    #define RTC_MASK_MSB                        (0x0F)
    #define RTC_MASK_LSB                        (0xF0)
    
    #define RTC_FIRST_DAY_OF_A_MONTH            (1)
    
    /* Day of week : valid range between 0 to 6. */
    #define RTC_DAYS_IN_A_WEEK                  (6)
    
    /* Month : valid range between 0 to 11.*/
    #define RTC_MONTHS_IN_A_YEAR                (11)
    #define RTC_LAST_DAY_OF_LEAP_FEB_MONTH      (29)
    #define RTC_LAST_DAY_OF_A_MONTH             (31)
    #define RTC_YEAR_VALUE_MIN                  (100)
    #define RTC_YEAR_VALUE_MAX                  (199)
    
    /* Seconds : valid range between 0 to 59.*/
    #define RTC_SECONDS_IN_A_MINUTE             (59)
    
    /* Minute : valid range between 0 to 59. */
    #define RTC_MINUTES_IN_A_HOUR               (59)
    
    /* Hours : valid range between 0 to 23. */
    #define RTC_HOURS_IN_A_DAY                  (23)
    
    /* In Zeller algorithm value of (-[Y/100] + [Y/400]) is 15 for Y = 2000 to Y = 2099) */
    #define RTC_ZELLER_ALGM_CONST_FIFTEEN       (15)
    
    /* Macro definitions for February and March months */
    #define RTC_FEBRUARY_MONTH                  (2U)
    #define RTC_MARCH_MONTH                     (3U)
    
    #define RTC_TIME_H_MONTH_OFFSET             (1)
    
    /*The RTC has a 100 year calendar to match the starting year 2000, year offset(1900) is added like 117 + 1900 = 2017 */
    #define RTC_TIME_H_YEAR_OFFSET              (1900)
    
    /** "RTC" in ASCII, used to determine if device is open. */
    #define RTC_OPEN                            (0x00525443ULL)
    
    #define RTC_MAX_ERROR_ADJUSTMENT_VALUE      (0x3FU)
    
    #define RTC_RHRCNT_HOUR_MASK                (0x3f)
    #define RTC_COMPARE_ENB_BIT                 (7U)
    #define RTC_MASK_8TH_BIT                    (0x7F)
    
    /* As per HW manual, value of Year is between 0 to 99, the RTC has a 100 year calendar from 2000 to 2099.
     * But as per C standards, tm_year is years since 1900.*/
    #define RTC_C_TIME_OFFSET                   (100)
    
    /* See section 26.2.20 Frequency Register (RFRH/RFRL)" of the RA6M3 manual R01UH0886EJ0100) */
    #define RTC_RFRL_MIN_VALUE_LOCO             (0x7U)
    #define RTC_RFRL_MAX_VALUE_LOCO             (0x1FFU)
    
    #define RTC_SUB_CLK_STABLIZATION_TIME_MS    (100)
    #define RTC_LOCO_STABLIZATION_TIME_US       (190)
    
    /***********************************************************************************************************************
     * Typedef definitions
     **********************************************************************************************************************/
    
    #if defined(__ARMCC_VERSION) || defined(__ICCARM__)
    typedef void (BSP_CMSE_NONSECURE_CALL * rtc_prv_ns_callback)(rtc_callback_args_t * p_args);
    #elif defined(__GNUC__)
    typedef BSP_CMSE_NONSECURE_CALL void (*volatile rtc_prv_ns_callback)(rtc_callback_args_t * p_args);
    #endif
    
    /***********************************************************************************************************************
     * Private function prototypes
     **********************************************************************************************************************/
    static uint8_t rtc_dec_to_bcd(uint8_t to_convert);
    static uint8_t rtc_bcd_to_dec(uint8_t to_convert);
    void           rtc_alarm_periodic_isr(void);
    void           rtc_carry_isr(void);
    
    /***********************************************************************************************************************
     * Private global variables
     **********************************************************************************************************************/
    
    /***********************************************************************************************************************
     * Global Variables
     **********************************************************************************************************************/
    
    /** RTC Implementation of Real Time Clock  */
    const rtc_api_t g_rtc_on_rtc =
    {
        .open               = R_RTC_Open,
        .close              = R_RTC_Close,
        .calendarTimeGet    = R_RTC_CalendarTimeGet,
        .calendarTimeSet    = R_RTC_CalendarTimeSet,
        .calendarAlarmGet   = R_RTC_CalendarAlarmGet,
        .calendarAlarmSet   = R_RTC_CalendarAlarmSet,
        .periodicIrqRateSet = R_RTC_PeriodicIrqRateSet,
        .infoGet            = R_RTC_InfoGet,
        .errorAdjustmentSet = R_RTC_ErrorAdjustmentSet,
        .callbackSet        = R_RTC_CallbackSet,
    };
    
    #if RTC_CFG_PARAM_CHECKING_ENABLE
    
    /* Number of days in each months start from January to December */
    static const uint8_t days_in_months[12] = {31U, 28U, 31U, 30U, 31U, 30U, 31U, 31U, 30U, 31U, 30U, 31U};
    #endif
    
    /***********************************************************************************************************************
     * Functions
     **********************************************************************************************************************/
    
    static void r_rtc_set_clock_source(rtc_instance_ctrl_t * const p_ctrl, rtc_cfg_t const * const p_cfg);
    
    static void r_rtc_start_bit_update(uint8_t value);
    
    static void r_rtc_software_reset(void);
    
    static void r_rtc_config_rtc_interrupts(rtc_instance_ctrl_t * const p_ctrl, rtc_cfg_t const * const p_cfg);
    
    static void r_rtc_irq_set(bool irq_enable_flag, uint8_t mask);
    
    static void r_rtc_call_callback(rtc_instance_ctrl_t * p_ctrl, rtc_event_t event);
    
    #if RTC_CFG_PARAM_CHECKING_ENABLE
    static fsp_err_t r_rtc_rfrl_validate(uint32_t value);
    
    static fsp_err_t r_rtc_err_adjustment_paramter_check(rtc_error_adjustment_cfg_t const * const err_adj_cfg);
    
    static fsp_err_t r_rtc_time_and_date_validate(rtc_time_t * const p_time);
    
    static fsp_err_t r_rtc_time_validate(rtc_time_t * const p_time);
    
    static fsp_err_t r_rtc_date_validate(rtc_time_t * const p_time);
    
    static fsp_err_t r_rtc_alarm_time_and_date_validate(rtc_alarm_time_t * const p_time);
    
    static fsp_err_t r_rtc_alarm_time_validate(rtc_alarm_time_t * const p_time);
    
    static fsp_err_t r_rtc_alarm_month_and_year_validate(rtc_alarm_time_t * const p_time);
    
    static fsp_err_t r_rtc_alarm_dayofmonth_and_dayofweek_validate(rtc_alarm_time_t * const p_time);
    
    #endif
    
    static void r_rtc_error_adjustment_set(rtc_error_adjustment_cfg_t const * const err_adj_cfg);
    
    /*******************************************************************************************************************//**
     * @addtogroup RTC
     * @{
     **********************************************************************************************************************/
    
    /***********************************************************************************************************************
     * Functions
     **********************************************************************************************************************/
    
    /*******************************************************************************************************************//**
     * Opens and configures the RTC driver module. Implements @ref rtc_api_t::open.
     * Configuration includes clock source, and interrupt callback function.
     *
     * Example:
     * @snippet r_rtc_example.c R_RTC_Open
     *
     * @retval FSP_SUCCESS          Initialization was successful and RTC has started.
     * @retval FSP_ERR_ASSERTION    Invalid p_ctrl or p_cfg pointer.
     * @retval FSP_ERR_ALREADY_OPEN Module is already open.
     * @retval FSP_ERR_INVALID_ARGUMENT Invalid time parameter field.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_Open (rtc_ctrl_t * const p_ctrl, rtc_cfg_t const * const p_cfg, 
    bool bPOR)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
        fsp_err_t             err             = FSP_SUCCESS;
    
        /* Parameter checking */
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ASSERT(NULL != p_cfg);
        FSP_ERROR_RETURN(RTC_OPEN != p_instance_ctrl->open, FSP_ERR_ALREADY_OPEN);
    #endif
    
        /* Save the configuration  */
        p_instance_ctrl->p_cfg = p_cfg;
    
        p_instance_ctrl->p_callback        = p_cfg->p_callback;
        p_instance_ctrl->p_context         = p_cfg->p_context;
        p_instance_ctrl->p_callback_memory = NULL;
    
    #if RTC_CFG_PARAM_CHECKING_ENABLE
    
        /* Verify the frequency comparison value for RFRL when using LOCO */
        if (RTC_CLOCK_SOURCE_LOCO == p_cfg->clock_source)
        {
            FSP_ERROR_RETURN(FSP_SUCCESS != r_rtc_rfrl_validate(p_cfg->freq_compare_value_loco), FSP_ERR_INVALID_ARGUMENT);
        }
        /* Validate the error adjustment parameters when using SubClock */
        else
        {
            FSP_ERROR_RETURN(FSP_SUCCESS == r_rtc_err_adjustment_paramter_check(p_instance_ctrl->p_cfg->p_err_cfg),
                             FSP_ERR_INVALID_ARGUMENT);
        }
    #endif
    
        p_instance_ctrl->carry_isr_triggered = false;
    
        r_rtc_config_rtc_interrupts(p_instance_ctrl, p_cfg);
    
        /* Check to see if the previous reset was Power cycle, we need to initialize the source clock & count mode*/
        if (bPOR)
        {
          /* Set the clock source for RTC.
          * The count source must be selected only once before making the initial settings of the RTC registers
          * at power on. (see section 26.2.19 RTC Control Register 4 (RCR4) of the RA6M3 manual R01UH0886EJ0100)*/
          r_rtc_set_clock_source(p_instance_ctrl, p_cfg);
    
        }
    
        /** Mark driver as open by initializing it to "RTC" in its ASCII equivalent. */
        p_instance_ctrl->open = RTC_OPEN;
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Close the RTC driver.
     * Implements @ref rtc_api_t::close
     *
     * @retval FSP_SUCCESS          De-Initialization was successful and RTC driver closed.
     * @retval FSP_ERR_ASSERTION    Invalid p_ctrl.
     * @retval FSP_ERR_NOT_OPEN     Driver not open already for close.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_Close (rtc_ctrl_t * const p_ctrl)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    
        /* Parameter checking */
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
    #endif
    
        /* Clear PIE, AIE, CIE*/
        R_RTC->RCR1 = 0U;
    
        /* Set the START bit to 0 */
        r_rtc_start_bit_update(0U);
    
        if (p_instance_ctrl->p_cfg->periodic_irq >= 0)
        {
            R_BSP_IrqDisable(p_instance_ctrl->p_cfg->periodic_irq);
            R_FSP_IsrContextSet(p_instance_ctrl->p_cfg->periodic_irq, NULL);
        }
    
        if (p_instance_ctrl->p_cfg->alarm_irq >= 0)
        {
            R_BSP_IrqDisable(p_instance_ctrl->p_cfg->alarm_irq);
            R_FSP_IsrContextSet(p_instance_ctrl->p_cfg->alarm_irq, NULL);
        }
    
        if (p_instance_ctrl->p_cfg->carry_irq >= 0)
        {
            R_BSP_IrqDisable(p_instance_ctrl->p_cfg->carry_irq);
            R_FSP_IsrContextSet(p_instance_ctrl->p_cfg->carry_irq, NULL);
        }
    
        p_instance_ctrl->open = 0U;
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * Set the calendar time.
     *
     * Implements @ref rtc_api_t::calendarTimeSet.
     *
     * @retval FSP_SUCCESS              Calendar time set operation was successful.
     * @retval FSP_ERR_ASSERTION        Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN         Driver not open already for operation.
     * @retval FSP_ERR_INVALID_ARGUMENT Invalid time parameter field.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_CalendarTimeSet (rtc_ctrl_t * const p_ctrl, rtc_time_t * const p_time)
    {
        fsp_err_t             err             = FSP_SUCCESS;
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ASSERT(p_time);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
    
        /* Verify the seconds, minutes, hours, year ,day of the week, day of the month, month and year are valid values */
        FSP_ERROR_RETURN(FSP_SUCCESS == r_rtc_time_and_date_validate(p_time), FSP_ERR_INVALID_ARGUMENT);
    #else
        FSP_PARAMETER_NOT_USED(p_ctrl);
    #endif
    
        /* See section "26.3.3 Setting the Time" of the RA6M3 manual R01UH0886EJ0100 for steps to set the time and error
         * adjustment value */
    
        /* Set the START bit to 0 */
        r_rtc_start_bit_update(0U);
    
        /* Set the year, month, day of the week, ... */
        R_RTC->RSECCNT = rtc_dec_to_bcd((uint8_t) p_time->tm_sec);
        R_RTC->RMINCNT = rtc_dec_to_bcd((uint8_t) p_time->tm_min);
        R_RTC->RHRCNT  = rtc_dec_to_bcd((uint8_t) p_time->tm_hour) & RTC_RHRCNT_HOUR_MASK;
        R_RTC->RWKCNT  = rtc_dec_to_bcd((uint8_t) p_time->tm_wday);
        R_RTC->RDAYCNT = rtc_dec_to_bcd((uint8_t) p_time->tm_mday);
    
        /* Add one to match with HW register */
        R_RTC->RMONCNT = rtc_dec_to_bcd((uint8_t) (p_time->tm_mon + 1));
    
        /* Subtract 100 to match with HW register */
        R_RTC->RYRCNT = rtc_dec_to_bcd((uint8_t) (p_time->tm_year - RTC_C_TIME_OFFSET));
    
        if (RTC_CLOCK_SOURCE_SUBCLK == p_instance_ctrl->p_cfg->clock_source)
        {
            /* Set Error Adjustment values */
            r_rtc_error_adjustment_set(p_instance_ctrl->p_cfg->p_err_cfg);
        }
    
        /* Set the START bit to 1 */
        r_rtc_start_bit_update(1U);
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Get the calendar time.
     * @warning Do not call this function from a critical section or from an interrupt with higher priority than the carry
     * interrupt, or the time returned may be inaccurate.
     *
     * Implements @ref rtc_api_t::calendarTimeGet
     *
     * @retval FSP_SUCCESS          Calendar time get operation was successful.
     * @retval FSP_ERR_ASSERTION    Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN     Driver not open already for operation.
     * @retval FSP_ERR_IRQ_BSP_DISABLED User IRQ parameter not valid
     **********************************************************************************************************************/
    fsp_err_t R_RTC_CalendarTimeGet (rtc_ctrl_t * const p_ctrl, rtc_time_t * const p_time)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ASSERT(p_time);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
        FSP_ERROR_RETURN(p_instance_ctrl->p_cfg->carry_irq >= 0, FSP_ERR_IRQ_BSP_DISABLED);
    #else
        FSP_PARAMETER_NOT_USED(p_instance_ctrl);
    #endif
    
        fsp_err_t err = FSP_SUCCESS;
    
        uint32_t carry_irq_status = NVIC_GetEnableIRQ(p_instance_ctrl->p_cfg->carry_irq);
    
        if ((uint32_t) 0U == carry_irq_status)
        {
            r_rtc_irq_set(true, R_RTC_RCR1_CIE_Msk);
            R_BSP_IrqEnable(p_instance_ctrl->p_cfg->carry_irq);
        }
    
        /* If a carry occurs while the 64-Hz counter and time are being read, the correct time is not obtained,
         * therefore they must be read again. 26.3.5 "Reading 64-Hz Counter and Time" of the RA6M3 manual R01UH0886EJ0100)*/
        do
        {
            p_instance_ctrl->carry_isr_triggered = false; /** This flag will be set to 'true' in the carry ISR */
            p_time->tm_sec  = (int32_t) rtc_bcd_to_dec(R_RTC->RSECCNT);
            p_time->tm_min  = (int32_t) rtc_bcd_to_dec(R_RTC->RMINCNT);
            p_time->tm_hour = (int32_t) rtc_bcd_to_dec(R_RTC->RHRCNT & RTC_RHRCNT_HOUR_MASK);
            p_time->tm_wday = (int32_t) rtc_bcd_to_dec(R_RTC->RWKCNT);
            p_time->tm_mday = (int32_t) rtc_bcd_to_dec(R_RTC->RDAYCNT);
    
            /* Subtract one to match with C time.h standards */
            p_time->tm_mon = (int32_t) rtc_bcd_to_dec(R_RTC->RMONCNT) - 1;
    
            /* Add 100 to match with C time.h standards */
            p_time->tm_year = (int32_t) rtc_bcd_to_dec((uint8_t) R_RTC->RYRCNT) + RTC_C_TIME_OFFSET;
        } while (p_instance_ctrl->carry_isr_triggered);
    
        /** Restore the state of carry IRQ. */
        if ((uint32_t) 0U == carry_irq_status)
        {
            r_rtc_irq_set(false, R_RTC_RCR1_CIE_Msk);
    
            /* Disable this interrupt in the NVIC */
            R_BSP_IrqDisable(p_instance_ctrl->p_cfg->carry_irq);
        }
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Set the calendar alarm time.
     *
     * Implements @ref rtc_api_t::calendarAlarmSet.
     *
     * @pre The calendar counter must be running before the alarm can be set.
     *
     * @retval FSP_SUCCESS              Calendar alarm time set operation was successful.
     * @retval FSP_ERR_INVALID_ARGUMENT Invalid time parameter field.
     * @retval FSP_ERR_ASSERTION        Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN         Driver not open already for operation.
     * @retval FSP_ERR_IRQ_BSP_DISABLED User IRQ parameter not valid
     **********************************************************************************************************************/
    fsp_err_t R_RTC_CalendarAlarmSet (rtc_ctrl_t * const p_ctrl, rtc_alarm_time_t * const p_alarm)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
        fsp_err_t             err             = FSP_SUCCESS;
    
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ASSERT(p_alarm);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
        FSP_ERROR_RETURN(p_instance_ctrl->p_cfg->alarm_irq >= 0, FSP_ERR_IRQ_BSP_DISABLED);
    
        /* Verify the seconds, minutes, hours, year ,day of the week, day of the month and month are valid values */
        FSP_ERROR_RETURN(FSP_SUCCESS == r_rtc_alarm_time_and_date_validate(p_alarm), FSP_ERR_INVALID_ARGUMENT);
    #endif
    
        if (p_instance_ctrl->p_cfg->alarm_irq >= 0)
        {
            /* Disable the ICU alarm interrupt request */
            R_BSP_IrqDisable(p_instance_ctrl->p_cfg->alarm_irq);
        }
    
        /* Set alarm time */
        volatile uint8_t field;
        if (p_alarm->sec_match)
        {
            field = rtc_dec_to_bcd((uint8_t) p_alarm->time.tm_sec) | (uint8_t) (p_alarm->sec_match << RTC_COMPARE_ENB_BIT);
        }
        else
        {
            field = 0U;
        }
    
        R_RTC->RSECAR = field;
    
        if (p_alarm->min_match)
        {
            field = rtc_dec_to_bcd((uint8_t) p_alarm->time.tm_min) | (uint8_t) (p_alarm->min_match << RTC_COMPARE_ENB_BIT);
        }
        else
        {
            field = 0U;
        }
    
        R_RTC->RMINAR = field;
    
        if (p_alarm->hour_match)
        {
            field = rtc_dec_to_bcd((uint8_t) p_alarm->time.tm_hour) |
                    (uint8_t) (p_alarm->hour_match << RTC_COMPARE_ENB_BIT);
        }
        else
        {
            field = 0U;
        }
    
        R_RTC->RHRAR = field;
    
        if (p_alarm->dayofweek_match)
        {
            field = (uint8_t) p_alarm->time.tm_wday | (uint8_t) (p_alarm->dayofweek_match << RTC_COMPARE_ENB_BIT);
        }
        else
        {
            field = 0U;
        }
    
        R_RTC->RWKAR = field;
    
        if (p_alarm->mday_match)
        {
            field = rtc_dec_to_bcd((uint8_t) p_alarm->time.tm_mday) |
                    (uint8_t) (p_alarm->mday_match << RTC_COMPARE_ENB_BIT);
        }
        else
        {
            field = 1U;
        }
    
        R_RTC->RDAYAR = field;
    
        if (p_alarm->mon_match)
        {
            /* Add one to month to match with HW register */
            field = rtc_dec_to_bcd((uint8_t) (p_alarm->time.tm_mon + 1)) |
                    (uint8_t) (p_alarm->mon_match << RTC_COMPARE_ENB_BIT);
        }
        else
        {
            field = 0U;
        }
    
        R_RTC->RMONAR = field;
    
        if (p_alarm->year_match)
        {
            field = rtc_dec_to_bcd((uint8_t) (p_alarm->time.tm_year - RTC_C_TIME_OFFSET));
        }
        else
        {
            field = 0U;
        }
    
        R_RTC->RYRAR         = field;
        R_RTC->RYRAREN_b.ENB = (p_alarm->year_match);
    
        /* Enable the alarm interrupt */
        r_rtc_irq_set(true, R_RTC_RCR1_AIE_Msk);
    
        R_BSP_IrqEnable(p_instance_ctrl->p_cfg->alarm_irq);
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Get the calendar alarm time.
     *
     * Implements @ref rtc_api_t::calendarAlarmGet
     *
     * @retval FSP_SUCCESS           Calendar alarm time get operation was successful.
     * @retval FSP_ERR_ASSERTION     Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN      Driver not open already for operation.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_CalendarAlarmGet (rtc_ctrl_t * const p_ctrl, rtc_alarm_time_t * const p_alarm)
    {
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ASSERT(NULL != p_alarm);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
    #else
        FSP_PARAMETER_NOT_USED(p_ctrl);
    #endif
    
        p_alarm->time.tm_sec  = rtc_bcd_to_dec(R_RTC->RSECAR & RTC_MASK_8TH_BIT);
        p_alarm->time.tm_min  = rtc_bcd_to_dec(R_RTC->RMINAR & RTC_MASK_8TH_BIT);
        p_alarm->time.tm_hour = rtc_bcd_to_dec(R_RTC->RHRAR & RTC_MASK_8TH_BIT);
        p_alarm->time.tm_wday = rtc_bcd_to_dec(R_RTC->RWKAR & RTC_MASK_8TH_BIT);
        p_alarm->time.tm_mday = rtc_bcd_to_dec(R_RTC->RDAYAR & RTC_MASK_8TH_BIT);
    
        /* Subtract one from month to match with C time.h standards */
        p_alarm->time.tm_mon = rtc_bcd_to_dec(R_RTC->RMONAR & RTC_MASK_8TH_BIT) - (uint8_t) 1;
    
        /* Add 100 to the year to match with C time.h standards */
        p_alarm->time.tm_year = rtc_bcd_to_dec((uint8_t) R_RTC->RYRAR) + (uint8_t) RTC_C_TIME_OFFSET;
    
        p_alarm->sec_match       = (bool) R_RTC->RSECAR_b.ENB;
        p_alarm->min_match       = (bool) R_RTC->RMINAR_b.ENB;
        p_alarm->hour_match      = (bool) R_RTC->RHRAR_b.ENB;
        p_alarm->dayofweek_match = (bool) R_RTC->RWKAR_b.ENB;
        p_alarm->mday_match      = (bool) R_RTC->RDAYAR_b.ENB;
        p_alarm->mon_match       = (bool) R_RTC->RMONAR_b.ENB;
        p_alarm->year_match      = (bool) R_RTC->RYRAREN_b.ENB;
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * Set the periodic interrupt rate and enable periodic interrupt.
     *
     * Implements @ref rtc_api_t::periodicIrqRateSet
     *
     * @note To start the RTC @ref R_RTC_CalendarTimeSet must be called at least once.
     *
     * Example:
     * @snippet r_rtc_example.c R_RTC_PeriodicIrqRateSet
     *
     * @retval FSP_SUCCESS               The periodic interrupt rate was successfully set.
     * @retval FSP_ERR_ASSERTION         Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN          Driver not open already for operation.
     * @retval FSP_ERR_IRQ_BSP_DISABLED  User IRQ parameter not valid
     **********************************************************************************************************************/
    fsp_err_t R_RTC_PeriodicIrqRateSet (rtc_ctrl_t * const p_ctrl, rtc_periodic_irq_select_t const rate)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
        FSP_ERROR_RETURN(p_instance_ctrl->p_cfg->periodic_irq >= 0, FSP_ERR_IRQ_BSP_DISABLED);
    #endif
        fsp_err_t err = FSP_SUCCESS;
    
        uint8_t rcr1 = R_RTC->RCR1;
        rcr1       &= (uint8_t) ~R_RTC_RCR1_PES_Msk;
        R_RTC->RCR1 = (uint8_t) (rcr1 | (rate << R_RTC_RCR1_PES_Pos));
    
        /* When the RCR1 register is modified, check that all the bits are updated before proceeding
         * (see section 26.2.17 "RTC Control Register 1 (RCR1)" of the RA6M3 manual R01UH0886EJ0100)*/
        FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR1 >> R_RTC_RCR1_PES_Pos, rate);
    
        r_rtc_irq_set(true, R_RTC_RCR1_PIE_Msk);
    
        R_BSP_IrqEnable(p_instance_ctrl->p_cfg->periodic_irq);
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Set RTC clock source and running status information ad store it in provided pointer p_rtc_info
     *
     * Implements @ref rtc_api_t::infoGet
     *
     * @retval FSP_SUCCESS          Get information Successful.
     * @retval FSP_ERR_ASSERTION    Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN     Driver not open already for operation.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_InfoGet (rtc_ctrl_t * const p_ctrl, rtc_info_t * const p_rtc_info)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(NULL != p_instance_ctrl);
        FSP_ASSERT(NULL != p_rtc_info);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
    #endif
    
        p_rtc_info->clock_source = p_instance_ctrl->p_cfg->clock_source;
        p_rtc_info->status       = (rtc_status_t) R_RTC->RCR2_b.START;
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * This function sets time error adjustment
     *
     * Implements @ref rtc_api_t::errorAdjustmentSet
     *
     * @retval FSP_SUCCESS                 Time error adjustment successful.
     * @retval FSP_ERR_ASSERTION           Invalid input argument.
     * @retval FSP_ERR_NOT_OPEN            Driver not open for operation.
     * @retval FSP_ERR_UNSUPPORTED         The clock source is not sub-clock.
     * @retval FSP_ERR_INVALID_ARGUMENT    Invalid error adjustment value.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_ErrorAdjustmentSet (rtc_ctrl_t * const p_ctrl, rtc_error_adjustment_cfg_t const * const err_adj_cfg)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    #if RTC_CFG_PARAM_CHECKING_ENABLE
        FSP_ASSERT(p_ctrl);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
    
        /* Error adjustment is supported only if clock source is sub-clock */
        if (p_instance_ctrl->p_cfg->clock_source != RTC_CLOCK_SOURCE_SUBCLK)
        {
            return FSP_ERR_UNSUPPORTED;
        }
    
        /* Verify the frequecy comparison valure for RFRL when using LOCO */
        FSP_ERROR_RETURN(FSP_SUCCESS == r_rtc_err_adjustment_paramter_check(err_adj_cfg), FSP_ERR_INVALID_ARGUMENT);
    #else
        FSP_PARAMETER_NOT_USED(p_instance_ctrl);
    #endif
    
        /* Set Error Adjustment values */
        r_rtc_error_adjustment_set(err_adj_cfg);
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * Updates the user callback and has option of providing memory for callback structure.
     * Implements rtc_api_t::callbackSet
     *
     * @retval  FSP_SUCCESS                  Baud rate was successfully changed.
     * @retval  FSP_ERR_ASSERTION            Pointer to RTC control block is NULL or the RTC is not configured to use the
     *                                       internal clock.
     * @retval  FSP_ERR_NOT_OPEN             The control block has not been opened
     * @retval  FSP_ERR_NO_CALLBACK_MEMORY   p_callback is non-secure and p_callback_memory is either secure or NULL.
     **********************************************************************************************************************/
    fsp_err_t R_RTC_CallbackSet (rtc_ctrl_t * const          p_ctrl,
                                 void (                    * p_callback)(rtc_callback_args_t *),
                                 void const * const          p_context,
                                 rtc_callback_args_t * const p_callback_memory)
    {
        rtc_instance_ctrl_t * p_instance_ctrl = (rtc_instance_ctrl_t *) p_ctrl;
    
    #if (RTC_CFG_PARAM_CHECKING_ENABLE)
        FSP_ASSERT(p_instance_ctrl);
        FSP_ASSERT(p_callback);
        FSP_ERROR_RETURN(RTC_OPEN == p_instance_ctrl->open, FSP_ERR_NOT_OPEN);
    #endif
    
        /* Store callback and context */
    
    #if BSP_TZ_SECURE_BUILD
    
        /* Get security state of p_callback */
        bool callback_is_secure =
            (NULL == cmse_check_address_range((void *) p_callback, sizeof(void *), CMSE_AU_NONSECURE));
    
     #if RTC_CFG_PARAM_CHECKING_ENABLE
    
        /* In secure projects, p_callback_memory must be provided in non-secure space if p_callback is non-secure */
        rtc_callback_args_t * const p_callback_memory_checked = cmse_check_pointed_object(p_callback_memory,
                                                                                          CMSE_AU_NONSECURE);
        FSP_ERROR_RETURN(callback_is_secure || (NULL != p_callback_memory_checked), FSP_ERR_NO_CALLBACK_MEMORY);
     #endif
    #endif
    
        /* Store callback and context */
    #if BSP_TZ_SECURE_BUILD
        p_instance_ctrl->p_callback = callback_is_secure ? p_callback :
                                      (void (*)(rtc_callback_args_t *))cmse_nsfptr_create(p_callback);
    #else
        p_instance_ctrl->p_callback = p_callback;
    #endif
        p_instance_ctrl->p_context         = p_context;
        p_instance_ctrl->p_callback_memory = p_callback_memory;
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * @} (end addtpgroup RTC)
     **********************************************************************************************************************/
    
    /***********************************************************************************************************************
     * Private Functions
     **********************************************************************************************************************/
    
    /*******************************************************************************************************************//**
     * Update the start bit
     *
     * @param[in]  value         Value to be updated
     **********************************************************************************************************************/
    static void r_rtc_start_bit_update (uint8_t value)
    {
        /* Set or Clear START bit in RCR2 register depending on the value */
        R_RTC->RCR2_b.START = value & 1U;
    
        /* The START bit is updated in synchronization with the next cycle of the count source. Check if the bit is updated
         * before proceeding (see section 26.2.18 "RTC Control Register 2 (RCR2)" of the RA6M3 manual R01UH0886EJ0100)*/
        FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.START, value);
    }
    
    /*******************************************************************************************************************//**
     * Perform a software reset
     **********************************************************************************************************************/
    static void r_rtc_software_reset (void)
    {
        /* Set the RESET bit in the RCR2 register */
        R_RTC->RCR2_b.RESET = 1U;
    
        /* When 1 is written to this bit, initialization starts in synchronization with the count source. When the
         * initialization is completed, the RESET bit is automatically set to 0. Check that this bit is 0 before proceeding.
         * (see section 26.2.18 "RTC Control Register 2 (RCR2)" of the RA6M3 manual R01UH0886EJ0100)*/
        FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.RESET, 0U);
    }
    
    /*******************************************************************************************************************//**
     * Set the RTC clock source
     *
     * @param[in]  p_ctrl                  Instance control block
     * @param[in]  p_cfg                   Pointer to rtc configuration.
     **********************************************************************************************************************/
    static void r_rtc_set_clock_source (rtc_instance_ctrl_t * const p_ctrl, rtc_cfg_t const * const p_cfg)
    {
        /* Select the count source (RCKSEL) */
        R_RTC->RCR4 = (uint8_t) p_ctrl->p_cfg->clock_source;
    
        /* Supply 6 clocks of the count source (LOCO, 183us, 32kHZ).
         * See 26.3.2 "Clock and Count Mode Setting Procedure" of the RA6M3 manual R01UH0886EJ0100)*/
        if (RTC_CLOCK_SOURCE_SUBCLK == p_ctrl->p_cfg->clock_source)
        {
            R_BSP_SoftwareDelay(RTC_SUB_CLK_STABLIZATION_TIME_MS, BSP_DELAY_UNITS_MILLISECONDS);
        }
        else
        {
            R_BSP_SoftwareDelay(RTC_LOCO_STABLIZATION_TIME_US, BSP_DELAY_UNITS_MICROSECONDS);
        }
    
        /* Set the START bit to 0 */
        r_rtc_start_bit_update(0U);
    
        /* Initialize registers. */
        R_RTC->RCR1 = 0U;
        R_RTC->RCR2 = 0U;
    
    
        /* Force RTC to 24 hour mode. Set HR24 bit in the RCR2 register */
        R_RTC->RCR2_b.HR24 = 1U;
    
        if (RTC_CLOCK_SOURCE_LOCO == p_ctrl->p_cfg->clock_source)
        {
            /* Write 0 before writing to the RFRL register after a cold start. (see section 26.2.20
             * Frequency Register (RFRH/RFRL)" of the RA6M3 manual R01UH0886EJ0100) */
            R_RTC->RFRH = 0;
    
            R_RTC->RFRL = (uint16_t) p_cfg->freq_compare_value_loco;
        }
    
        /* Clear the the CNTMD bit in the RCR2 register */
        R_RTC->RCR2_b.CNTMD = 0U;
    
        /* Wait for the CNTMD bit to become 0 */
    
        /* When setting the count mode, execute an RTC software reset and start again from the initial settings.
         * This bit is updated synchronously with the count source, and its value is fixed before the RTC software
         * reset is completed (see section 26.2.18 "RTC Control Register 2 (RCR2)" of the RA6M3 manual R01UH0886EJ0100)*/
        FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.CNTMD, RTC_CALENDAR_MODE);
    
        /* Execute RTC software reset */
        r_rtc_software_reset();
    }
    
    /*******************************************************************************************************************//**
     * Set IRQ priority and control info for IRQ handler .
     *
     * @param[in]  p_ctrl                  Instance control block
     * @param[in]  p_cfg                   Pointer to rtc configuration.
     **********************************************************************************************************************/
    static void r_rtc_config_rtc_interrupts (rtc_instance_ctrl_t * const p_ctrl, rtc_cfg_t const * const p_cfg)
    {
        if (p_cfg->periodic_irq >= 0)
        {
            R_BSP_IrqCfg(p_cfg->periodic_irq, p_cfg->periodic_ipl, p_ctrl);
        }
    
        if (p_cfg->alarm_irq >= 0)
        {
            R_BSP_IrqCfg(p_cfg->alarm_irq, p_cfg->alarm_ipl, p_ctrl);
        }
    
        if (p_cfg->carry_irq >= 0)
        {
            R_BSP_IrqCfg(p_cfg->carry_irq, p_cfg->carry_ipl, p_ctrl);
        }
    }
    
    /*******************************************************************************************************************//**
     * Helper function to enable or disable the Alarm/ Periodic/ Carry interrupt
     *
     * @param[in]  irq_enable_flag         Interrupt enable
     * @param[in]  mask                    Mask for the corresponding interrupt enable bit in RCR1
     **********************************************************************************************************************/
    static void r_rtc_irq_set (bool irq_enable_flag, uint8_t mask)
    {
        /* Enable the RTC carry interrupt request */
        if (irq_enable_flag)
        {
            /* Set the Interrupt Enable in RCR1 */
            R_RTC->RCR1 |= mask;
    
            /* When the RCR1 register is modified, check that all the bits are updated before proceeding
             * (see section 26.2.17 "RTC Control Register 1 (RCR1)" of the RA6M3 manual R01UH0886EJ0100)*/
            FSP_HARDWARE_REGISTER_WAIT((R_RTC->RCR1 & mask), mask);
        }
        else
        {
            /* Clear the Interrupt Enable in RCR1 */
            R_RTC->RCR1 &= (uint8_t) ~mask;
    
            FSP_HARDWARE_REGISTER_WAIT((R_RTC->RCR1 & mask), 0U);
        }
    }
    
    /*******************************************************************************************************************//**
     * Calls user callback.
     *
     * @param[in]     p_ctrl     Pointer to RTC instance control block
     * @param[in]     event      Event code
     **********************************************************************************************************************/
    static void r_rtc_call_callback (rtc_instance_ctrl_t * p_ctrl, rtc_event_t event)
    {
        rtc_callback_args_t args;
    
        /* Store callback arguments in memory provided by user if available.  This allows callback arguments to be
         * stored in non-secure memory so they can be accessed by a non-secure callback function. */
        rtc_callback_args_t * p_args = p_ctrl->p_callback_memory;
        if (NULL == p_args)
        {
            /* Store on stack */
            p_args = &args;
        }
        else
        {
            /* Save current arguments on the stack in case this is a nested interrupt. */
            args = *p_args;
        }
    
        p_args->event     = event;
        p_args->p_context = p_ctrl->p_context;
    
    #if BSP_TZ_SECURE_BUILD
    
        /* p_callback can point to a secure function or a non-secure function. */
        if (!cmse_is_nsfptr(p_ctrl->p_callback))
        {
            /* If p_callback is secure, then the project does not need to change security state. */
            p_ctrl->p_callback(p_args);
        }
        else
        {
            /* If p_callback is Non-secure, then the project must change to Non-secure state in order to call the callback. */
            rtc_prv_ns_callback p_callback = (rtc_prv_ns_callback) (p_ctrl->p_callback);
            p_callback(p_args);
        }
    
    #else
    
        /* If the project is not Trustzone Secure, then it will never need to change security state in order to call the callback. */
        p_ctrl->p_callback(p_args);
    #endif
        if (NULL != p_ctrl->p_callback_memory)
        {
            /* Restore callback memory in case this is a nested interrupt. */
            *p_ctrl->p_callback_memory = args;
        }
    }
    
    #if RTC_CFG_PARAM_CHECKING_ENABLE
    
    /*******************************************************************************************************************//**
     * Validate RFRL value for LOCO
     *
     * @param[in]  value                      Frequency Comparision Value
     * @retval FSP_SUCCESS                    validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_rfrl_validate (uint32_t value)
    {
        fsp_err_t err;
        err = FSP_SUCCESS;
    
        /* A value from 0007h through 01FFh can be specified as the frequency comparison value (see section 26.2.20
         * Frequency Register (RFRH/RFRL)" of the RA6M3 manual R01UH0886EJ0100) */
        if ((RTC_RFRL_MIN_VALUE_LOCO <= value) &&
            (RTC_RFRL_MAX_VALUE_LOCO >= value))
        {
            err = FSP_ERR_INVALID_ARGUMENT;
        }
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Validate Error Adjustment configuration when using SubClock
     *
     * @param[in]  err_adj_cfg             Pointer to error adjustment config
     * @retval FSP_SUCCESS                 Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT    Invalid error configuration
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_err_adjustment_paramter_check (rtc_error_adjustment_cfg_t const * const err_adj_cfg)
    {
        rtc_error_adjustment_mode_t   mode   = err_adj_cfg->adjustment_mode;
        rtc_error_adjustment_period_t period = err_adj_cfg->adjustment_period;
        uint32_t value = err_adj_cfg->adjustment_value;
    
        /* Validate adjustment mode and period */
        if (RTC_ERROR_ADJUSTMENT_MODE_AUTOMATIC == mode)
        {
            if (RTC_ERROR_ADJUSTMENT_PERIOD_NONE == period)
            {
                return FSP_ERR_INVALID_ARGUMENT;
            }
        }
    
        /* Validate adjustment value */
        if (value > RTC_MAX_ERROR_ADJUSTMENT_VALUE)
        {
            return FSP_ERR_INVALID_ARGUMENT;
        }
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * Validate time and date fields of time parameter fields
     * Checking for seconds, minutes, hours are valid values by calling sub-function time validate.
     * Checking for year, month, day of the week and day of a month are valid values by calling sub-function
     * date validate.
     *
     * @param[in]  p_time                     Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_time_and_date_validate (rtc_time_t * const p_time)
    {
        fsp_err_t err = FSP_SUCCESS;
        err = r_rtc_time_validate(p_time);
        FSP_ERROR_RETURN(err == FSP_SUCCESS, err);
        err = r_rtc_date_validate(p_time);
        FSP_ERROR_RETURN(err == FSP_SUCCESS, err);
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * Validate time fields of time type parameter
     * Checking for the seconds, minutes, hours values for valid specified range.
     * Seconds 0 to 59.
     * Minutes 0 to 59.
     * Hours   0 to 23.
     *
     * @param[in]  p_time                      Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_time_validate (rtc_time_t * p_time)
    {
        fsp_err_t err;
        err = FSP_SUCCESS;
        if ((p_time->tm_sec < 0) || (p_time->tm_sec > RTC_SECONDS_IN_A_MINUTE) ||
            (p_time->tm_min < 0) || (p_time->tm_min > RTC_MINUTES_IN_A_HOUR) ||
            (p_time->tm_hour < 0) || (p_time->tm_hour > RTC_HOURS_IN_A_DAY))
        {
            err = FSP_ERR_INVALID_ARGUMENT;
        }
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Validate date fields of time type parameter
     * validating r_rtc date fields and setting day of a Week using Zeller's congruence.
     * Checking for year, month, day of the week and day of a month are valid values.
     * Leap year validation and Week of the day is calculated and updated in rtc time.
     * Day of week between 0 to 6
     * Day between 1 to 31
     * Month between 0 to 11 as per standard time.h, There's a mismatch between hardware configuration,
     * UM indicates that "A value from 01 through 12 (in BCD) can be specified" for Month Counter register in the RTC.
     * This difference will be taken care in the Set and Get functions.
     *
     * As per HW manual, value of Year is between 0 to 99, the RTC has a 100 year calendar from 2000 to 2099.
     * (see section 26.1 "Overview" of the RA6M3 manual R01UH0886EJ0100)
     * But as per C standards, tm_year is years since 1900.
     * A sample year set in an application would be like time.tm_year = 2019-1900; (to set year 2019)
     * Since RTC API follows the Date and time structure defined in C standard library <time.h>, the valid value of year is
     * between 100 and 199, which will be internally converted to HW required value.
     *
     * @param[in]  p_time                     Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_date_validate (rtc_time_t * const p_time)
    {
        uint32_t day_of_week;
        uint32_t num_days_month;
        uint32_t day_of_a_month;
        uint32_t temp_month;
        uint32_t temp_year;
    
        day_of_a_month = (uint32_t) p_time->tm_mday;
        temp_month     = (uint32_t) (p_time->tm_mon + RTC_TIME_H_MONTH_OFFSET);
    
        /* The valid value of year is between 100 to 199, The RTC has a 100 year calendar from 2000 to 2099
         * to match the starting year 2000, a sample year offset(1900) is added like 117 + 1900 = 2017*/
        temp_year = (uint32_t) (p_time->tm_year + RTC_TIME_H_YEAR_OFFSET);
    
        /* Checking the error condition for year and months values, here valid value of year is between 100 to 199
         * and for month 0 to 11*/
        if ((p_time->tm_year < RTC_YEAR_VALUE_MIN) || (p_time->tm_year > RTC_YEAR_VALUE_MAX) ||
            (p_time->tm_mon < 0) || (p_time->tm_mon > RTC_MONTHS_IN_A_YEAR))
        {
            return FSP_ERR_INVALID_ARGUMENT;
        }
    
        /*For particular valid month, number of days in a month is updated */
        num_days_month = days_in_months[p_time->tm_mon];
    
        /* Checking for February month and Conditions for Leap year : Every fourth year is a leap year,
         * The RTC has a 100 year calendar from 2000 to 2099  */
        if ((RTC_FEBRUARY_MONTH == temp_month) && ((temp_year % 4U) == 0))
        {
            num_days_month = RTC_LAST_DAY_OF_LEAP_FEB_MONTH;
        }
    
        /* Checking for day of a month values for valid range */
        if ((p_time->tm_mday >= RTC_FIRST_DAY_OF_A_MONTH) && (day_of_a_month <= num_days_month))
        {
            /* Adjust month to run from 3 to 14 for March to February */
            if (temp_month < RTC_MARCH_MONTH)
            {
                temp_month = (temp_month + 12U);
    
                /* Adjust year if January or February*/
                --temp_year;
            }
    
            /*For the Gregorian calendar, Zeller's congruence formulas is
             * h = ( q + [13(m+1)/5] + Y + [Y/4] - [Y/100] + [Y/400])mod 7 (mod : modulo)
             * h is the day of the week , q is the day of the month,
             * m is the month (3 = March, 4 = April,..., 14 = February)
             * Y is year, which is Y - 1 during January and February */
            day_of_week = (uint32_t) p_time->tm_mday + ((13 * (temp_month + 1)) / 5) + temp_year + (temp_year / 4);
            day_of_week = (day_of_week - RTC_ZELLER_ALGM_CONST_FIFTEEN) % 7;
    
            /* Day of week between 0 to 6 :- Sunday to Saturday */
            /* d = (h + 6)mod 7 (mod : modulo) */
            p_time->tm_wday = (int16_t) ((day_of_week + 6U) % 7U);
    
            return FSP_SUCCESS;
        }
    
        return FSP_ERR_INVALID_ARGUMENT;
    }
    
    /*******************************************************************************************************************//**
     * Validate alarm time and date of Alarm time type parameter
     * Checking for alarm enable bit with the seconds, minutes, hours are valid values.
     * Checking for alarm enable bit with year, month, day of the week and day of a month are valid values.
     * If alarm enable bit is set for year, month, and day of a month for valid range, Week of the day is
     * calculated and updated in alarm time.
     *
     * @param[in]  p_time                     Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_alarm_time_and_date_validate (rtc_alarm_time_t * const p_time)
    {
        fsp_err_t err = FSP_SUCCESS;
        err = r_rtc_alarm_time_validate(p_time);
        FSP_ERROR_RETURN(err == FSP_SUCCESS, err);
    
        /* Checking for alarm enable bit for year, month, day of the month */
        if ((p_time->year_match) && (p_time->mon_match) && (p_time->mday_match))
        {
            err = r_rtc_date_validate(&p_time->time);
            FSP_ERROR_RETURN(err == FSP_SUCCESS, err);
        }
        else
        {
            err = r_rtc_alarm_month_and_year_validate(p_time);
            FSP_ERROR_RETURN(err == FSP_SUCCESS, err);
            err = r_rtc_alarm_dayofmonth_and_dayofweek_validate(p_time);
            FSP_ERROR_RETURN(err == FSP_SUCCESS, err);
        }
    
        return FSP_SUCCESS;
    }
    
    /*******************************************************************************************************************//**
     * Validate alarm time fields of Alarm time type parameter
     * Checking for alarm enable bit with the seconds, minutes, hours value for valid specified range.
     * Seconds 0 to 59.
     * Minutes 0 to 59.
     * Hours   0 to 23.
     *
     * @param[in]  p_time                     Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_alarm_time_validate (rtc_alarm_time_t * const p_time)
    {
        fsp_err_t err;
        err = FSP_SUCCESS;
        if (((p_time->sec_match) &&
             ((p_time->time.tm_sec < 0) || (p_time->time.tm_sec > RTC_SECONDS_IN_A_MINUTE))) ||
            ((p_time->min_match) &&
             ((p_time->time.tm_min < 0) || (p_time->time.tm_min > RTC_MINUTES_IN_A_HOUR))) ||
            ((p_time->hour_match) &&
             ((p_time->time.tm_hour < 0) || (p_time->time.tm_hour > RTC_HOURS_IN_A_DAY))))
        {
            err = FSP_ERR_INVALID_ARGUMENT;
        }
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Validate alarm month and year of time type parameter
     * Checking for alarm enable bit with month and year value for valid specified range.
     * Month : 0 to 11.
     * Year  : 100 to 199.
     * Since RTC API follows the Date and time structure defined in C standard library <time.h>, the valid value of year is
     * between 100 to 199.
     *
     * @param[in]  p_time                     Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_alarm_month_and_year_validate (rtc_alarm_time_t * const p_time)
    {
        fsp_err_t err;
        err = FSP_SUCCESS;
        if (((p_time->mon_match) &&
             ((p_time->time.tm_mon < 0) || (p_time->time.tm_mon > RTC_MONTHS_IN_A_YEAR))) ||
            ((p_time->year_match) &&
             ((p_time->time.tm_year < RTC_YEAR_VALUE_MIN) || (p_time->time.tm_year > RTC_YEAR_VALUE_MAX))))
        {
            err = FSP_ERR_INVALID_ARGUMENT;
        }
    
        return err;
    }
    
    /*******************************************************************************************************************//**
     * Validate alarm day of a month and day of the week of time type parameter
     * Checking for alarm enable bit with day of a month and day of the week values for valid specified range.
     * Day of a month  : 1 to 31.
     * Day of the week : 0 to 6.
     * If alarm enable bit is set for particular valid month, number of days in a month is updated from that particular
     * month, by default 31 days in a month and for February month days are considered as 29 days in a month.
     *
     * @param[in]  p_time                     Pointer to rtc_time_t
     * @retval FSP_SUCCESS                    Validation successful
     * @retval FSP_ERR_INVALID_ARGUMENT       Invalid field in rtc_time_t structure
     **********************************************************************************************************************/
    static fsp_err_t r_rtc_alarm_dayofmonth_and_dayofweek_validate (rtc_alarm_time_t * const p_time)
    {
        fsp_err_t err;
        uint8_t   num_days_month;
        uint8_t   day_of_a_month;
    
        day_of_a_month = (uint8_t) p_time->time.tm_mday;
        err            = FSP_SUCCESS;
    
        /* checking for alarm enable bit of valid month */
        if (p_time->mon_match)
        {
            /* Checking condition for February month in time.h months start from 0 to 11, for February 1 */
            if ((RTC_FEBRUARY_MONTH - 1U) == p_time->time.tm_mon)
            {
                /*For February month, number of days can be 28 for regular year and 29 for leap year.
                 * Hence consider 29 days for February.*/
                num_days_month = (uint8_t) RTC_LAST_DAY_OF_LEAP_FEB_MONTH;
            }
            else
            {
                /* For valid month, number of days in month is assigned*/
                num_days_month = days_in_months[p_time->time.tm_mon];
            }
        }
        else
        {
            /* default 31 days in a month*/
            num_days_month = (uint8_t) RTC_LAST_DAY_OF_A_MONTH;
        }
    
        if (((p_time->mday_match) &&
             ((p_time->time.tm_mday < RTC_FIRST_DAY_OF_A_MONTH) || (day_of_a_month > num_days_month))) ||
            ((p_time->dayofweek_match) &&
             ((p_time->time.tm_wday < 0) || (p_time->time.tm_wday > RTC_DAYS_IN_A_WEEK))))
        {
            err = FSP_ERR_INVALID_ARGUMENT;
        }
    
        return err;
    }
    
    #endif
    
    /*******************************************************************************************************************//**
     * This function sets time error adjustment mode, period, type and value.
     *
     *@param[in] err_adj_cfg  Pointer to the Error Adjustment Configuration
     **********************************************************************************************************************/
    static void r_rtc_error_adjustment_set (rtc_error_adjustment_cfg_t const * const err_adj_cfg)
    {
        uint8_t error_adjustment = 0;
    
        rtc_error_adjustment_mode_t   mode   = err_adj_cfg->adjustment_mode;
        rtc_error_adjustment_period_t period = err_adj_cfg->adjustment_period;
        rtc_error_adjustment_t        type   = err_adj_cfg->adjustment_type;
        uint32_t value = err_adj_cfg->adjustment_value;
    
        /* Check if mode change is required */
        if (mode != R_RTC->RCR2_b.AADJE)
        {
            /* Clear error adjustment before configuring the error adjustment mode
             * (see section "26.3.8.3 Procedure for changing the mode of adjustment" of the RA6M3 manual R01UH0886EJ0100) */
            R_RTC->RADJ = 0U;
    
            /* When RADJ is modified, check that all the bits are updated before continuing with more processing.
             * (see section 26.2.21 "Time Error Adjustment Register (RADJ)" of the RA6M3 manual R01UH0886EJ0100) */
            FSP_HARDWARE_REGISTER_WAIT(R_RTC->RADJ, 0U);
    
            /* Set the error adjustment enable, 1: Enable Automatic adjsutment 0: Disable Automatic adjsutment */
            R_RTC->RCR2_b.AADJE = (uint8_t) mode & 1U;
            FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.AADJE, mode);
        }
    
        /* Set the period if mode is Automatic adjustment */
        if (RTC_ERROR_ADJUSTMENT_MODE_AUTOMATIC == mode)
        {
            /* Check if period change is required */
            if (period != R_RTC->RCR2_b.AADJP)
            {
                /* Set time error adjustment period */
                R_RTC->RCR2_b.AADJP = (uint8_t) (period & 1U);
    
                /* When RCR2 is modified, check that all the bits are updated before continuing with more processing.
                 * (see section 26.2.18 "RTC Control Register 2 (RCR2) of the RA6M3 manual R01UH0886EJ0100) */
                FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.AADJP, period);
            }
        }
    
        error_adjustment = (uint8_t) ((uint8_t) (((uint8_t) type) << 6U) |
                                      (RTC_MAX_ERROR_ADJUSTMENT_VALUE & value));
        R_RTC->RADJ = error_adjustment;
    
        /* When RADJ is modified, check that all the bits are updated before continuing with more processing.
         * (see section 26.2.21 "Time Error Adjustment Register (RADJ)" of the RA6M3 manual R01UH0886EJ0100) */
        FSP_HARDWARE_REGISTER_WAIT(R_RTC->RADJ, error_adjustment);
    }
    
    /*******************************************************************************************************************//**
     * RTC Callback ISR for alarm and periodic interrupt.
     *
     * Saves context if RTOS is used, stops the timer if one-shot mode, clears interrupts, calls callback if one was
     * provided in the open function, and restores context if RTOS is used.
     **********************************************************************************************************************/
    
    void rtc_alarm_periodic_isr (void)
    {
        /* Save context if RTOS is used */
        FSP_CONTEXT_SAVE;
    
        IRQn_Type             irq    = R_FSP_CurrentIrqGet();
        rtc_instance_ctrl_t * p_ctrl = (rtc_instance_ctrl_t *) R_FSP_IsrContextGet(irq);
    
        /* Call the callback routine if one is available */
        if (NULL != p_ctrl->p_callback)
        {
            /* Set data to identify callback to user, then call user callback. */
            rtc_event_t event;
            if (irq == p_ctrl->p_cfg->alarm_irq)
            {
                event = RTC_EVENT_ALARM_IRQ;
            }
            else
            {
                event = RTC_EVENT_PERIODIC_IRQ;
            }
    
            /* Call callback */
            r_rtc_call_callback(p_ctrl, event);
        }
    
        /* Clear the IR flag in the ICU */
        R_BSP_IrqStatusClear(irq);
    
        /* Restore context if RTOS is used */
        FSP_CONTEXT_RESTORE;
    }
    
    /*******************************************************************************************************************//**
     * RTC Carry ISR.
     *
     * Saves context if RTOS is used, clears interrupts, calls callback if one was
     * provided in the open function, and restores context if RTOS is used.
     **********************************************************************************************************************/
    void rtc_carry_isr (void)
    {
        /* Save context if RTOS is used */
        FSP_CONTEXT_SAVE;
    
        IRQn_Type             irq    = R_FSP_CurrentIrqGet();
        rtc_instance_ctrl_t * p_ctrl = (rtc_instance_ctrl_t *) R_FSP_IsrContextGet(irq);
    
        p_ctrl->carry_isr_triggered = true;
    
        /* Clear the IR flag in the ICU */
        R_BSP_IrqStatusClear(irq);
    
        /* Restore context if RTOS is used */
        FSP_CONTEXT_RESTORE;
    }
    
    /*******************************************************************************************************************//**
     * Convert decimal to BCD
     *
     * @param[in] to_convert   Decimal Value to be converted
     **********************************************************************************************************************/
    static uint8_t rtc_dec_to_bcd (uint8_t to_convert)
    {
        return (uint8_t) ((((to_convert / (uint8_t) 10) << 4) & (uint8_t) RTC_MASK_LSB) | (to_convert % (uint8_t) 10));
    }
    
    /*******************************************************************************************************************//**
     * Convert  BCD to decimal
     *
     * @param[in] to_convert   BCD Value to be converted
     **********************************************************************************************************************/
    static uint8_t rtc_bcd_to_dec (uint8_t to_convert)
    {
        return (uint8_t) ((((to_convert & (uint8_t) RTC_MASK_LSB) >> 4) * (uint8_t) 10) +
                          (to_convert & (uint8_t) RTC_MASK_MSB));
    }
    

    Here are the code diff between the r_rtc.c in FSP 3.5.0 and our version:

  • The issue where "the time resets to 12:00 AM within one hour after setting the time" appears to occur randomly - it happens occasionally but not consistently.

    In contrast, the issue where "the time resets to 12:00 AM exactly 12 hours after setting the time" is consistent and occurs every time.

  • Hello Pilot,

    Thank you for reaching out to Renesas! I would suggest you use the latest FSP version 5.7.0 for better performance. You can add the latest FSP version in the existing e2 studio, as you do not need to reinstall the e2 studio. Also, could you please share your clock and configuration settings of RTC stack. Thank you!

    Kind regards,

    Payodhi

  • Hi Payodhi,

    Thanks for your response. We'll consider to upgrade the FSP in future. For now, we'll have to use this FSP 3.5.0. Was there any issue on RTC in FSP 3.5.0 as you know of?

    Here is the clock configuration and the RTC stack configuration:

    Thanks.

Reply Children
  • If I set time to the afternoon time, e.g, 1:57PM, the time will reset to 12AM when it should be 2PM.

    If I set time to the morning time, e.g, 10:58AM, the time will be 11AM soon - there is no time reset.

    It seems this issue is related to the 12 hours/24 hours, or AM/PM. I wonder if there is any setting in the RTC driver relates to the 12 hours/24 hours or AM/PM.

    Any clues? Thanks.

  • I figured it out by porting some of the RTC driver 4.4.0 to our existing FSP 3.5.0. After that, it seems working by setting the 24 horus mode. 

    Here is the code I added:

    static void r_rtc_set_clock_source (rtc_instance_ctrl_t * const p_ctrl, rtc_cfg_t const * const p_cfg)
    {
    . . .
        /* Execute RTC software reset */
        r_rtc_software_reset();
    
        /* Disable RTC interrupts */
        R_RTC->RCR1 = 0;
    
        /* Force RTC to 24 hour mode. Set HR24 bit in the RCR2 register */
        R_RTC->RCR2_b.HR24 = 1U;
    
        /*
         * See 23.6.5 "Notes on Writing to and Reading from Registers" of the RA6M5 manual R01UH0891EJ0120.
         * The value written is reflected when fourth read operations are performed after writing.
         */
        FSP_HARDWARE_REGISTER_WAIT(R_RTC->RCR2_b.HR24, 1);
    }

    Thanks!