Hi there,
I was trying to run the sx1261 Lora module on the RE01-1500KB devkit board.
I found a sample code for RE01-256KB and tried to port it to the 1500 version.
First, I tried the change device button in the e2studio, which did not work and then tried to copy the related code of Lora I 256KB version to 1500KB version.
It seems that the Lora code is optimized for the 256KB version. The final code is compiling but still, the Lora module is not working and there are some differences in registries of RE01-1500KB and RE01-256KB.
Can anyone help me on this matter?
My question is that is this module compatible with 1500KB and how I can port the code from the 256KB version.
Thank you so much.
Best regards,
MSH.
Hi Msh,
the LoRa project for the RE01-1500 is somewhat different to the RE01-256 project you obtained.
I can send it to you but cannot figure out how to attach it to this forum thread...... any ideas?
Regards,
Lou
Dear Lou,
Thank you for your reply and help,
I guess the best way is to upload it on Github or google drive and share the link with me here.
Thank you so much once again.
MSH
Hi MSH,
I posted the project in the Synergy Media Gallery:
https://renesasrulz.com/synergy/m/mediagallery/3477
Dear Lau,
Thank you so much for the help,