Hi,
I would like to ask if there is a possibility to program a RL78 family microcontroller (R5F100) without any Renesas programmer? Using some diy programmer or another housing method?
Thanks in advance.
Marcin
Hi to all. Am newer to the renesas controller. I am using R5F102AAA. am having Windows 10 OS. am installed Cygwin. Am confused for the next stage. if any one available then kindly given the details for serial programming. Am already prepared the hardware based on the given circuit. thanks in advance
You can use the hardware and software to write RL78/G13, but you cannot read the memory.In fact, there's no way you can read the memory, just compare a file with the memory data is possible.
Thank you,
Andre
Hi Uva,
Did you download the windows tools from here?
https://github.com/msalau/rl78flash/releases/download/v0.7.0/rl78flash-0.7.0-win64.zipThe usage examples are very clear too:
https://github.com/msalau/rl78flash
Hello,
Please create a new post as this thread is very old.
Best regards
Yes sir. am download the windows tool from the above link. Download and extract the files. When am try to run the application means it will automatically close suddenly. Not even open the application.
Thank you