This discussion has been locked.
You can no longer post new replies to this discussion. If you have a question you can start a new discussion

[RL78/G13] - EEPROM Emulation Library

Hello,

We need to use EEPROM Emulation Library for writing and reading data to flash.
We got the application note and docs for rl78/g13 cc-rl

But we need a sample reference code for rl78/g13. So that we can understand the code.

Please can you provide the sample code link for EEPROM Emulation Library? (EEL  and  FDL libraries)

Thank you in advance,




[locked by: AZ_Renesas at 8:01 (GMT 0) on 12 Feb 2024]
Parents
  • Which EEL are you looking to use?  Unfortunately there is a distinct lack of sample code available for the FDL/EEL on RL78.

    Type T01 / Standard - for larger memory devices, typically requires > 4KB of on-chip data-flash, higher RAM+ROM requirement to use

    Type T02 / Tiny - for smaller memory devices, requires less resources (RAM+ROM) from the application

    If you search this forum you will find many threads on this topic.

  • Hello JimB,

    Thank you for your reply. We were looking to use Type T02. Can we get a sample code for RL78/G13 to understand how to implement the EEPROM Emulation library?

    Thank You

Reply Children