Hello,We need to use EEPROM Emulation Library for writing and reading data to flash.We got the application note and docs for rl78/g13 cc-rlBut we need a sample reference code for rl78/g13. So that we can understand the code.Please can you provide the sample code link for EEPROM Emulation Library? (EEL and FDL libraries)Thank you in advance,
Which EEL are you looking to use? Unfortunately there is a distinct lack of sample code available for the FDL/EEL on RL78.
Type T01 / Standard - for larger memory devices, typically requires > 4KB of on-chip data-flash, higher RAM+ROM requirement to use
Type T02 / Tiny - for smaller memory devices, requires less resources (RAM+ROM) from the application
If you search this forum you will find many threads on this topic.
Hello JimB,Thank you for your reply. We were looking to use Type T02. Can we get a sample code for RL78/G13 to understand how to implement the EEPROM Emulation library?Thank You
RL78-EEL_T02-CCRL-R5F100LE.zip
Attached is a project using CC-RL on the command-line for R5F100LE. You didn't mention the exact device or which compiler you are using, but this is a start.
Thank You for guiding me.We were using R5F100LF CCRL compiler v1.11.00, e2 studio