RL78 - LIN communication - delay between 2 transmissions

Hi,

I'm using RL78 F13 48 pin controller with LIN.

LIN IC used is TJA1021 - Master.

2 slaves are connected to the master & in while loop in 50 ms timer interval i am trying to transmit header to both the slaves one by one to receive data.

If i add around 2.5 ms of delay between both transmissions - LIN communication is working fine.

Otherwise I'm unable to get data from LIN.

-------------------------------------------------------------------

Example: 

Works fine with a delay between 2 transmissions.

LIN_Master_HeaderTransmit(0x81);  //LIN Slave 1
for(int i =ZERO; i<=2500; i++) 
{
    Wait1us();
}
LIN_Master_HeaderTransmit(0x82);  //LIN Slave 2

----------------------------------------------------------------------

The below code does not work:

LIN_Master_HeaderTransmit(0x81);  //LIN Slave 1

LIN_Master_HeaderTransmit(0x82);  //LIN Slave 2

----------------------------------------------------------------------

We are not supposed to have a delay in the program, so kindly let me know your comments on this.

Is the delay expected ? or will it work without the delay?

Thank you.

Parents Reply
  • The best way to do this is to wait for the send end interrupt and then start receiving data. Similarly, you can wait then for the receive end interrupt and then start the next function. Of course this will require some processing inside the ISRs.

    You can do this with delay but it would not be as efficient.

Children