Hi, I would like to have Self-Programming library for IAR version 3.10 (the fsl.a). Currently I have file fsl.87 but it seems the IAR FS 3.10 cannot understand this file.
Best regards,
You don't mention which device you are using, but assuming it is not one of the newer devices that requires RFD (i.e. F2x, G2x, G15), then you would would need to download the installer package:
Flash Self Programming Library Type01 Package Ver.3.00 for the RL78 Family
When running the installer you would need to choose IAR v2.10 as the component to install:
V2/V3/V4/V5 supports the ELF file format while the V1 components support the legacy UBROF file format.