Hello, I am currently working with the QB-R5F10BMG-TB card together with the IAR program. I have imported the example for "rlin3-slave" but when I try to pass it to debug (E1 emulator [R0E000010KCE00]) I get an error that is: Does anyone know what causes this and if there is a way to run and test the sample code correctly?
Hello,
Thanks for reaching out Renesas Engineering Community!
Could you please give us the exact IAR version you are using?
There is a separate IAR Workbench for RL78 available to download from here:
https://www.iar.com/products/architectures/renesas/iar-embedded-workbench-for-renesas-rl78/
With all the necessary plugins and drivers for Renesas Emulators.
Are you using this version?
Thank you!
Best Regards,
IK
I'm using IAR EW for Renesas RL78 4.21.1
Probably plugins and drivers aren't the problem, because Startup and Applilet examples work correctly.
I have this issue with LIN master LIN slave example.
Kind regards,
skiner876
Hello again,
Could you please send me a picture of debug settings for the specific project?
On what hardware are you trying to connect and run this example build? Have you tried other projects / builds, is this issue only with this particular project? Can you connect to the hardware using the CS+ for CC IDE/debugger?
You could try creating a new debug-only project and load the ELF file built from this LIN demo, as a way to start from scratch and possibly avoid and incompatible setting from the legacy tool version project.