Bootswapping operation is very unstable, even more in release

Hi everyone,

Context of the project

I'm working on a bootloader project based on RL78. I set my memory like this : 

This idea is to jump from application to bootloader when I want to update the application and to jump from bootloader to application when I'm finished with the upload.

Major Issue

I'm able to start bootloader, flash the program, jump to application, jump to bootloader and flash program again. But this is ok like 50% of the time in DEBUG. The first start and flash is always working, the first jump is almost always working and after that it depends.

In release mode, it is even worse. I can start bootloader, flash the program and most of the time I can't even jump to the application

How did I code that ?

I'm based on the renesas FSL library and working on the R5F10DPJ microcontroller. To perform the bootswapping, I'm using this function : 

void Flash_SwapBootCluster()
{
	fsl_u08 fsl_status;
	UINT32 wait;
	
	// Open FSL and prepare all functions
	FSL_Open();
	FSL_PrepareExtFunctions();

	// Invert bootflag to start correct bootloader and close FSL
	fsl_status = FSL_InvertBootFlag();
	while(fsl_status != FSL_OK)
	{
		fsl_status = FSL_InvertBootFlag();
	}

	// Close FSL
	FSL_Close();

	/* Delay */
	wait = (UINT32)0;
	while(wait < (UINT32)10000)
	{
		wait++;
	}

	// Perform swapping of bootcluster
	fsl_status = FSL_SwapBootCluster();
	while(fsl_status != FSL_OK)
	{
		fsl_status = FSL_SwapBootCluster();
	}
}

I start to be out of idea, am I doing something wrong with this boot swapping ?

Thanks in advance and have a good day !

Parents Reply
  • The RAM initialization happens during startup in the cstart file as I mentioned on the post I shared. The RAM initialization has nothing to do with linker file.

    The cstart file will just fill the RAM with an initial value so any RAM parity errors are prevented.

    The linker will reserve the self RAM area so that nothing else is placed there so the flash library can use this are for its operations.

Children
  • My linker file is used to set the value of the stack, to process the RAM initialization through the assembly code you mentionned in the other post.

    I reserved selfram in both of my linker script but still, everything works in debug and not in release, always blocked after the jump to application.

    Maybe I can add more context to my project:

    1. I'm flashing a first program, the bootloader, which needs to update the flash for the second program

    2. To communicate with it, we use CAN bus. So after flashing the bootloader, I send data to flash the program (which is boot cluster 1 and application)

    3. When finished, I jump from bootloader to application

    4. I send a frame test to check if the application answers. In debug, it always answer. In release (which I program using a .s19 file on RFP), the frame I send is never received

  • Can you show what modifications have you done in the cstart file to initialize whole RAM ?

  • I did no modification.

    My cstartup is like this (at least the part similar to the other post) : 

    ?C_STARTUP:
    `@cstart`:
    __program_start:
            DI
    
            MOV     A, #(_NEAR_CONST_LOCATION & 1)  ; Near/Far, set mirror area
            MOV1    CY, A.0
            MOV1    PMC.0, CY
            
            MOVW    SP, #sfe(CSTACK)
    
    
            ; Init stack segment for as the generated code may sometimes
            ; access the 4th byte of a return address before it is initialized
            MOVW    HL, #sfb(CSTACK)
            MOVW    BC, #LWRD(sizeof(CSTACK))
            CMP0    C
            SKZ
            INC     B
            MOV     A, #0xCD        ; 0xCD to fool C-SPY's stack limit check
    loop_s:
            MOV     [HL], A
            INCW    HL
            DEC     C
            BNZ     loop_s
            DEC     B
            BNZ     loop_s
    
            MOV     CS, #0

    And, through the linker file, I update the CSTACK value:

    //-------------------------------------------------------------------------
    //      Stack segment.
    //-------------------------------------------------------------------------
    -Z(DATA)CSTACK+_CSTACK_SIZE=FBF00-FFEE0

  • The RAM will not be entirely initialized with the default cstart file.

    Please modify according to this post:

    https://community.renesas.com/automotive/rh850/f/rh850-forum/33274/ram-parity-error-in-rl78-d1a-controller

    As you can see my cstart file covers the entire address range of RAM - not only stack.

  • Hi, I finally understook what you mean and I added a new cstartup file to both of my project and hardcoded values that you told me about. I also had to check 'Override default program entry'.

    But, unfortunately, the process still doesn'r work in release mode :/ 

    1. I added new cstartup + redo my linker file for the application. The application is able to communicate in debug. I flashed the application throught RFP and it is still communicating

    2. I did the same with the bootloader, it works too

    3. I start the bootloader in debug mode through IAR. I flash the application through CAN bus and then jump to application: the application is communicating

    4. I flash the bootloader through RFP. I flash the application through CAN bus (and I can assure you that the bootloader is communication). Then I jump to application : Everything is blocked.

    I'm running out of idea :/ Can a softreset (FSL_ForseReset in my case) block the MCU definitely?

  • What do you mean by 'added a new cstart file' ? The cstart file is only one. Just add the lines to initialize RAM in the existing cstart file:

    If you pause the program after these lines you should see the RAM filled with 0xAA vaues.

    cstart.zip

  • What I meant is that IAR is based, by default, on the cstartup.s87 located in installation folder. So I copy paste it to my project and modified it to avoid modifying the default file for other project.

    Here is my cstartup file, for IAR

     cstartup.zip

    I modified those lines since it look the same as you for your startup file (In comment, after 'Adrien -', is the initial line)

            ; Init stack segment for as the generated code may sometimes
            ; access the 4th byte of a return address before it is initialized
            MOVW    HL, #LWRD(0xBF00) ;Adrien - MOVW    HL, #sfb(CSTACK) ;
            MOVW    BC, #LWRD(0x3FE0) ;Adrien - MOVW    BC, #LWRD(sizeof(CSTACK))
            CMP0    C
            SKZ
            INC     B
            MOV     A, #0xCD        ; 0xCD to fool C-SPY's stack limit check
    loop_s:
            MOV     [HL], A
            INCW    HL
            DEC     C
            BNZ     loop_s
            DEC     B
            BNZ     loop_s
    
            MOV     CS, #0

    I tried added your lines in my startup file but I got errors unfortunately. I'm quite a newbie in assembly :/ 

    Sorry for taking a lot of your time with this issue

    EDIT : I also tried another thing, set the RPERDIS flag to 1, to avoid reset link to RAM parity error

    EDIT 2 : After reset, RPERDIS is reset to 0 and a parity error might happen before I set it again so it may be useless in my case then

    EDIT 3 : Alright, RAM Initialization was the answer like you said. It was important to fill with 0xAA while my code was filling with 0xCD. Thanks a lot !

  • Hello,

    That's very good news.

    One doubt about your last comment though. I do not think the value for RAM initialization is important to prevent RAM parity errors.

    My guess is that your RAM was not fully initialized before but after you modified the cstart file as instructed, the RAM is now initialized with a random value (0xAA in this case) and the RAM parity errors are prevented.

    If a reset will occur after a RAM parity error is controlled by RPERDIS bit:

    So if you have this bit to its default value 0 and everything works as expected then no RAM parity errors occur during RAM access.

  • That's strange because everything is working fine since I only modified the 0xCD to 0xAA but I guess maybe something was not taken into account and then the RAM was not correctly initialized

  • So instead of 0xAA in the lines of code, you filled with 0xCD and it didn't work ?