How to separate flash memory

Hi team,

            The controller RL78_G23-(R7F100GSN2DFB) have 768 KB code flash memory. controller should need to keep the main application code & RL78_G13 application code. So that purpose the flash memory was needed to separate two sections. So how to make this appropriate setting in RL78_G23 controller. please let me know

Parents Reply
  • From first image - we need to separate the flash memory? if yes. 

    example: The RL78_G23 µC have 768 KB code flash memory. But run time code was 60 KB. Now where I should start address the memory separation to load the .MOT file for transferring to RL78_G13 µC. help to me

Children