RFP shows that a COM port and 2-wire UART can be used to program a target RL78/G23. It also allows configuring a reset signal from one of the control lines (DTR/RTS)According to documentation I've read, including "RL78 Microcontroller (RL78 Protocol C) Serial Programming Guide" R01AN5756EJ0100, TOOL0 is essential to enter programming mode.Am I misunderstanding the RFP in that it can program a target MCU using two wire communications?Thanks.
Hello,
RFP can support serial programming using 2-wire UART if the dedicated UART pins TOOLTxD and TOOLRxD are used:
But, isn't a specific sequence required on TOOL0 to enter programming mode before 2-wire communications can take place on Tx/Rx? RFP allows /RESET to be controlled but what physical pin would the TOOL0 signal come over from the PC?
TOOL0 should be handled accordingly so the device enters flash memory programming mode:
But following the level on TOOL0 when /RESET goes low->high, (<1>, <2>) 1 byte of data is still required on TOOL0 to proceed to enter flash memory programming mode. How does that get from RFP to the target MCU?
As listed RFP supports 2-wire dedicated UART with TypeD connection settings:
For examples of recommended connections of type D, refer to the RL78 Debugging functions Using Serial port Application notes
However, I see no reason to prefer 2-wire UART over single wire UART for RFP connection. With a 2-wire connection you will just use 1 more pin for the same baud rate.
TOOL0 needs to be controlled by the programmer to set the mode. Connect TOOL0 to the incoming TxD via a serial resistor. The G23 Fast ProtoBoard is a suitable reference design (and is very low-cost).
There is sample code to use a Raspberry Pi to program RL78/G23: