Hello there,
I have wroted my code a while ago. And I need to modify it and add some variable.
So, when I add it, the MCU get reset while working. In my opinion, some rom/ram area overwrited.
I am not much experienced, so could not find solution. Adding some picture below. If I add this two 16-bit variable, the mcu get reset.
Thank you for your help.
Hi,Can you check the status of Reset control flag register (RESF) and see what is cause of the reset ?
Additionally confirm the exact MPN you are using.Best Regards,
Vasanth