While function did not work below image

Hi Team,

The while function did not work in the below section.  on the RL78/G23 microcontroller.

The "delay_wait_timer" variable is decremented in a 1ms timer interrupt. When the "delay_wait_timer" reaches zero, the microcontroller exits the first while loop but does not exit the case.

NOTE: Address didn't create. while debugging