RL78/G23 Can't flash the program to the MCU

Before that, I encountered a RAM parity error. We found a temporary solution by deleting the settings for the ROM-to-RAM mapped section.
Additionally, other functions that could not operate correctly before deleting mapped section are now working (though this is only when debugging by E2 debugger).
After deleting the settings, we encountered a problem when writing software using E2 Lite and Flash Pro 6 again. The errors are shown below:
E2-Lite: Error (E0000305): Specified file contains data outside the device's memory area.
FP6: ERROR (E302): HEX file exceeds target device flash range.
I have attached the map files (before and after the change). Please kindly investigate what the problem might be.

R7F100GGG(Setting ROM RAM map section).txtR7F100GGG(No setting ROM RAM map section).txt
*I couldn't upload the .map file, so I changed it to .txt.

Could you suggest what the problem might be and how to solve it?
Parents Reply Children
No Data