Reg : UART2 interrupt did not occur

Hi Team,

I am working with the R7F100GSN - RL78/G23 controller, and the UART interrupt is not being triggered. However, data is being received at the µC pins, but the interrupt is not being generated. UART2 settings are below given, also start the UART2 module.