PicoFDL (T04) with IAR RL78 2.xx

Hello,

MCU: RL78/G13

We are now migrating from IAR 1.xx to 2.xx due to other issues and our dataflash library doesn´t compile with the new version because the tool provided by Renesas "RENESAS_FDL_RL78_T04E_V1.20" only allows generating libraries for 1.20 version of IAR.

Should we expect Renesas to update this tool for new versions soon? Or is it better to switch to other flash emulation library (T01 e.g.) assuming the cost in code size? Any alternative?

Thanks in advance!

Parents Reply
  • This is extremely incomprehensible.
    Because your project, in which I changed only the frequency source and deleted from the project * .a, it behaves normally with my E1 debugger.
    I mean the food on the board itself, and not what you feed it.
    Try to debug the FDL function to see where the problem is. I assure you that the call agreement has not changed since IAR 2.1.
Children
No Data