RL78 Pico Flash Data Library T04 usage example IAR

A usage example of the PicoFDL library with the IAR tool chain. Includes explanation slides IAR EW workspace. 

Requires PicoFDL library, Applilet for RL78G13, IAR EW for RL78 , E1 and RL78G13 target board.

Anonymous
  • It is a very good example. But to read values from data flash I recommend to use the read command of the Flash Library instead of the direct access to be sure that only the allowed 8bit access is used and to avoid a known restriction of data flash read access and DMA (-> RL78/G13 Renesas Direction of Use TN-RL*-A009A/E)