error(E0000016): The program file is not correct

Hello,

I have the following error message when i load the program file: The program file is not correct.

I use the Renesas Flash Programmer V3.00.00 whith a microcontroler R5F100AC.

In  IAR Embedded workbench IDE RL78 2.21.1, i replaced my file test.out per test.hex in the linker.

It is correct.

Can you help me?

Thanks you.

Anonymous