No toolchain set or toolchain not integrated.

Hi, i am new e2 studio and renesas.

 

i have software project and some how i change my pc then i reinstall e2 studio V6.0.

 

Then i got below error

Extracting support files...
[ERROR] No toolchain set or toolchain not integrated.
09:19:42 **** Incremental Build of configuration HardwareDebug for project Besgen ****
make -j4 all
Cannot run program "make": Launching failed

Error: Program "make" not found in PATH
PATH=[D:/ProgramFiles/Renesas/e2_studio/eclipse//features/com.renesas.jre.win32.win32.x86_1.8.0.65/jre/bin/client;D:/ProgramFiles/Renesas/e2_studio/eclipse//features/com.renesas.jre.win32.win32.x86_1.8.0.65/jre/bin;D:/ProgramFiles/Renesas/e2_studio/eclipse//features/com.renesas.jre.win32.win32.x86_1.8.0.65/jre/lib/i386;C:\Program Files (x86)\GCC for Renesas RX 4.8.4.201703-GNURX-ELF\rx-elf\rx-elf\bin;C:\ProgramData\Oracle\Java\javapath;C:\Program Files (x86)\STMicroelectronics\st_toolset\asm;C:\Python26\Lib\site-packages\PyQt4\bin;C:\Program Files (x86)\Intel\iCLS Client\;C:\Program Files\Intel\iCLS Client\;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files (x86)\SlikSvn\bin\;C:\Program Files (x86)\Microsoft SQL Server\90\Tools\binn\;D:\MatlabKurulum\bin;C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8;C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM32;C:\Program Files\TortoiseSVN\bin;C:\Program Files (x86)\COSMIC\CXSTM8_32K;C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8;C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM32;C:\Program Files\gs\gs9.22\bin;C:\Program Files\gs\gs9.22\lib;D:\ProgramFiles\Renesas\e2_studio\eclipse;]

09:19:42 Build Failed. 1 errors, 0 warnings. (took 99ms)

 

When i check tool chain. it look like Ok as you seen below;

 

 

Where i do wrong?Can you help me?

Parents Reply Children
No Data