hi, i can't read flash M16c - m30280F8 show id code verification
present i'want read flash have id code verification
What are the steps to fix it? When I want to read data to use with another flash
It isn't clear what the issue is. Are you wanting to read the memory from a MCU that is protected with the ID code, but you do not have the code? If this is the case, I'm sorry but you are out of luck…
It isn't clear what the issue is. Are you wanting to read the memory from a MCU that is protected with the ID code, but you do not have the code? If this is the case, I'm sorry but you are out of luck, there is no way to bypass the check of the ID code.